[#5946] Disable anomaly 456 on bf526-ezbrd, gadget serial in dma mode fails to work
Submitted By: Vivi Li
Open Date
2010-03-05 05:16:59
Priority:
Medium Assignee:
Bob Liu
Status:
Open Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Category:
N/A Board:
Processor:
BF526 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Duplicate
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2010_Jan_22
App binary format:
Summary: Disable anomaly 456 on bf526-ezbrd, gadget serial in dma mode fails to work
Details:
Anomaly 456 is disabled on bf526-ezbrd, gadget serial driver in dma mode fails to work with Generic USB Serial driver or Linux ACM driver on Linux host.
Bellow is the log for gadget serial with Generic USB Serial driver.
On target:
--
root:/> modprobe g_serial use_acm=0
g_serial gadget: Gadget Serial v2.4
g_serial gadget: g_serial ready
g_serial gadget: high speed config #1: Generic Serial config
root:/>
root:/> dmesg|tail
dma_alloc_init: dma_page @ 0x0251f000 - 512 pages at 0x03e00000
IP-Config: Complete:
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf526-ezbrd, domain=, nis-domain=(none),
bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=
Freeing unused kernel memory: 3464k freed
PHY: 0:01 - Link is Up - 100/Full
On host:
uclinux63-527-usbdev:..testsuites/usbdev # sudo mount -t usbfs none /proc/bus/usb/
mount: none already mounted or /proc/bus/usb/ busy
uclinux63-527-usbdev:..testsuites/usbdev # mount
/dev/sda3 on / type ext3 (rw,acl,user_xattr)^M
proc on /proc type proc (rw)^M
sysfs on /sys type sysfs (rw)^M
debugfs on /sys/kernel/debug type debugfs (rw)^M
udev on /dev type tmpfs (rw)^M
devpts on /dev/pts type devpts (rw,mode=0620,gid=5)^M
/dev/sdb1 on /home type ext3 (rw,acl,user_xattr)^M
/dev/sda2 on /opt type ext3 (rw,acl,user_xattr)^M
fusectl on /sys/fs/fuse/connections type fusectl (rw)^M
securityfs on /sys/kernel/security type securityfs (rw)^M
none on /proc/sys/fs/binfmt_misc type binfmt_misc (rw)^M
gvfs-fuse-daemon on /home/test/.gvfs type fuse.gvfs-fuse-daemon (rw,nosuid,nodev,user=test)^M
none on /proc/bus/usb type usbfs (rw)^M
uclinux63-527-usbdev:..testsuites/usbdev # cat /proc/bus/usb/devices|grep -i gadget
S: Product=Gadget Serial v2.4^M
uclinux63-527-usbdev:..testsuites/usbdev # sudo modprobe usbserial vendor=0x0525 product=0xA4A6
uclinux63-527-usbdev:..testsuites/usbdev # lsmod |grep usbserial
usbserial 51116 0
usbcore 164940 10 usbtest,usb_storage,cdc_acm,usbserial,cdc_ether,usbnet,usbhid,ehci_hcd,uhci_hcd
uclinux63-527-usbdev:..testsuites/usbdev # stty -F /dev/ttyUSB0 -icrnl
uclinux63-527-usbdev:..testsuites/usbdev # cat /dev/ttyUSB0 > host_file
root:/> ls /dev/tty*
/dev/tty /dev/ttyBF1 /dev/ttyGS0
root:/> cat /proc/kallsyms > test_file
root:/> cat test_file > /dev/ttyGS0
(it hangs here)
Follow-ups
--- Sonic Zhang 2010-08-24 00:10:00
No hardware fix in bf526 v0.2 for anomaly 456 is reported to
processor.support@analog.com.
Duplicate of 5944.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
anomaly.diff application/octet-stream 906 Vivi Li
config.linux.usbdev.dma application/octet-stream 37916 Vivi Li