[#5951] ADAU ASoC drivers fail to build after linux-2.6.33 upgrade
Submitted By: Mike Frysinger
Open Date
2010-03-05 09:34:22 Close Date
2010-03-16 10:29:41
Priority:
Medium Assignee:
Cliff Cai
Status:
Closed Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Category:
N/A Board:
Processor:
ALL Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
trunk
App binary format:
Summary: ADAU ASoC drivers fail to build after linux-2.6.33 upgrade
Details:
the machine interfaces fail like so:
sound/soc/blackfin/bf5xx-adau1361.c: In function ‘bf5xx_adau1361_hw_params’:
sound/soc/blackfin/bf5xx-adau1361.c:80: error: too few arguments to function ‘codec_dai->ops->set_pll’
sound/soc/blackfin/bf5xx-adau1381.c: In function ‘bf5xx_adau1381_hw_params’:
sound/soc/blackfin/bf5xx-adau1381.c:80: error: too few arguments to function ‘codec_dai->ops->set_pll’
sound/soc/blackfin/bf5xx-adau1761.c: In function ‘bf5xx_adau1761_hw_params’:
sound/soc/blackfin/bf5xx-adau1761.c:80: error: too few arguments to function ‘codec_dai->ops->set_pll’
while the codecs fail like so:
sound/soc/codecs/adau1361.c: In function ‘adau1361_probe’:
sound/soc/codecs/adau1361.c:739: warning: initialization from incompatible pointer type
sound/soc/codecs/adau1361.c:900: error: implicit declaration of function ‘snd_soc_init_card’
sound/soc/codecs/adau1371.c: In function ‘adau1371_probe’:
sound/soc/codecs/adau1371.c:977: error: implicit declaration of function ‘snd_soc_init_card’
sound/soc/codecs/adau1381.c: In function ‘adau1381_probe’:
sound/soc/codecs/adau1381.c:589: warning: initialization from incompatible pointer type
sound/soc/codecs/adau1381.c:745: error: implicit declaration of function ‘snd_soc_init_card’
sound/soc/codecs/adau1761.c: In function ‘adau1761_probe’:
sound/soc/codecs/adau1761.c:765: warning: initialization from incompatible pointer type
sound/soc/codecs/adau1761.c:950: error: implicit declaration of function ‘snd_soc_init_card'
Follow-ups
--- Cliff Cai 2010-03-16 04:51:38
fixed
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found