[#5987] Can not detect spimmc when ad1836 is also installed on bf537-stamp
Submitted By: Vivi Li
Open Date
2010-03-24 07:11:53 Close Date
2010-03-29 06:32:26
Priority:
Medium Assignee:
Barry Song
Status:
Closed Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Category:
N/A Board:
N/A
Processor:
BF537 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2010_Jan_22
App binary format:
N/A
Summary: Can not detect spimmc when ad1836 is also installed on bf537-stamp
Details:
Can not detect spimmc when ad1836 is also installed on bf537-stamp.
Last passed version:
--
kernel: Linux release 2.6.33.1-ADI-2010R1-pre-svn8523, build #40 Mon Mar 22 02:51:21 GMT 2010
toolchain: bfin-linux-uclibc-gcc release gcc version 4.3.4 (ADI-trunk/svn-3815)
user-dist: release svn-9521, build #787 Mon Mar 22 02:50:03 GMT 2010
--
First failed version:
--
kernel: Linux release 2.6.33.1-ADI-2010R1-pre-svn8527, build #4 Tue Mar 23 07:08:12 GMT 2010
toolchain: bfin-linux-uclibc-gcc release gcc version 4.3.4 (ADI-trunk/svn-3951)
user-dist: release svn-9522, build #50 Tue Mar 23 07:06:56 GMT 2010
--
--
Linux version 2.6.33.1-ADI-2010R1-pre-svn8542 (test@uclinux58-mmc-usblan-btuart) (gcc version 4.3.4 (ADI-trunk/svn-3951) ) #8 We0
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart0] enabled
early printk enabled on early_BFuart0
Limiting kernel memory to 56MB due to anomaly 05000263
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x0014a840
rodata = 0x0014a840-0x001b9a54
bss = 0x001ba000-0x001cacd4
data = 0x001cacd4-0x001de000
stack = 0x001dc000-0x001de000
init = 0x001de000-0x008a9000
available = 0x008a9000-0x03800000
DMA Zone = 0x03f00000-0x04000000
Hardware Trace Active and Enabled
Boot Mode: 0
Blackfin support (C) 2004-2009 Analog Devices, Inc.
Compiled for ADSP-BF537 Rev 0.2
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 500 MHz core clock and 125 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-back) in data cache
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 14224
Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 47908k/65536k RAM, (6956k init code, 1318k kernel code, 590k data, 1024k dma, 7740k reserved)
Hierarchical RCU implementation.
NR_IRQS:138
Configuring Blackfin Priority Driven Interrupts
console [ttyBF0] enabled, bootconsole disabled
console [ttyBF0] enabled, bootconsole disabled
Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)
Security Framework initialized
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (35 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
stamp_init(): registering device resources
bio: create slab <bio-0> at 0
Advanced Linux Sound Architecture Driver Version 1.0.21.
Switching to clocksource bfin_cs_cycles
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
msgmni has been set to 93
io scheduler noop registered
io scheduler cfq registered (default)
bfin-uart: Blackfin serial driver
bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART
brd: module loaded
bfin-spi bfin-spi.0: chipselect 4 already in use
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7
bfin_mii_bus: probed
bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)
bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
dma rx:5 tx:6, err irq:46, regs:ffc00900
dma_alloc_init: dma_page @ 0x028cd000 - 256 pages at 0x03f00000
asoc: AD183X <-> bf5xx-tdm mapping ok
ALSA device list:
#0: bf5xx_ad183x (AD183X)
TCP cubic registered
NET: Registered protocol family 17
IP-Config: Complete:etting system clock to 2014-11-15 13:19:27 UTC (1416057567)
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf537-stamp, domain=, nis-domain=(none),
bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=
Freeing unused kernel memory: 6956k freed
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - https://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.15.3 (2010-03-24 08:15:42 GMT) hush - the humble shell
root:/> PHY: 0:01 - Link is Up - 100/Full
root:/> version
kernel: Linux release 2.6.33.1-ADI-2010R1-pre-svn8542, build #8 Wed Mar 24 08:19:16 GMT 2010
toolchain: bfin-linux-uclibc-gcc release gcc version 4.3.4 (ADI-trunk/svn-3951)
user-dist: release svn-9527, build #129 Wed Mar 24 08:18:00 GMT 2010
root:/> ls /dev/
audio network_latency ram13 rtc0
console network_throughput ram14 snd
controlC0 null ram15 stderr
cpu_dma_latency pcmC0D0c ram2 stdin
dsp pcmC0D0p ram3 stdout
fd ptmx ram4 timer
full pts ram5 tty
kmsg ram0 ram6 ttyBF0
log ram1 ram7 urandom
mdev.seq ram10 ram8 watchdog
mem ram11 ram9 zero
mixer ram12 random
root:/>
--
Follow-ups
--- Barry Song 2010-03-29 02:53:09
A device uses one slave select, but in board file:
#if defined(CONFIG_SND_BF5XX_SOC_AD183X) \
|| defined(CONFIG_SND_BF5XX_SOC_AD183X_MODULE)
{
.modalias = "ad183x",
.max_speed_hz = 3125000, /* max spi clock (SCK) speed in HZ
*/
.bus_num = 0,
.chip_select = 4,
.platform_data = "ad1836", /* only includes chip name
for the moment */
.controller_data = &ad1836_spi_chip_info,
.mode = SPI_MODE_3,
},
#endif
#if defined(CONFIG_MMC_SPI) || defined(CONFIG_MMC_SPI_MODULE)
{
.modalias = "mmc_spi",
.max_speed_hz = 20000000, /* max spi clock (SCK) speed in
HZ */
.bus_num = 0,
.chip_select = 4,
.platform_data = &bfin_mmc_spi_pdata,
.controller_data = &mmc_spi_chip_info,
.mode = SPI_MODE_3,
},
#endif
In hardware connection, to run AD1836 and MMC at the same time, pls switch
AD1836 cs to PF5 or other, not sharing with MMC. And change the board file.
-barry
--- Vivi Li 2010-03-29 06:31:03
Build script failed to change chip_select value because board file has been
changed.
Fixed in test script.
Close it.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.linux.spi_coexistence application/octet-stream 37075 Vivi Li
config.config.spi_coexistence application/octet-stream 47940 Vivi Li