Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers
    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers

    Introduction to Industrial I/O, libIIO, and Python software tools

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Evaluating Power Supplies with Different Compensation Settings

    Evaluating Power Supplies with Different Compensation Settings

EngineerZone
EngineerZone
Linux Bug Archive
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Linux Bug Archive
  • Processors & DSP
  • Software & Development Tools
  • Linux Distribution for Blackfin
  • Linux Bug Archive
  • Cancel
Linux Bug Archive
Documents [#6033] traps test case 93 will make kernel panic on bf526 when stack set to L1 instruction(2010)
  • Q&A
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ad1836: FAQ
  • +ad1938: FAQ
  • +ad1939: FAQ
  • +AD5280: FAQ
  • +ad73311: FAQ
  • +adau1361: FAQ
  • +adau1371: FAQ
  • +adau1373: FAQ
  • +adau1761: FAQ
  • +adp5588-gpio: FAQ
  • +adv7393: FAQ
  • +ADXL34x: FAQ
  • +bf518-ezbrd: FAQ
  • +bf518: FAQ
  • +bf51x: FAQ
  • -bf526-ezbrd: FAQ
    • [#5944] Disable anomaly 456 for bf526-ezbrd, gadget fs bulk test fails in dma mode (2010)
    • [#5945] Gadget ethernet fails to work in dma mode when anomaly 456 is disabled on bf526-ezbrd(2010)
    • [#5946] Disable anomaly 456 on bf526-ezbrd, gadget serial in dma mode fails to work(2010)
    • [#5947] Disable anomaly 456 on bf526-0.2-ezbrd, host can't find gadget ram storage in dma mode(2010)
    • [#6033] traps test case 93 will make kernel panic on bf526 when stack set to L1 instruction(2010)
    • [#6074] Build bf526 kernel with nand support fail(2010)
  • +bf527-ezkit: FAQ
  • +bf533-stamp/ezkit: FAQ
  • +bf533: FAQ
  • +bf538-ezkit: FAQ
  • +bf548-ezkit: FAQ
  • +BF54x: FAQ
  • +bf561-ezkit: FAQ
  • +bf5xx: FAQ
  • +bfin-mac driver: FAQ
  • +bfin-uclinux-gdb: FAQ
  • +bfin_can.c: FAQ
  • +Blackfin: FAQ
  • +bluetooth: FAQ
  • +Build kernel: FAQ
  • +Build: FAQ
  • +cfcard test: FAQ
  • [#6170] section mismatches in cifs code(2010)
  • [#6173] linphone testing problem(2010)
  • [#6190] BF561-EZKIT SMP kernel can not wake up by uart(2010)
  • [#6194] libxenomai.so.0 can't be found in xenomai kernel with fdpic mode(2010)
  • [#6207] Build error in CTS/RTS testing on board BF548-EZKIT(2010)
  • [#6251] pread/pwrite arent decoded correctly by strace(2010)
  • [#6253] strace build failed in trunk with outdated toolchain (missing asm/cachectl.h)(2010)
  • [#6255] Busybox inetd crashes/rsh noconnet/ssh(2010)
  • [#6265] libpng build fails due to not finding zlib(2010)
  • [#6271] "nand unlock" is an unsupported command in u-boot update in nand flash(2010)
  • [#6272] After update u-boot in spi flash, BF548-EZKIT can not boot from spi flash(2010)
  • +gadget fs bulk: FAQ
  • +gadget zero bulk: FAQ
  • +gadget zero control: FAQ
  • +Kernel xip: FAQ
  • +ltp test: FAQ
  • +microwin test: FAQ
  • +MPU kernel: FAQ
  • +Sl811-hcd.c USB: FAQ
  • +SPORT channel: FAQ
  • +trunk head kernel: FAQ
  • +usb otg driver: FAQ
  • +zlib: FAQ
  • +Illegal i2c: FAQ
  • +isp1362-hcd: FAQ
  • +Kernel: FAQ
  • +KGDBOE: FAQ
  • [#4646] Varittronix LCD driver mixes blue and Red
  • +serial driver: FAQ
  • +sigma firmware: FAQ
  • +spi transaction: FAQ
  • +strace FAQ
  • [#4787] [ltp] LTP test case shmctl01 failed in trunk for ltp-full-20081130
  • +tiff-4.0.0beta4: FAQ
  • [#5264] ping packet size test will fail for gadget ethernet test with DMA mode
  • +USBHOST: FAQ
  • +USB_EP_NI7_RXINTERVAL: FAQ
  • [#5257] Build usb gadget driver with DMA mode will fail
  • [#4708] Blackfin irda build fails for bf533-stamp
  • [#4735] unaligned accesses in qt webkit
  • [#5168] build cpufrequtils into fdpic format has error
  • [#5321] modprobe i2c lcd on bf533 stamp wait long time
  • [#4922] unwanted sound comes up after g_audio module is installed on BF548 and BF527
  • [#5176] app cpufrequtils in Blackfin app programs fails to build in FDPIC
  • [#5237] musb driver is broken after linux-2.6.30 update
  • [#5255] ping target board sometimes get wrong data byte for gadget ethernet pio mode
  • [#5336] canbus and ppifcd drivers can not be built on BF538-EZKIT
  • [#6614] Kernel panic frequently when test sdio mmc on bf518-ezbrd(2011)
  • +SPI driver: FAQ
  • [#4714] the first time to build mtd-utils will fail in trunk
  • [#5524] drivers/video/bfin_adv7393fb.c build fails in 2.6.31 due to old i2c usage
  • [#5525] drivers/video/bf537-lq035.c build fails in 2.6.31 due to old i2c usage
  • [#5399] no sound when record in board and listen in PC for linphone test of ad1836 on bf533-stamp
  • [#5458] Drivers Serial:bfin_5xx:ttyBFx fails to generate resume from standby
  • [#4647] build samba fails on trunk now for redefinition in fcntl.h
  • [#5526] ip0x board has broken UART defines after resource reorganization
  • [#5527] drivers/media/video/blackfin/blackfin_cam.c build fails in 2.6.31 due to old i2c usage
  • [#5352] bfin_sport.c setup 2D DMA
  • [#5528] fs/binfmt_elf_fdpic.c build fails when CONFIG_ELF_CORE is enabled in 2.6.31
  • [#5464] isram_write() seems to be busted
  • [#5376] mmap05 sometimes can not pass when MPU
  • [#5534] run aplay/arecord will make system panic after kernel upgraded to 2.6.31
  • [#5361] Microwin (nanox) failed on trunk using AD7897 touch screen
  • [#5544] Sport uart TX stop waiting loop is too long to block RX interrupt in PIO mode when do duplex communication
  • [#5363] spi mmc is not supported in bf533-stamp
  • [#5550] fail to flash ubifs.img to nand
  • [#5470] build xenomai fails for no switchbench
  • [#5437] mathtest fails to compile
  • [#5551] SPI message lost when bus locked
  • [#5370] alsa tool fails to work after wake up from mem in bf537-stamp with ad1836 (can't resolve symbol)
  • [#5561] [ltp ]Kernel dump info when run ltp test cases access02, chown03, fchmod06, fchown03, fchown04
  • [#5377] amixer fail to run on ad1836 audio driver on BF537-STAMP
  • [#5475] build mkfs.ubifs on trunk head fails
  • [#5562] [ltp]some ltp test case is broken for getipckey and getcwd
  • [#5487] build usb.c fail in testsuites/usbdev/ test at asm/swab.h
  • [#5489] t2/t4 failed in gadget zero bulk test with dma mode
  • [#5567] build nand for bf537 fails on trunk
  • [#5494] Run tftlcd test case in bf548-ezkit, kernel crashed at the end
  • [#4879] traps test case 21 exception 0x3f: l1_instruction_access would make kernel panic on bf533 stamp
  • [#5568] Framebuffer DMA Error!!
  • [#5515] 4 more trap cases fails on bf533
  • [#5379] run scratchpad case sometimes would fail
  • [#5519] pushing Blackfin serial resources to boards broke many boards
  • [#5389] build pictureflow fails at branch head
  • [#5531] Usb SL811 failed on uclinux2009r1-rc6 on bf532 board.
  • [#5523] Blackfin MUSB build fails after update to 2.6.31
  • [#5391] For ad1836 and ad1981b, sometimes sound shakes at the end
  • [#5404] build kernel with 0x2000 as BOOT_LOAD address sometimes would fails at build-busybox-1.13.4
  • [#5469] CPU hardly idles anymore in svn trunk
  • [#5695] Build bf537-stamp fails at ad73322 for the latest trunk
  • [#5702] build xenomai into fdpic format fails for no libnative.so
  • [#5427] ircp failed on bf533-stamp
  • [#5708] Kernel can not boot up when spimmc driver is interrupt drivern in PIO mode
  • [#5711] gfortran case default_format_1.exe fails on 09r1 kernel but pass on trunk head
  • [#5712] I2C client drivers using dev_pm_ops fail to receive suspend/resume callbacks
  • [#5715] libpcap fails to compile in trunk
  • [#5589] STLport build fails
  • [#5724] SPORT driver crash on reload
  • [#5449] bfin_sdh doesn't save and restore peripheral context upon resume
  • [#5580] GPIO pin not reserved for CTS function on SPORT-UART driver
  • [#5521] trunk head build fails at ipc/shm.c
  • [#5636] generic gpio works on bf533 in the opposite way
  • [#5637] Kernel crashed when arecord and aplay on bf537-stamp with SoC I2S audio
  • [#5647] SPI driver bus_unlock() does not schedule postponed SPI messages
  • [#5683] build nand fails for format error
  • [#5689] while two or multi spi devices use gpio cs, spi setup will fail
  • [#5558] bfin mac multi-cast sending fails to work
  • [#5816] PREEMPT_RT: cyclic test stalls in some test mode
  • [#5824] some kernel modules fail to link due to losing strcpy in trunk head
  • [#5707] error in user/procps/Makefile
  • [#5841] [ltp] ltp test case shmctl01/semctl01 can not execute
  • [#5605] Build bf537-stamp fail at bf5xx-i2s.c in latest trunk
  • [#5614] With latest toolchain in trunk, fail to build some apps and libs at fork
  • [#5625] Build microwin app fails in trunk with 4.3 toolchain
  • [#5626] Build lib mad fail at option "-fforce-mem" with gcc 4.3
  • [#5722] bfin_sport_spi broken by cs_gpio changes
  • [#5627] fail to control gpio used by led and button through /sys/class/gpio/
  • [#5927] PR bit other than RAF bit in EMAC OPMODE register should be set for promisuous mode in bfin_mac driver
  • [#5727] build e2fsprogs-1.41.12 fail sometimes because of compiling order
  • [#5631] Build lib confuse failed with gcc 4.3 toolchain
  • [#5759] fix build for pwlib
  • [#5651] Build lirc failed at missing files
  • [#5931] Trying to compile CAN4LINUX for BF537-STAMP board but compilation is failing
  • [#5656] Build iproute2 fails at trunk for dlfcn.h when built as FLAT
  • [#5743] sound/soc/blackfin/bf5xx-ad1938.c build fails after 2.6.32 upgrade
  • [#5801] No interrupt occurs when reconnect gadget device in OTG mode.
  • [#5657] [ltp] ltp test case mount03/umount03 fail with error of "No such device"
  • [#5808] mmc configuration error in make config
  • [#5804] bf531: ethernet not working when switching to 2009R1
  • [#5810] initial sp is given wrong value and INIT_TASK_DATA is not linked into data
  • [#6335] Build xip failed in fdpic format when xenomai is enabled
  • [#7224] undifined variable x25_address in ./user/net-tools/lib/x25_src.c
  • [#5598] bluez-utils has parallel build issues with parser.h
  • [#5668] Fail to build app bluez-utils
  • [#7251] Blackfin SPI driver doesn't handle repeated changes in CPOL, CPHA and LSBF correctly
  • [#5767] In 09r1.1 branch, all ltp test cases show stack overflow in bf561 SMP kernel
  • [#5684] touching keypad on bf548 will make system dead and restart
  • [#7287] Can not build usb.c with libaio
  • [#5687] SPI read/write be wrong after suspend to memory and resume
  • [#7315] [ltp] ltp test case getrusage04 from ltp-full-20120903 fails in trunk
  • [#7328] Fail to compile pthread_test after toolchain update
  • [#5876] Repeating rsh/rcp causes error "poll: protocol failure in circuit setup"
  • [#7329] Fail to compile netperf after toolchain update
  • [#7333] Test dll fails to run after toolchain update
  • [#5741] adau1371 and adau1761 fail to build after 2.6.32 upgrade
  • [#7337] [ltp] ltp test case mount02 fails in ltp-full-20120903
  • [#7338] [ltp] ltp test case mount03 fails in ltp-full-20120903
  • [#5821] Fail to build pngview on regression machines with suse 10.2
  • [#5900] hardware single stepping in userspace does not handle syscalls correctly
  • [#5659] [ltp] ltp test case eventfd01 fail
  • [#7339] [ltp] can not apply patch of lchown02 in ltp-full-20101031 to ltp-full-20120903
  • [#7343] [ltp] LTP test case chdir04 fails in ltp-full-20120903
  • [#7396] build netperf fails for undefined reference to `___CPU_ZERO'
  • [#7483] bfin_sport driver does not work well in TDM DMA mode
  • [#7506] Dropbear does not build
  • [#5757] drop USER_SQUASHFS_MKSQUASHFS7Z as squashfs 4.0 does not support 7z anymore
  • [#5758] fix build for libopenh323
  • [#5833] trap test running on the second core of bf561 has serveral fails
  • [#5755] romfs target fails for lib/pwlib
  • [#5760] fix asterisk build
  • [#5756] romfs target fails for lib/libopenh323
  • [#5877] SPI transmit cs_change flag not properly handled
  • [#5939] bfin-can fails to build after linux-2.6.33 upgrade
  • [#5879] GPIO controlled slave request may fail when bfin_spi_setup() gets executed twice
  • [#5774] [ltp]ltp test case will be killed by oom-killer on bf533-ezkit in 09r1 branch occasionally
  • [#5894] BF527 uImage Flashing issue(Copy to Flash... Flash not Erased)
  • [#5941] links fails in trunk due to using fork()
  • [#5942] build usb host fail when remove anomaly 456 for BF526-EZBRD
  • [#7250] On bfin ppi test, it fails to quit from slave when send "q" from master
  • [#7379] Fail to build alsa lib in latest trunk with upgraded toolchain
  • [#5792] enc28j60 spi net fails to ping with host on trunk head kernel
  • [#4436] BF527-EZKIT unable to receive large files over UART in DMA mode
  • [#4764] Kernel prints warning when booting from jffs2 rootfs in nor flash on bf548-ezkit
  • [#5903] Impossible to work properly with two or more SPI slave devices using spi_bfin5xx driver.
  • [#6386] build iproute2 may fail at ifstat.c sometimes in latest trunk(2010)
  • [#6331] There is error in adau1371 audio testing on bf527-ezkit(2010)
  • [#5933] BF561-EZKIT SMP kernel can not wake up from standby mode by uart interrupt
  • [#4713] dmacopy tries to test L2 on BF537
  • [#6564] dmacopy test on bf561-ezkit failed at sram_alloc in L1(2011)
  • [#4997] ppitest fails for bfin_ppi driver on bf537
  • [#5940] lynx fails in trunk due to using fork()
  • [#4104] Format usbdisk failed with mke2fs in trunk
  • [#6578] iccutils build fails at scalar.c(2011)
  • [#3883] ftp server crash after connetion or chdir with MidnightCommander4.6.1
  • [#4697] kernel crash on bf533-stamp/bf533-ezkit after config IP for ethernet port
  • [#4050] xip test case failed in BF548-EZKIT
  • [#3991] mmc_spi not working out of the box.
  • [#3996] dhcpcd not stable on BF548-EZKIT
  • [#5136] Linphone: Can't hear each other and "Data access misaligned address violation"
  • [#5214] trunk applications don't build with trunk toolchain due to missing fork()
  • [#4055] top (busybox) crashs
  • [#5162] Linphone: Data access misaligned address
  • [#4992] bfin_sdh fails to build for BF514/BF516
  • [#5570] reboot on bf527-ezkit with nand and ubifs enabled fails
  • [#4955] 548 SDH: netperf, iperf triggers libertas error
  • [#5522] Lib DirectFB-1.4.0 crashes when run DirectFB demo on SVN trunk
  • [#3882] copy file function cp, after few times consume all memory
  • [#4773] BF527 usb-ide hard disk error

[#6033] traps test case 93 will make kernel panic on bf526 when stack set to L1 instruction(2010)

[#6033] traps test case 93 will make kernel panic on bf526 when stack set to L1 instruction

Submitted By: Vivi Li

Open Date

2010-05-18 06:12:17     Close Date

2011-06-08 03:45:42

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1-RC5     Release:

Category:

N/A     Board:

N/A

Processor:

BF526     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Not reproducible

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2010_Apr_07

App binary format:

N/A     

Summary: traps test case 93 will make kernel panic on bf526 when stack set to L1 instruction

Details:

traps test case 85 on bf526 will make kernel panic at Stack set to L1 instruction.

Last passed version:

--

kernel:    Linux release 2.6.33.3-ADI-2010R1-pre-svn8681, build #16 Tue May 4 00:46:31 CST 2010

toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3951)

user-dist: release svn-9599, build #282 Tue May 4 00:45:49 CST 2010

--

First failed version:

--

kernel:    Linux release 2.6.33.3-ADI-2010R1-pre-svn8682, build #20 Wed May 5 04:41:41 CST 2010

toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3951)

user-dist: release svn-9599, build #361 Wed May 5 04:41:00 CST 2010

--

--

Linux version 2.6.33.4-ADI-2010R1-pre-svn8711 (test@uclinux81-bf526) (gcc version 4.3.4 (ADI-trunk/svn-3951) ) #60 Mon May 17 19:00:57 CST 2010

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart1] enabled

early printk enabled on early_BFuart1

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0013f780

  rodata    = 0x0013f780-0x001adae4

  bss       = 0x001ae000-0x001bedc0

  data      = 0x001bedc0-0x001d6000

    stack   = 0x001d4000-0x001d6000

  init      = 0x001d6000-0x00712000

  available = 0x00712000-0x03f00000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 1

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF526 Rev 0.0

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 400 MHz core clock and 80 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16002

Kernel command line: root=/dev/mtdblock0 rw ip=10.100.4.50 earlyprintk=serial,uart1,57600 console=ttyBF1,57600 ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:bf526-ezbrd:eth0:off

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 56704k/65536k RAM, (5360k init code, 1273k kernel code, 603k data, 1024k dma, 572k reserved)

Hierarchical RCU implementation.

NR_IRQS:159

Configuring Blackfin Priority Driven Interrupts

console [ttyBF1] enabled, bootconsole disabled

console [ttyBF1] enabled, bootconsole disabled

Calibrating delay loop... 796.67 BogoMIPS (lpj=1593344)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

ezbrd_init(): registering device resources

bio: create slab <bio-0> at 0

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

musb_hdrc: version 6.0, musb-dma, host, debug=0

musb_hdrc: USB Host mode controller at ffc03800 using DMA, IRQ 59

musb_hdrc musb_hdrc.0: MUSB HDRC host driver

musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

msgmni has been set to 110

io scheduler noop registered (default)

bfin-otp: initialized

bfin-uart: Blackfin serial driver

bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART

brd: module loaded

physmap platform flash device: 00400000 at 20000000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank

Intel/Sharp Extended Query Table at 0x0039

Intel/Sharp Extended Query Table at 0x0039

Intel/Sharp Extended Query Table at 0x0039

Intel/Sharp Extended Query Table at 0x0039

Intel/Sharp Extended Query Table at 0x0039

cfi_cmdset_0001: Erase suspend on write enabled

cmdlinepart partition parsing not available

RedBoot partition parsing not available

Using physmap partition information

Creating 3 MTD partitions on "physmap-flash.0":

0x000000000000-0x000000040000 : "bootloader(nor)"

0x000000040000-0x000000200000 : "linux kernel(nor)"

0x000000200000-0x000000400000 : "file system(nor)"

m25p80 spi0.1: sst25wf040 (512 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x000000000000-0x000000040000 : "bootloader(spi)"

0x000000040000-0x000000080000 : "linux kernel(spi)"

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

bfin_mii_bus: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=15)@sclk=80MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2004-05-31 14:42:52 UTC (1086014572)

dma_alloc_init: dma_page @ 0x0270f000 - 256 pages at 0x03f00000

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf526-ezbrd, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 5360k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.16.1 (2010-05-17 15:52:23 CST) hush - the humble shell

root:/>

root:/> traps_test 85

Running test 85 for exception 0x3f: Stack set to L1 instruction

... PASS (test completed 1/1 times, as expected by signal 7: Bus error)

1/1 tests passed

root:/> traps_test 85

Running test 85 for exception 0x3f: Stack set to L1 instruction

... External Memory Addressing Error

Kernel OOPS in progress

HW Error context

CURRENT PROCESS:

COMM=traps_test PID=242  CPU=0

TEXT = 0x02990040-0x029988e0        DATA = 0x02998900-0x0299bf64

BSS = 0x0299bf64-0x0299c3f0  USER-STACK = 0x0299df40

return address: [0xffa00aae]; contents of:

0xffa00a80:  0160  0161  0162  0163  0170  0173  0171  0174

0xffa00a90:  0172  0175  0166  0140  0167  31c3  0140  017c

0xffa00aa0:  017d  017e  0179  0140  017b  6000  3620 [3628]

0xffa00ab0:  3630  3638  e108  203c  e148  ffe0  e109  0efc

Looks like this was a deferred error - sorry

It might be better to look around here :

-------------------------------------------

ADSP-BF526-0.0 400(MHz CCLK) 80(MHz SCLK) (mpu off)

Linux version 2.6.33.4-ADI-2010R1-pre-svn8711 (test@uclinux81-bf526) (gcc version 4.3.4 (ADI-trunk/svn-3951) ) #60 Mon May 17 190

SEQUENCER STATUS:               Not tainted

SEQSTAT: 0000c000  IPEND: 2990f4c  IMASK: 0000  SYSCFG: 0006

  Peripheral interrupts masked off

  Kernel interrupts masked off

  EXCAUSE   : 0x0

  physical IVG2 asserted : <0xffa00d18> { _evt_nmi + 0x0 }

  physical IVG3 asserted : <0xffa006c0> { _trap + 0x0 }

  physical IVG6 asserted : <0xffa00d1c> { _evt_timer + 0x0 }

  physical IVG8 asserted : <0xffa00d94> { _evt_evt8 + 0x0 }

  physical IVG9 asserted : <0xffa00dd0> { _evt_evt9 + 0x0 }

  physical IVG10 asserted : <0xffa00e0c> { _evt_evt10 + 0x0 }

  physical IVG11 asserted : <0xffa00e48> { _evt_evt11 + 0x0 }

  logical irq   6 mapped  : <0xffa00358> { _bfin_coretmr_interrupt + 0x0 }

  logical irq  21 mapped  : <0x000dfc98> { _bfin_rtc_interrupt + 0x0 }

  logical irq  27 mapped  : <0x000e1da8> { _bfin_twi_interrupt_entry + 0x0 }

  logical irq  31 mapped  : <0x000a2ef8> { _bfin_serial_dma_rx_int + 0x0 }

  logical irq  32 mapped  : <0x000a2c6c> { _bfin_serial_dma_tx_int + 0x0 }

  logical irq  35 mapped  : <0x000c3860> { _bfin_mac_interrupt + 0x0 }

  logical irq  59 mapped  : <0x000d80b8> { _blackfin_interrupt + 0x0 }

  logical irq  62 mapped  : <0x000db4a4> { _dma_controller_irq + 0x0 }

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x0207a000> /* kernel dynamic memory (maybe user-space) */

RETX: <0x029919d8> /* kernel dynamic memory (maybe user-space) */

RETS: <0x029917f0> /* kernel dynamic memory (maybe user-space) */

PC  : <0x02990f4c> /* kernel dynamic memory (maybe user-space) */

PROCESSOR STATE:

R0 : 00000001    R1 : 00000055    R2 : 00000001    R3 : 00000100

R4 : 00000006    R5 : 00000001    R6 : 0299a6a0    R7 : 0299decc

P0 : 00000550    P1 : 02998a40    P2 : 02998a40    P3 : 00000001

P4 : 0299df44    P5 : 0299bd7c    FP : ffa10000    SP : 02079f24

LB0: 02991879    LT0: 0299186c    LC0: 00000000

LB1: 029827a5    LT1: 029827a4    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000004    I0 : 0299dc11

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 02998920

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000

USP : ffa10000  ASTAT: 02003004

-------------------------------------------

ADSP-BF526-0.0 400(MHz CCLK) 80(MHz SCLK) (mpu off)

Linux version 2.6.33.4-ADI-2010R1-pre-svn8711 (test@uclinux81-bf526) (gcc version 4.3.4 (ADI-trunk/svn-3951) ) #60 Mon May 17 190

SEQUENCER STATUS:               Not tainted

SEQSTAT: 0000c03f  IPEND: 8030  IMASK: 0000  SYSCFG: 0006

  Global Interrupts Disabled (IPEND[4])

  Peripheral interrupts masked off

  Kernel interrupts masked off

  HWERRCAUSE: 0x3

  EXCAUSE   : 0x3f

  interrupts disabled

  physical IVG5 asserted : <0xffa00c0c> { _evt_ivhw + 0x0 }

  physical IVG15 asserted : <0xffa00a54> { _schedule_and_signal + 0x0 }

  logical irq   6 mapped  : <0xffa00358> { _bfin_coretmr_interrupt + 0x0 }

  logical irq  21 mapped  : <0x000dfc98> { _bfin_rtc_interrupt + 0x0 }

  logical irq  27 mapped  : <0x000e1da8> { _bfin_twi_interrupt_entry + 0x0 }

  logical irq  31 mapped  : <0x000a2ef8> { _bfin_serial_dma_rx_int + 0x0 }

  logical irq  32 mapped  : <0x000a2c6c> { _bfin_serial_dma_tx_int + 0x0 }

  logical irq  35 mapped  : <0x000c3860> { _bfin_mac_interrupt + 0x0 }

  logical irq  59 mapped  : <0x000d80b8> { _blackfin_interrupt + 0x0 }

  logical irq  62 mapped  : <0x000db4a4> { _dma_controller_irq + 0x0 }

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x0207a000> /* kernel dynamic memory (maybe user-space) */

RETX: <0x029919d8> /* kernel dynamic memory (maybe user-space) */

RETS: <0x029917f0> /* kernel dynamic memory (maybe user-space) */

PC  : <0xffa00aae> { _schedule_and_signal + 0x5a }

PROCESSOR STATE:

R0 : 00000000    R1 : 00000055    R2 : 00000001    R3 : 00000100

R4 : 00000006    R5 : 00000001    R6 : 0299a6a0    R7 : 0299decc

P0 : 00000550    P1 : 02998a40    P2 : 02998a40    P3 : 00000001

P4 : 0299df44    P5 : 0299bd7c    FP : ffa10000    SP : 02079e48

LB0: 02991879    LT0: 0299186c    LC0: 00000000

LB1: 029827a5    LT1: 029827a4    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000004    I0 : 0299dc11

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 02998920

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000

USP : ffa10000  ASTAT: 02003004

Hardware Trace:

   0 Target : <0x00003ef8> { _trap_c + 0x0 }

     Source : <0xffa00cb6> { _evt_ivhw + 0xaa } CALL pcrel

   1 Target : <0xffa00c98> { _evt_ivhw + 0x8c }

     Source : <0xffa00c8a> { _evt_ivhw + 0x7e } IF !CC JUMP pcrel

   2 Target : <0xffa00c0c> { _evt_ivhw + 0x0 }

      FAULT : <0xffa00aac> { _schedule_and_signal + 0x58 } 0x3620

   3 Target : <0xffa00a54> { _schedule_and_signal + 0x0 }

     Source : <0xffa00d14> { _evt_ivhw + 0x108 } RTI

   4 Target : <0xffa00cc0> { _evt_ivhw + 0xb4 }

     Source : <0xffa00996> { _ret_from_exception + 0x66 } RTS

   5 Target : <0xffa00930> { _ret_from_exception + 0x0 }

     Source : <0xffa00cbc> { _evt_ivhw + 0xb0 } JUMP.L

   6 Target : <0xffa00cba> { _evt_ivhw + 0xae }

     Source : <0x00004026> { _trap_c + 0x12e } RTS

Kernel Stack

Stack info:

SP: [0x02079dec] <0x02079dec> /* kernel dynamic memory (maybe user-space) */

Memory from 0x02079de0 to 0207a000

02079de0: 00044b83  00000000  0000e4dc [00000006] 00000007  ffa10000  0000003f  ffa10000

02079e00: 00019acc  028f9918  02045b64  02079e80  00000000  00000007  02990f60  02990f4c

02079e20: 00000000  ffa00cba  0299bd7c  0299decc  0299a6a0  00000001  00000006  00000007

02079e40: 02079e80  00000013  029919d8  00008030  0000c03f  00000000  0207a000  029919d8

02079e60: ffa00aae <029917f0> 00000000  02003004  029827a5  02991879  029827a4  0299186c

02079e80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

02079ea0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

02079ec0: 00000000  00000004  00000000  00000000  02998920  0299dc11  ffa10000  ffa10000

02079ee0: 0299bd7c  0299df44  00000001  02998a40  02998a40  00000550  0299decc  0299a6a0

02079f00: 00000001  00000006  00000100  00000001  00000055  00000000  00000000  00000550

02079f20: 00000006  02990f4c  02990f4c  0000c000  00000000  0207a000  029919d8  02990f4c

02079f40:<029917f0> 00000001  02003004  029827a5  02991879  029827a4  0299186c  00000000

02079f60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

02079f80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

02079fa0: 00000004  00000000  00000000  02998920  0299dc11  ffa10000  ffa10000  0299bd7c

02079fc0: 0299df44  00000001  02998a40  02998a40  00000550  0299decc  0299a6a0  00000001

02079fe0: 00000006  00000100  00000001  00000055  00000001  00000001  00000550  00000006

Return addresses in stack:

    address : <0x029917f0> /* kernel dynamic memory (maybe user-space) */

    address : <0x029917f0> /* kernel dynamic memory (maybe user-space) */

Modules linked in:

Kernel panic - not syncing: Kernel exception

Hardware Trace:

Stack info:

SP: [0x02079d64] <0x02079d64> /* kernel dynamic memory (maybe user-space) */

Memory from 0x02079d60 to 0207a000

02079d60: 00000013 [00174748] 0013df8e  02079e48  00174748  001b34be  001b34be  001b34be

02079d80: 02079d9c  00004334  02079e48  0299df44  00000001  0299decc  02079e48  0000ffff

02079da0: ffffffff  00006334  00010a20  00030002  ffffffff  6678303c  30316166  3e303030

02079dc0: 202a2f20  6e72656b  64206c65  6d616e79  6d206369  726f6d65  00000000  0001991c

02079de0: 00044b83  00000000  0000e4dc  00000006  00000007  ffa10000  0000003f  ffa10000

02079e00: 00019acc  028f9918  02045b64  02079e80  00000000  00000007  02990f60  02990f4c

02079e20: 00000000  ffa00cba  0299bd7c  0299decc  0299a6a0  00000001  00000006  00000007

02079e40: 02079e80  00000013  029919d8  00008030  0000c03f  00000000  0207a000  029919d8

02079e60: ffa00aae <029917f0> 00000000  02003004  029827a5  02991879  029827a4  0299186c

02079e80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

02079ea0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

02079ec0: 00000000  00000004  00000000  00000000  02998920  0299dc11  ffa10000  ffa10000

02079ee0: 0299bd7c  0299df44  00000001  02998a40  02998a40  00000550  0299decc  0299a6a0

02079f00: 00000001  00000006  00000100  00000001  00000055  00000000  00000000  00000550

02079f20: 00000006  02990f4c  02990f4c  0000c000  00000000  0207a000  029919d8  02990f4c

02079f40:<029917f0> 00000001  02003004  029827a5  02991879  029827a4  0299186c  00000000

02079f60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

02079f80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

02079fa0: 00000004  00000000  00000000  02998920  0299dc11  ffa10000  ffa10000  0299bd7c

02079fc0: 0299df44  00000001  02998a40  02998a40  00000550  0299decc  0299a6a0  00000001

02079fe0: 00000006  00000100  00000001  00000055  00000001  00000001  00000550  00000006

Return addresses in stack:

    address : <0x029917f0> /* kernel dynamic memory (maybe user-space) */

    address : <0x029917f0> /* kernel dynamic memory (maybe user-space) */

--

Follow-ups

--- Vivi Li                                                  2010-06-03 03:34:34

This test failed on May, 2/4/9/17/20, and not happened all the time.

Need to recheck from time to time.

--- Vivi Li                                                  2010-06-29 05:27:58

I see this bug again with following revision. Need to recheck from time to

time.

--

kernel:    Linux release 2.6.34-ADI-2010R1-pre-svn8929, build #160 Tue Jun 22

05:54:58 CST 2010

toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3951)

user-dist: release svn-9683, build #3057 Tue Jun 22 05:54:16 CST 2010

--

--- Sonic Zhang                                              2010-07-13 02:49:10

Can't replicate on uClinux-dist svn 9723 and kernel svn 8985.

Running test 84 for exception 0x2e: Illegal use of supervisor resource -

Instruction

... PASS (test completed 1/1 times, as expected by signal 4: Illegal

instruction)

--- Vivi Li                                                  2010-07-22 03:09:42

85 test case at present is not the same one when I report this bug.

Now test 93 will make kernel panic.

--

root:/> traps_test 93

Running test 93 for exception 0x3f: Stack set to non-existant L1

... External Memory Addressing Error

Kernel OOPS in progress

HW Error context

CURRENT PROCESS:

COMM=traps_test PID=243  CPU=0

TEXT = 0x029a0040-0x029a88e0        DATA = 0x029a8900-0x029ac068

BSS = 0x029ac068-0x029ac4f0  USER-STACK = 0x029adf54

return address: [0xffa00b36]; contents of:

0xffa00b10:  0170  0173  0171  0174  0172  0175  0166  0140

0xffa00b20:  0167  31c3  0140  017c  017d  017e  0179  0140

0xffa00b30:  017b  6000  3620 [3628] 3630  3638  e108  203c

0xffa00b40:  e148  ffe0  e109  0f84  e149  ffa0  9341  0023

Looks like this was a deferred error - sorry

It might be better to look around here :

-------------------------------------------

ADSP-BF526-0.0 400(MHz CCLK) 80(MHz SCLK) (mpu off)

Linux version 2.6.34.1-ADI-2010R1-pre-svn8996 (test@uclinux81-bf526) (gcc

version 4.3.4 (ADI-trunk/svn-3951) ) #260 Thu Jul 22 00

SEQUENCER STATUS:               Not tainted

SEQSTAT: 0000c000  IPEND: 29a0f44  IMASK: 0000  SYSCFG: 0006

  Peripheral interrupts masked off

  Kernel interrupts masked off

  EXCAUSE   : 0x0

  physical IVG2 asserted : <0xffa00da0> { _evt_nmi + 0x0 }

  physical IVG6 asserted : <0xffa00da4> { _evt_timer + 0x0 }

  physical IVG8 asserted : <0xffa00e1c> { _evt_evt8 + 0x0 }

  physical IVG9 asserted : <0xffa00e58> { _evt_evt9 + 0x0 }

  physical IVG10 asserted : <0xffa00e94> { _evt_evt10 + 0x0 }

  physical IVG11 asserted : <0xffa00ed0> { _evt_evt11 + 0x0 }

  logical irq   6 mapped  : <0xffa00380> { _bfin_coretmr_interrupt + 0x0

}

  logical irq  21 mapped  : <0x000e0bb8> { _bfin_rtc_interrupt + 0x0 }

  logical irq  27 mapped  : <0x000e2cf0> { _bfin_twi_interrupt_entry +

0x0 }

  logical irq  31 mapped  : <0x000a3978> { _bfin_serial_dma_rx_int + 0x0

}

  logical irq  32 mapped  : <0x000a36ec> { _bfin_serial_dma_tx_int + 0x0

}

  logical irq  35 mapped  : <0x000c4470> { _bfin_mac_interrupt + 0x0 }

  logical irq  59 mapped  : <0x000d8d10> { _blackfin_interrupt + 0x0 }

  logical irq  62 mapped  : <0x000dc214> { _dma_controller_irq + 0x0 }

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x0298a000> /* kernel dynamic memory (maybe user-space) */

RETX: <0x029a19d0> /* kernel dynamic memory (maybe user-space) */

RETS: <0x029a17e8> /* kernel dynamic memory (maybe user-space) */

PC  : <0x029a0f44> /* kernel dynamic memory (maybe user-space) */

PROCESSOR STATE:

R0 : 00000001    R1 : 0000005d    R2 : 00000001    R3 : 00000100

R4 : 00000006    R5 : 00000001    R6 : 029aa6a0    R7 : 029adee0

P0 : 000005d0    P1 : 029a8a38    P2 : 029a8a38    P3 : 00000001

P4 : 029adf58    P5 : 029abe80    FP : ffafff00    SP : 02989f24

LB0: 029a1871    LT0: 029a1864    LC0: 00000000

LB1: 0299279d    LT1: 0299279c    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000004    I0 : 029adc25

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 029a8920

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000

USP : ffafff00  ASTAT: 02003004

(...)

--

--- Sonic Zhang                                              2010-08-17 04:02:08

Can't replicate on kernel rev. 9029 and bf526 v0.2 and v0.0.

Running test 93 for exception 0x3f: Stack set to non-existant L1

... PASS (test completed 1/1 times, as expected by signal 7: Bus error)

--- Vivi Li                                                  2011-04-29 02:28:28

I see this bug happen again on Jan and Feb in 2011 for 3 times.

--- Vivi Li                                                  2011-06-08 03:44:28

I don't see this bug for several months.

Can't replicate now. Close this bug.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

  • Share
  • History
  • More