[#6044] Fail to build kgdb in SMP kernel in trunk
Submitted By: Vivi Li
Open Date
2010-05-28 02:23:23 Close Date
2010-07-22 03:43:32
Priority:
Medium Assignee:
Sonic Zhang
Status:
Closed Fixed In Release:
2010R1
Found In Release:
2010R1 Release:
Category:
N/A Board:
EZKIT Lite
Processor:
BF561 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2010_Apr_07
App binary format:
N/A
Summary: Fail to build kgdb in SMP kernel in trunk
Details:
Fail to build kgdb in bf561-ezkit SMP kernel after kernel upgrade in latest trunk.
Last passed version:
--
kernel: Linux release 2.6.33.4-ADI-2010R1-pre-svn8727, build #130 SMP Fri May 21 08:01:19 GMT 2010
toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3815)
user-dist: release svn-9637, build #953 Fri May 21 08:00:37 GMT 2010
First failed version:
kernel: Linux release 2.6.34-ADI-2010R1-pre-svn8849, build #4 SMP Wed May 26 17:21:15 GMT 2010
toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3951)
user-dist: release svn-9645, build #20 Wed May 26 17:20:35 GMT 2010
CC kernel/fork.o
CC arch/blackfin/kernel/kgdb_test.o
CC arch/blackfin/kernel/kgdb.o
arch/blackfin/kernel/kgdb.c:403: error: ‘KGDB_THR_PROC_SWAP’ undeclared here (not in a function)
make[2]: *** [arch/blackfin/kernel/kgdb.o] Error 1
make[2]: *** Waiting for unfinished jobs....
make[1]: *** [arch/blackfin/kernel] Error 2
make[1]: *** Waiting for unfinished jobs....
Follow-ups
--- Sonic Zhang 2010-07-16 06:50:50
--- Vivi Li 2010-07-22 03:43:32
OK. Close it.
--- Vivi Li 2010-11-09 01:52:02
Sonic,
I can see that as early as Jul. 21st, this bug had already disappeared before
your fixing.
-Vivi
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.linux.kgdb_smp application/octet-stream 30075 Vivi Li