[#6051] Can not find pcmcia device in /proc/devices for cfcard test
Submitted By: Vivi Li
Open Date
2010-06-01 00:30:26 Close Date
2010-08-12 02:09:19
Priority:
Medium Assignee:
Michael Hennerich
Status:
Closed Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Category:
Drivers Board:
STAMP
Processor:
BF537 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Rejected
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2010_Apr_07
App binary format:
Summary: Can not find pcmcia device in /proc/devices for cfcard test
Details:
Can not find pcmcia device in /proc/devices for cfcard test.
Last passed version:
--
kernel: Linux release 2.6.33.4-ADI-2010R1-pre-svn8724, build #81 Thu May 20 21:27:54 CST 2010
toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3815)
user-dist: release svn-9633, build #1663 Thu May 20 21:27:09 CST 2010
First failed version:
kernel: Linux release 2.6.34-ADI-2010R1-pre-svn8738, build #85 Sat May 22 02:29:05 CST 2010
user-dist: release svn-9641, build #1749 Sat May 22 02:28:25 CST 2010
Bellow is the log:
Linux version 2.6.34-ADI-2010R1-pre-svn8738 (test@uclinux55-bf537-cf) (gcc version 4.3.4 (ADI-trunk/svn-3815) ) #87 Sat May 22 00
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart0] enabled
early printk enabled on early_BFuart0
Limiting kernel memory to 56MB due to anomaly 05000263
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x0014a530
rodata = 0x0014a530-0x001bdc68
bss = 0x001be000-0x001cf73c
data = 0x001cf73c-0x001e4000
stack = 0x001e2000-0x001e4000
init = 0x001e4000-0x00a03000
available = 0x00a03000-0x03800000
DMA Zone = 0x03f00000-0x04000000
Hardware Trace Active and Enabled
Boot Mode: 0
Reset caused by Software reset
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF537 Rev 0.2
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 500 MHz core clock and 62 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-back) in data cache
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 14224
Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 46524k/65536k RAM, (8316k init code, 1317k kernel code, 615k data, 1024k dma, 7740k reserved)
Hierarchical RCU implementation.
NR_IRQS:138
Configuring Blackfin Priority Driven Interrupts
console [ttyBF0] enabled, bootconsole disabled
Calibrating delay loop... 991.23 BogoMIPS (lpj=1982464)
Security Framework initialized
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (35 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
stamp_init(): registering device resources
bio: create slab <bio-0> at 0
SCSI subsystem initialized
Switching to clocksource bfin_cs_cycles
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
msgmni has been set to 90
io scheduler noop registered
io scheduler cfq registered (default)
bfin-uart: Blackfin serial driver
bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART
brd: module loaded
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7
bfin_mii_bus: probed
bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=11)@sclk=62MHz)
bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1
bfin_cf_pcmcia bfin_cf_pcmcia: Blackfin CompactFlash/PCMCIA Socket Driver
bfin_cf_pcmcia bfin_cf_pcmcia: : on irq 54
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
TCP cubic registered
NET: Registered protocol family 17
rtc-bfin rtc-bfin: setting system clock to 1970-01-01 05:37:11 UTC (20231)
pcmcia_socket pcmcia_socket0: pccard: PCMCIA card inserted into slot 0
pcmcia 0.0: pcmcia: registering new device pcmcia0.0
scsi0 : pata_pcmcia
ata1: PATA max PIO0 cmd 0x20310000 ctl 0x2031000e irq 54
ata1.00: CFA: TRANSCEND, 20070831, max MWDMA4
ata1.00: 15662304 sectors, multi 0: LBA
ata1.00: Drive reports diagnostics failure. This may indicate a drive
ata1.00: fault or invalid emulation. Contact drive vendor for information.
ata1.00: configured for PIO0
ata1: EH complete
scsi 0:0:0:0: Direct-Access ATA TRANSCEND 2007 PQ: 0 ANSI: 5
sd 0:0:0:0: [sda] 15662304 512-byte logical blocks: (8.01 GB/7.46 GiB)
sd 0:0:0:0: [sda] Write Protect is off
sd 0:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA
sda: sda1
sd 0:0:0:0: [sda] Attached SCSI removable disk
IP-Config: Complete:
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf537-stamp, domain=, nis-domain=(none),
bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=
dma_alloc_init: dma_page @ 0x02a74000 - 256 pages at 0x03f00000
Freeing unused kernel memory: 8316k freed
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - http://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.16.1 (2010-05-21 19:18:42 CST) hush - the humble shell
root:/> PHY: 0:01 - Link is Up - 100/Full
root:/> cardctl ident
no pcmcia driver in /proc/devices
root:/> cat /proc/devices
Character devices:
1 mem
5 /dev/tty
5 /dev/console
5 /dev/ptmx
10 misc
13 input
128 ptm
136 pts
204 ttyBF
254 rtc
Block devices:
1 ramdisk
259 blkext
8 sd
31 mtdblock
65 sd
66 sd
67 sd
68 sd
69 sd
70 sd
71 sd
128 sd
129 sd
130 sd
131 sd
132 sd
133 sd
134 sd
135 sd
root:/>
Follow-ups
--- Michael Hennerich 2010-06-15 08:39:54
This bug is caused due to the fact that CONFIG_PCMCIA_IOCTL (obsolete) is not
selected.
Read below:
config PCMCIA_IOCTL
bool "PCMCIA control ioctl (obsolete)"
depends on PCMCIA && ARM && !SMP && !PREEMPT
default y
help
If you say Y here, the deprecated ioctl interface to the PCMCIA
subsystem will be built. It is needed by the deprecated pcmcia-cs
tools (cardmgr, cardctl) to function properly.
You should use the new pcmciautils package instead (see
<file:Documentation/Changes> for location and details).
This config option will most likely be removed from kernel 2.6.35,
the associated code from kernel 2.6.36.
As the PCMCIA ioctl is not locking safe, it depends on !SMP and
!PREEMPT.
If unsure, say N.
Since this will be removed anyways - I see no point supporting it any further.
Please remove the failing test cases!
These tools are not really needed!
I tested that hot plugging PCMCIA cards still works...
root:/> pcmcia_socket pcmcia_socket0: pccard: card ejected from slot 0
hda: SanDisk SDCFH-512, CFA DISK drive
ide0 at 0x20310000-0x20310007,0x2031000e on irq 54
hda: max request size: 128KiB
hda: 1000944 sectors (512 MB) w/1KiB Cache, CHS=993/16/63
hda: hda1 hda2 hda3
ide-cs: hda: Vpp = 0.0
--- Sonic Zhang 2010-06-17 02:09:41
Michael,
The old document based on pcmcia-cs cardctl is also out of date. Could you
please update the document with new pcmica_socket tools?
--- Sonic Zhang 2010-06-17 02:10:23
http://docs.blackfin.uclinux.org/doku.php?id=linux-kernel:drivers:bfin_cf_pcmcia
--- Michael Hennerich 2010-06-17 04:25:09
Ok
Michael
--- Vivi Li 2010-08-12 02:09:19
Close this bug.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.linux.cfcard application/octet-stream 39296 Vivi Li