[#6056] Build bf538-ezkit fail at bfin_gpio.c
Submitted By: Vivi Li
Open Date
2010-06-03 00:04:11 Close Date
2010-06-03 02:12:03
Priority:
Medium Assignee:
Nobody
Status:
Closed Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Category:
N/A Board:
EZKIT Lite
Processor:
BF538 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2010_Apr_07
App binary format:
Summary: Build bf538-ezkit fail at bfin_gpio.c
Details:
Build bf538-ezkit fail at bfin_gpio.c.
First failed kernel version is 8881.
Last passed version:
--
kernel: Linux release 2.6.34-ADI-2010R1-pre-svn8869, build #125 Wed Jun 2 05:28:40 CST 2010
toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3951)
user-dist: release svn-9657, build #2457 Wed Jun 2 05:27:56 CST 2010
Bellow is the error log:
CC arch/blackfin/kernel/bfin_gpio.o
arch/blackfin/kernel/bfin_gpio.c:929:49: error: macro "unlikely" passed 2 arguments, but takes just 1
arch/blackfin/kernel/bfin_gpio.c: In function ‘bfin_special_gpio_request’:
arch/blackfin/kernel/bfin_gpio.c:929: error: ‘unlikely’ undeclared (first use in this function)
arch/blackfin/kernel/bfin_gpio.c:929: error: (Each undeclared identifier is reported only once
arch/blackfin/kernel/bfin_gpio.c:929: error: for each function it appears in.)
arch/blackfin/kernel/bfin_gpio.c:936:41: error: macro "unlikely" passed 2 arguments, but takes just 1
make[2]: *** [arch/blackfin/kernel/bfin_gpio.o] Error 1
make[1]: *** [arch/blackfin/kernel] Error 2
Follow-ups
--- Mike Frysinger 2010-06-03 00:16:58
should be fixed now
--- Vivi Li 2010-06-03 02:09:37
OK now. Close it.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found