[#6061] Fail to build kernel with nand on bf527-ezkit
Submitted By: Vivi Li
Open Date
2010-06-08 23:09:47 Close Date
2010-06-23 05:39:49
Priority:
Medium Assignee:
Barry Song
Status:
Closed Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Category:
Make Errors Board:
Processor:
BF527 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2010_Apr_07
App binary format:
Summary: Fail to build kernel with nand on bf527-ezkit
Details:
Fail to build kernel with nand on bf527-ezkit in latest trunk.
Last passed time:
--
kernel: Linux release 2.6.34-ADI-2010R1-pre-svn8869, build #149 Wed Jun 2 16:27:27 CST 2010
toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3951)
user-dist: release svn-9657, build #1908 Wed Jun 2 16:26:50 CST 2010
First failed version:
kernel: Linux release 2.6.34-ADI-2010R1-pre-svn8884, build #153 Thu Jun 3 22:44:31 CST 2010
user-dist: release svn-9660, build #1994 Thu Jun 3 22:43:54 CST 2010
Bellow is the log:
CHK include/linux/version.h^M
CHK include/generated/utsrelease.h^M
CALL scripts/checksyscalls.sh^M
CHK include/generated/compile.h^M
GEN usr/initramfs_data.cpio^M
AS usr/initramfs_data.o^M
LD usr/built-in.o^M
CC arch/blackfin/mach-common/ints-priority.o^M
CC arch/blackfin/mach-bf527/boards/ezkit.o^M
GZIP kernel/config_data.gz^M
IKCFG kernel/config_data.h^M
CC kernel/configs.o^M
arch/blackfin/mach-bf527/boards/ezkit.c:237: error: unknown field ‘page_size’ specified in initializer^M
arch/blackfin/mach-bf527/boards/ezkit.c:237: error: ‘NFC_PG_SIZE_256’ undeclared here (not in a function)^M
make[2]: *** [arch/blackfin/mach-bf527/boards/ezkit.o] Error 1^M
make[1]: *** [arch/blackfin/mach-bf527/boards] Error 2^M
make[1]: *** Waiting for unfinished jobs....^M
Follow-ups
--- Barry Song 2010-06-10 02:14:56
lost updates for some board files for:
task [#6046]: delete wrong page_size field from bfin nand platform_data
page size is detected by matching id automatically, and ecc size/byte are
decided by page size.
The origin codes misunderstood the meaning of page size.
--- Vivi Li 2010-06-23 05:37:03
OK now.
Close it.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.config.nand application/octet-stream 48680 Vivi Li
config.linux.nand application/octet-stream 44258 Vivi Li