Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers
    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers

    Introduction to Industrial I/O, libIIO, and Python software tools

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Evaluating Power Supplies with Different Compensation Settings

    Evaluating Power Supplies with Different Compensation Settings

EngineerZone
EngineerZone
Linux Bug Archive
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Linux Bug Archive
  • Processors & DSP
  • Software & Development Tools
  • Linux Distribution for Blackfin
  • Linux Bug Archive
  • Cancel
Linux Bug Archive
Documents [#6074] Build bf526 kernel with nand support fail(2010)
  • Q&A
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +ad1836: FAQ
  • +ad1938: FAQ
  • +ad1939: FAQ
  • +AD5280: FAQ
  • +ad73311: FAQ
  • +adau1361: FAQ
  • +adau1371: FAQ
  • +adau1373: FAQ
  • +adau1761: FAQ
  • +adp5588-gpio: FAQ
  • +adv7393: FAQ
  • +ADXL34x: FAQ
  • +bf518-ezbrd: FAQ
  • +bf518: FAQ
  • +bf51x: FAQ
  • -bf526-ezbrd: FAQ
    • [#5944] Disable anomaly 456 for bf526-ezbrd, gadget fs bulk test fails in dma mode (2010)
    • [#5945] Gadget ethernet fails to work in dma mode when anomaly 456 is disabled on bf526-ezbrd(2010)
    • [#5946] Disable anomaly 456 on bf526-ezbrd, gadget serial in dma mode fails to work(2010)
    • [#5947] Disable anomaly 456 on bf526-0.2-ezbrd, host can't find gadget ram storage in dma mode(2010)
    • [#6033] traps test case 93 will make kernel panic on bf526 when stack set to L1 instruction(2010)
    • [#6074] Build bf526 kernel with nand support fail(2010)
  • +bf527-ezkit: FAQ
  • +bf533-stamp/ezkit: FAQ
  • +bf533: FAQ
  • +bf538-ezkit: FAQ
  • +bf548-ezkit: FAQ
  • +BF54x: FAQ
  • +bf561-ezkit: FAQ
  • +bf5xx: FAQ
  • +bfin-mac driver: FAQ
  • +bfin-uclinux-gdb: FAQ
  • +bfin_can.c: FAQ
  • +Blackfin: FAQ
  • +bluetooth: FAQ
  • +Build kernel: FAQ
  • +Build: FAQ
  • +cfcard test: FAQ
  • [#6170] section mismatches in cifs code(2010)
  • [#6173] linphone testing problem(2010)
  • [#6190] BF561-EZKIT SMP kernel can not wake up by uart(2010)
  • [#6194] libxenomai.so.0 can't be found in xenomai kernel with fdpic mode(2010)
  • [#6207] Build error in CTS/RTS testing on board BF548-EZKIT(2010)
  • [#6251] pread/pwrite arent decoded correctly by strace(2010)
  • [#6253] strace build failed in trunk with outdated toolchain (missing asm/cachectl.h)(2010)
  • [#6255] Busybox inetd crashes/rsh noconnet/ssh(2010)
  • [#6265] libpng build fails due to not finding zlib(2010)
  • [#6271] "nand unlock" is an unsupported command in u-boot update in nand flash(2010)
  • [#6272] After update u-boot in spi flash, BF548-EZKIT can not boot from spi flash(2010)
  • +gadget fs bulk: FAQ
  • +gadget zero bulk: FAQ
  • +gadget zero control: FAQ
  • +Kernel xip: FAQ
  • +ltp test: FAQ
  • +microwin test: FAQ
  • +MPU kernel: FAQ
  • +Sl811-hcd.c USB: FAQ
  • +SPORT channel: FAQ
  • +trunk head kernel: FAQ
  • +usb otg driver: FAQ
  • +zlib: FAQ
  • +Illegal i2c: FAQ
  • +isp1362-hcd: FAQ
  • +Kernel: FAQ
  • +KGDBOE: FAQ
  • [#4646] Varittronix LCD driver mixes blue and Red
  • +serial driver: FAQ
  • +sigma firmware: FAQ
  • +spi transaction: FAQ
  • +strace FAQ
  • [#4787] [ltp] LTP test case shmctl01 failed in trunk for ltp-full-20081130
  • +tiff-4.0.0beta4: FAQ
  • [#5264] ping packet size test will fail for gadget ethernet test with DMA mode
  • +USBHOST: FAQ
  • +USB_EP_NI7_RXINTERVAL: FAQ
  • [#5257] Build usb gadget driver with DMA mode will fail
  • [#4708] Blackfin irda build fails for bf533-stamp
  • [#4735] unaligned accesses in qt webkit
  • [#5168] build cpufrequtils into fdpic format has error
  • [#5321] modprobe i2c lcd on bf533 stamp wait long time
  • [#4922] unwanted sound comes up after g_audio module is installed on BF548 and BF527
  • [#5176] app cpufrequtils in Blackfin app programs fails to build in FDPIC
  • [#5237] musb driver is broken after linux-2.6.30 update
  • [#5255] ping target board sometimes get wrong data byte for gadget ethernet pio mode
  • [#5336] canbus and ppifcd drivers can not be built on BF538-EZKIT
  • [#6614] Kernel panic frequently when test sdio mmc on bf518-ezbrd(2011)
  • +SPI driver: FAQ
  • [#4714] the first time to build mtd-utils will fail in trunk
  • [#5524] drivers/video/bfin_adv7393fb.c build fails in 2.6.31 due to old i2c usage
  • [#5525] drivers/video/bf537-lq035.c build fails in 2.6.31 due to old i2c usage
  • [#5399] no sound when record in board and listen in PC for linphone test of ad1836 on bf533-stamp
  • [#5458] Drivers Serial:bfin_5xx:ttyBFx fails to generate resume from standby
  • [#4647] build samba fails on trunk now for redefinition in fcntl.h
  • [#5526] ip0x board has broken UART defines after resource reorganization
  • [#5527] drivers/media/video/blackfin/blackfin_cam.c build fails in 2.6.31 due to old i2c usage
  • [#5352] bfin_sport.c setup 2D DMA
  • [#5528] fs/binfmt_elf_fdpic.c build fails when CONFIG_ELF_CORE is enabled in 2.6.31
  • [#5464] isram_write() seems to be busted
  • [#5376] mmap05 sometimes can not pass when MPU
  • [#5534] run aplay/arecord will make system panic after kernel upgraded to 2.6.31
  • [#5361] Microwin (nanox) failed on trunk using AD7897 touch screen
  • [#5544] Sport uart TX stop waiting loop is too long to block RX interrupt in PIO mode when do duplex communication
  • [#5363] spi mmc is not supported in bf533-stamp
  • [#5550] fail to flash ubifs.img to nand
  • [#5470] build xenomai fails for no switchbench
  • [#5437] mathtest fails to compile
  • [#5551] SPI message lost when bus locked
  • [#5370] alsa tool fails to work after wake up from mem in bf537-stamp with ad1836 (can't resolve symbol)
  • [#5561] [ltp ]Kernel dump info when run ltp test cases access02, chown03, fchmod06, fchown03, fchown04
  • [#5377] amixer fail to run on ad1836 audio driver on BF537-STAMP
  • [#5475] build mkfs.ubifs on trunk head fails
  • [#5562] [ltp]some ltp test case is broken for getipckey and getcwd
  • [#5487] build usb.c fail in testsuites/usbdev/ test at asm/swab.h
  • [#5489] t2/t4 failed in gadget zero bulk test with dma mode
  • [#5567] build nand for bf537 fails on trunk
  • [#5494] Run tftlcd test case in bf548-ezkit, kernel crashed at the end
  • [#4879] traps test case 21 exception 0x3f: l1_instruction_access would make kernel panic on bf533 stamp
  • [#5568] Framebuffer DMA Error!!
  • [#5515] 4 more trap cases fails on bf533
  • [#5379] run scratchpad case sometimes would fail
  • [#5519] pushing Blackfin serial resources to boards broke many boards
  • [#5389] build pictureflow fails at branch head
  • [#5531] Usb SL811 failed on uclinux2009r1-rc6 on bf532 board.
  • [#5523] Blackfin MUSB build fails after update to 2.6.31
  • [#5391] For ad1836 and ad1981b, sometimes sound shakes at the end
  • [#5404] build kernel with 0x2000 as BOOT_LOAD address sometimes would fails at build-busybox-1.13.4
  • [#5469] CPU hardly idles anymore in svn trunk
  • [#5695] Build bf537-stamp fails at ad73322 for the latest trunk
  • [#5702] build xenomai into fdpic format fails for no libnative.so
  • [#5427] ircp failed on bf533-stamp
  • [#5708] Kernel can not boot up when spimmc driver is interrupt drivern in PIO mode
  • [#5711] gfortran case default_format_1.exe fails on 09r1 kernel but pass on trunk head
  • [#5712] I2C client drivers using dev_pm_ops fail to receive suspend/resume callbacks
  • [#5715] libpcap fails to compile in trunk
  • [#5589] STLport build fails
  • [#5724] SPORT driver crash on reload
  • [#5449] bfin_sdh doesn't save and restore peripheral context upon resume
  • [#5580] GPIO pin not reserved for CTS function on SPORT-UART driver
  • [#5521] trunk head build fails at ipc/shm.c
  • [#5636] generic gpio works on bf533 in the opposite way
  • [#5637] Kernel crashed when arecord and aplay on bf537-stamp with SoC I2S audio
  • [#5647] SPI driver bus_unlock() does not schedule postponed SPI messages
  • [#5683] build nand fails for format error
  • [#5689] while two or multi spi devices use gpio cs, spi setup will fail
  • [#5558] bfin mac multi-cast sending fails to work
  • [#5816] PREEMPT_RT: cyclic test stalls in some test mode
  • [#5824] some kernel modules fail to link due to losing strcpy in trunk head
  • [#5707] error in user/procps/Makefile
  • [#5841] [ltp] ltp test case shmctl01/semctl01 can not execute
  • [#5605] Build bf537-stamp fail at bf5xx-i2s.c in latest trunk
  • [#5614] With latest toolchain in trunk, fail to build some apps and libs at fork
  • [#5625] Build microwin app fails in trunk with 4.3 toolchain
  • [#5626] Build lib mad fail at option "-fforce-mem" with gcc 4.3
  • [#5722] bfin_sport_spi broken by cs_gpio changes
  • [#5627] fail to control gpio used by led and button through /sys/class/gpio/
  • [#5927] PR bit other than RAF bit in EMAC OPMODE register should be set for promisuous mode in bfin_mac driver
  • [#5727] build e2fsprogs-1.41.12 fail sometimes because of compiling order
  • [#5631] Build lib confuse failed with gcc 4.3 toolchain
  • [#5759] fix build for pwlib
  • [#5651] Build lirc failed at missing files
  • [#5931] Trying to compile CAN4LINUX for BF537-STAMP board but compilation is failing
  • [#5656] Build iproute2 fails at trunk for dlfcn.h when built as FLAT
  • [#5743] sound/soc/blackfin/bf5xx-ad1938.c build fails after 2.6.32 upgrade
  • [#5801] No interrupt occurs when reconnect gadget device in OTG mode.
  • [#5657] [ltp] ltp test case mount03/umount03 fail with error of "No such device"
  • [#5808] mmc configuration error in make config
  • [#5804] bf531: ethernet not working when switching to 2009R1
  • [#5810] initial sp is given wrong value and INIT_TASK_DATA is not linked into data
  • [#6335] Build xip failed in fdpic format when xenomai is enabled
  • [#7224] undifined variable x25_address in ./user/net-tools/lib/x25_src.c
  • [#5598] bluez-utils has parallel build issues with parser.h
  • [#5668] Fail to build app bluez-utils
  • [#7251] Blackfin SPI driver doesn't handle repeated changes in CPOL, CPHA and LSBF correctly
  • [#5767] In 09r1.1 branch, all ltp test cases show stack overflow in bf561 SMP kernel
  • [#5684] touching keypad on bf548 will make system dead and restart
  • [#7287] Can not build usb.c with libaio
  • [#5687] SPI read/write be wrong after suspend to memory and resume
  • [#7315] [ltp] ltp test case getrusage04 from ltp-full-20120903 fails in trunk
  • [#7328] Fail to compile pthread_test after toolchain update
  • [#5876] Repeating rsh/rcp causes error "poll: protocol failure in circuit setup"
  • [#7329] Fail to compile netperf after toolchain update
  • [#7333] Test dll fails to run after toolchain update
  • [#5741] adau1371 and adau1761 fail to build after 2.6.32 upgrade
  • [#7337] [ltp] ltp test case mount02 fails in ltp-full-20120903
  • [#7338] [ltp] ltp test case mount03 fails in ltp-full-20120903
  • [#5821] Fail to build pngview on regression machines with suse 10.2
  • [#5900] hardware single stepping in userspace does not handle syscalls correctly
  • [#5659] [ltp] ltp test case eventfd01 fail
  • [#7339] [ltp] can not apply patch of lchown02 in ltp-full-20101031 to ltp-full-20120903
  • [#7343] [ltp] LTP test case chdir04 fails in ltp-full-20120903
  • [#7396] build netperf fails for undefined reference to `___CPU_ZERO'
  • [#7483] bfin_sport driver does not work well in TDM DMA mode
  • [#7506] Dropbear does not build
  • [#5757] drop USER_SQUASHFS_MKSQUASHFS7Z as squashfs 4.0 does not support 7z anymore
  • [#5758] fix build for libopenh323
  • [#5833] trap test running on the second core of bf561 has serveral fails
  • [#5755] romfs target fails for lib/pwlib
  • [#5760] fix asterisk build
  • [#5756] romfs target fails for lib/libopenh323
  • [#5877] SPI transmit cs_change flag not properly handled
  • [#5939] bfin-can fails to build after linux-2.6.33 upgrade
  • [#5879] GPIO controlled slave request may fail when bfin_spi_setup() gets executed twice
  • [#5774] [ltp]ltp test case will be killed by oom-killer on bf533-ezkit in 09r1 branch occasionally
  • [#5894] BF527 uImage Flashing issue(Copy to Flash... Flash not Erased)
  • [#5941] links fails in trunk due to using fork()
  • [#5942] build usb host fail when remove anomaly 456 for BF526-EZBRD
  • [#7250] On bfin ppi test, it fails to quit from slave when send "q" from master
  • [#7379] Fail to build alsa lib in latest trunk with upgraded toolchain
  • [#5792] enc28j60 spi net fails to ping with host on trunk head kernel
  • [#4436] BF527-EZKIT unable to receive large files over UART in DMA mode
  • [#4764] Kernel prints warning when booting from jffs2 rootfs in nor flash on bf548-ezkit
  • [#5903] Impossible to work properly with two or more SPI slave devices using spi_bfin5xx driver.
  • [#6386] build iproute2 may fail at ifstat.c sometimes in latest trunk(2010)
  • [#6331] There is error in adau1371 audio testing on bf527-ezkit(2010)
  • [#5933] BF561-EZKIT SMP kernel can not wake up from standby mode by uart interrupt
  • [#4713] dmacopy tries to test L2 on BF537
  • [#6564] dmacopy test on bf561-ezkit failed at sram_alloc in L1(2011)
  • [#4997] ppitest fails for bfin_ppi driver on bf537
  • [#5940] lynx fails in trunk due to using fork()
  • [#4104] Format usbdisk failed with mke2fs in trunk
  • [#6578] iccutils build fails at scalar.c(2011)
  • [#3883] ftp server crash after connetion or chdir with MidnightCommander4.6.1
  • [#4697] kernel crash on bf533-stamp/bf533-ezkit after config IP for ethernet port
  • [#4050] xip test case failed in BF548-EZKIT
  • [#3991] mmc_spi not working out of the box.
  • [#3996] dhcpcd not stable on BF548-EZKIT
  • [#5136] Linphone: Can't hear each other and "Data access misaligned address violation"
  • [#5214] trunk applications don't build with trunk toolchain due to missing fork()
  • [#4055] top (busybox) crashs
  • [#5162] Linphone: Data access misaligned address
  • [#4992] bfin_sdh fails to build for BF514/BF516
  • [#5570] reboot on bf527-ezkit with nand and ubifs enabled fails
  • [#4955] 548 SDH: netperf, iperf triggers libertas error
  • [#5522] Lib DirectFB-1.4.0 crashes when run DirectFB demo on SVN trunk
  • [#3882] copy file function cp, after few times consume all memory
  • [#4773] BF527 usb-ide hard disk error

[#6074] Build bf526 kernel with nand support fail(2010)

[#6074] Build bf526 kernel with nand support fail

Submitted By: Vivi Li

Open Date

2010-06-23 05:29:28     Close Date

2010-06-29 04:48:36

Priority:

Medium     Assignee:

Barry Song

Status:

Closed     Fixed In Release:

2010R1

Found In Release:

2010R1     Release:

Category:

N/A     Board:

N/A

Processor:

BF526     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2010_Apr_07

App binary format:

N/A     

Summary: Build bf526 kernel with nand support fail

Details:

Build bf526 kernel with nand support fail.

bf527-ezkit is OK.

Last passed version:

--

kernel:    Linux release 2.6.34-ADI-2010R1-pre-svn8869, build #108 Thu Jun 3 00:22:20 CST 2010

toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3951)

user-dist: release svn-9657, build #2038 Thu Jun 3 00:21:39 CST 2010

--

First failed version:

--

kernel:    Linux release 2.6.34-ADI-2010R1-pre-svn8886, build #112 Fri Jun 4 08:07:11 CST 2010

toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3951)

user-dist: release svn-9662, build #2115 Fri Jun 4 08:06:30 CST 2010

--

Bellow is the log:

--

  CHK     include/linux/version.h^M

  CHK     include/generated/utsrelease.h^M

  CALL    scripts/checksyscalls.sh^M

  CHK     include/generated/compile.h^M

  GEN     usr/initramfs_data.cpio^M

  AS      usr/initramfs_data.o^M

  LD      usr/built-in.o^M

  CC      arch/blackfin/mach-common/ints-priority.o^M

  LD      arch/blackfin/mach-common/built-in.o^M

  CC      arch/blackfin/mach-bf527/boards/ezbrd.o^M

arch/blackfin/mach-bf527/boards/ezbrd.c:152: error: unknown field ‘page_size’ specified in initializer^M

arch/blackfin/mach-bf527/boards/ezbrd.c:152: error: ‘NFC_PG_SIZE_256’ undeclared here (not in a function)^M

make[2]: *** [arch/blackfin/mach-bf527/boards/ezbrd.o] Error 1^M

make[1]: *** [arch/blackfin/mach-bf527/boards] Error 2^M

make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x'^M

make: *** [linux] Error 1^M

--

Follow-ups

--- Barry Song                                               2010-06-23 05:40:57

Fixed.

forget to delete page size in bf526 board.

-barry

--- Vivi Li                                                  2010-06-29 04:45:45

OK now. Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.linux.nand    application/octet-stream    42994    Vivi Li

Attachments:
2664.config.linux.nand.zip
  • Share
  • History
  • More