[#6106] adp5588-gpio sometimes fails as a module
Submitted By: Mike Frysinger
Open Date
2010-07-11 14:15:09 Close Date
2010-08-30 08:01:24
Priority:
Medium Assignee:
Michael Hennerich
Status:
Closed Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Category:
N/A Board:
N/A
Processor:
ALL Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
trunk
App binary format:
N/A
Summary: adp5588-gpio sometimes fails as a module
Details:
with the attached .config created via randconfig, the build fails:
ERROR: "set_irq_noprobe" [drivers/gpio/adp5588-gpio.ko] undefined!
ERROR: "set_irq_chip_and_handler" [drivers/gpio/adp5588-gpio.ko] undefined!
ERROR: "irq_to_desc" [drivers/gpio/adp5588-gpio.ko] undefined!
make[1]: *** [__modpost] Error 1
Follow-ups
--- Michael Hennerich 2010-07-12 05:13:49
These errors are caused by the generic kernel irq core not exporting them.
Two options:
Change the generic code to export them - or prevent the driver being build as a
module.
--- Michael Hennerich 2010-08-03 07:59:47
Do it like others: Exclude irq_chip functionality in case driver is built as
module.
http://lkml.org/lkml/2010/7/15/117
Fixed on trunk
--- Michael Hennerich 2010-08-30 08:01:24
close it
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
randconfig-8.config application/octet-stream 51209 Mike Frysinger