[#6168] kernel autoboot when i input "hciconfig hci0 up" in bluetooth cf testing
Submitted By: angelia wu
Open Date
2010-08-09 02:27:49 Close Date
2010-08-18 22:46:13
Priority:
Medium Assignee:
steven miao
Status:
Closed Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Blackfin Linux:2010R1
Category:
N/A Board:
STAMP
Processor:
BF537 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Duplicate
Uboot version or rev.:
Toolchain version or rev.:
svn-4681
App binary format:
N/A
Summary: kernel autoboot when i input "hciconfig hci0 up" in bluetooth cf testing
Details:
kernel autoboot when i input "hciconfig hci0 up" in bluetooth cf testing.it will show the following message.
U-Boot 2010.06-svn2366 (ADI-2010R1-pre) (Jul 27 2010 - 21:47:44)
CPU: ADSP bf537-0.2 (Detected Rev: 0.2) (bypass boot)
Board: ADI BF537 stamp board
Support: http://blackfin.uclinux.org/
Clock: VCO: 500 MHz, Core: 500 MHz, System: 125 MHz
RAM: 64 MiB
Flash: 4 MiB
In: serial
Out: serial
Err: serial
KGDB: [on serial] ready
Net: bfin_mac
Hit any key to stop autoboot: 0
Besides,it can't autoboot successfully.only drag power line out ,it can autoboot successfully.
Follow-ups
--- steven miao 2010-08-18 21:39:22
We should drop the test case as well.
The reason is same as bug 6166.
--- Vivi Li 2010-08-18 22:46:13
OK, this test is deleted from test list.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config-config-blcf application/octet-stream 49129 angelia wu
kernel-config-blcf application/octet-stream 36941 angelia wu