[#6176] error happend when test tftlcd
Submitted By: angelia wu
Open Date
2010-08-12 04:23:46 Close Date
2010-08-23 01:36:15
Priority:
Medium Assignee:
Sonic Zhang
Status:
Closed Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Blackfin Linux:2010R1
Category:
N/A Board:
STAMP
Processor:
BF537 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
svn-4681
App binary format:
Summary: error happend when test tftlcd
Details:
when modprobe bf537-lq035 module,some error happend as following.but the show of tftlcd testing is right.
root:/> modprobe bf537-lq035
i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400
bf537-lq035-ad5280 0-002c: write fail: -1
bf537-lq035-ad5280: probe of 0-002c failed with error -1
root:/> video_test
Hit any key to stop autoboot: 0
Using bfin_mac device
TFTP from server 10.100.4.174; our IP address is 10.100.4.50
Filename 'uImage'.
Load address: 0x1000000
Loading: #################################################################
#################################################################
###################################################
done
Bytes transferred = 4562396 (459ddc hex)
## Booting kernel from Legacy Image at 01000000 ...
Image Name: bf537-2.6.34.2-ADI-2010R1-pre-sv
Created: 2010-08-05 1:07:17 UTC
Image Type: Blackfin Linux Kernel Image (gzip compressed)
Data Size: 4562332 Bytes = 4.4 MiB
Load Address: 00001000
Entry Point: 001a568c
Verifying Checksum ... OK
Uncompressing Kernel Image ... OK
Starting Kernel at = 001a568c
Linux version 2.6.34.2-ADI-2010R1-pre-svn9041 (test@uclinux71-digiumPBX) (gcc version 4.3.4 (ADI-trunk/svn-3951) ) #227 Thu Aug 5 09:07:03 CST 2010
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart0] enabled
early printk enabled on early_BFuart0
Limiting kernel memory to 56MB due to anomaly 05000263
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x00118058
rodata = 0x00118058-0x00176ad8
bss = 0x00177000-0x001875e0
data = 0x001875e0-0x0019a000
stack = 0x00198000-0x0019a000
init = 0x0019a000-0x00881000
available = 0x00881000-0x03800000
DMA Zone = 0x03f00000-0x04000000
Hardware Trace Active and Enabled
Boot Mode: 0
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF537 Rev 0.2
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 500 MHz core clock and 125 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-back) in data cache
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 14224
Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50:10.100.4.174:10.100.4.174:2f
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 48068k/65536k RAM, (7068k init code, 1116k kernel code, 520k data, 1024k dma, 7740k reserved)
Hierarchical RCU implementation.
NR_IRQS:138
Configuring Blackfin Priority Driven Interrupts
console [ttyBF0] enabled, bootconsole disabled
Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)
Security Framework initialized
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (35 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
stamp_init(): registering device resources
bio: create slab <bio-0> at 0
Switching to clocksource bfin_cs_cycles
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
msgmni has been set to 93
io scheduler noop registered
io scheduler cfq registered (default)
bfin-uart: Blackfin serial driver
bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART
brd: module loaded
bfin_mii_bus: probed
bfin_mii_bus: Can't get IRQ 65535 (PHY)
bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)
bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
TCP cubic registered
NET: Registered protocol family 17
IP-Config: Complete:tting system clock to 1970-01-04 07:31:33 UTC (286293)
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf537-stamp, domain=, nis-domain=(none),
bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=
dma_alloc_init: dma_page @ 0x028e1000 - 256 pages at 0x03f00000
Freeing unused kernel memory: 7068k freed
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - http://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.16.2 (2010-08-05 08:02:50 CST) hush - the humble shell
root:/> PHY: 0:01 - Link is Up - 100/Full
root:/> lsmod
Module Size Used by
^C
Follow-ups
--- Sonic Zhang 2010-08-18 05:18:30
Fixed. The predefined i2c address 0x2c doesn't match the configuration of ad5280
PINs AD0 and AD1 on the tftlcd addon board. Both AD0 and AD1 are of voltage
3.3V, which means the i2c address should be 0x2F.
--- angelia wu 2010-08-23 01:36:15
i test this case again and it indeed fixed, so i closed the bug.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.tftlcd.portrait application/octet-stream 37623 angelia wu