[#6201] can't regonize lcd device in i2c lcd driver testing over twi on bf548-ezkit
Submitted By: angelia wu
Open Date
2010-08-23 07:12:06 Close Date
2010-08-30 01:45:51
Priority:
Medium Assignee:
steven miao
Status:
Closed Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Blackfin Linux:2010R1
Category:
N/A Board:
EZKIT Lite
Processor:
BF548 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
svn-4681
App binary format:
Summary: can't regonize lcd device in i2c lcd driver testing over twi on bf548-ezkit
Details:
can't regonize lcd device in i2c lcd driver testing over twi on bf548-ezkit.
when 'ls' in the folder 'sys/bus/i2c/devices' ,it should show a folder "0022.*(\[0-9]-002f)",but it hasn't. so the lcd can't show anything.the bus is the same as bug 6197.
so i guess the other board bf537-stamp,bf527-ezkit may also have the bug. so i will the case later.
the test steps as follow.
Hit any key to stop autoboot: 0
smc911x: initializing
smc911x: detected LAN9218 controller
smc911x: phy initialized
smc911x: MAC 00:e0:22:fe:bd:b8
Using smc911x-0 device
TFTP from server 10.100.4.174; our IP address is 10.100.4.50
Filename 'uImage'.
Load address: 0x1000000
Loading: #################################################################
#################################################################
##############################################
done
Bytes transferred = 5437125 (52f6c5 hex)
## Booting kernel from Legacy Image at 01000000 ...
Image Name: bf548-2.6.34.5-ADI-2010R1-pre-sv
Created: 2010-08-23 10:56:13 UTC
Image Type: Blackfin Linux Kernel Image (gzip compressed)
Data Size: 5437061 Bytes = 5.2 MB
Load Address: 00001000
Entry Point: 002a28b4
Verifying Checksum ... OK
Uncompressing Kernel Image ... OK
Starting Kernel at = 002a28b4
Linux version 2.6.34.5-ADI-2010R1-pre-svn9094 (test@uclinux41) (gcc version 4.3.5 (ADI-trunk/svn-4681) ) #94 Mon Aug 23 18:56:06 CST 2010
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart1] enabled
early printk enabled on early_BFuart1
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x001b96c8
rodata = 0x001b96c8-0x002579d8
bss = 0x00258000-0x0026f99c
data = 0x0026f99c-0x00290000
stack = 0x0028e000-0x00290000
init = 0x00290000-0x00a1a000
available = 0x00a1a000-0x03e00000
DMA Zone = 0x03e00000-0x04000000
Hardware Trace Active and Enabled
Boot Mode: 1
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF548 Rev 0.2
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 525 MHz core clock and 131 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
L2 SRAM : uncacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-through) in data cache
L2 SRAM : uncacheable in data cache
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 15748
Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart1,57600 console=ttyBF1,57600 ip=10.100.4.50:10.100.4.174:10.100.4.174:f
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 52576k/65536k RAM, (7720k init code, 1761k kernel code, 859k data, 2048k dma, 572k reserved)
Hierarchical RCU implementation.
NR_IRQS:295
Configuring Blackfin Priority Driven Interrupts
Console: colour dummy device 80x25
console [ttyBF1] enabled, bootconsole disabled
Calibrating delay loop... 1046.52 BogoMIPS (lpj=2093056)
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (42 KB free)
Blackfin L2 SRAM: 128 KB (128 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
ezkit_init(): registering device resources
bio: create slab <bio-0> at 0
SCSI subsystem initialized
spi spi0.2: Warning: SPI CPHA not set: Slave Select not under software control!
See Documentation/blackfin/bfin-spi-notes.txt
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@4
bfin-spi bfin-spi.1: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc02300, dma channel@5
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc00700
i2c-bfin-twi i2c-bfin-twi.1: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc02200
Advanced Linux Sound Architecture Driver Version 1.0.22.1.
musb_hdrc: version 6.0, musb-dma, host, debug=0
musb_hdrc musb_hdrc.0: MUSB HDRC host driver
musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb_hdrc musb_hdrc.0: USB Host mode controller at ffc03c00 using DMA, IRQ 82
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
Slow work thread pool: Starting up
Slow work thread pool: Ready
msgmni has been set to 102
io scheduler noop registered (default)
bf54x-lq043: FrameBuffer initializing...
dma_alloc_init: dma_page @ 0x029e4000 - 512 pages at 0x03e00000
Console: switching to colour frame buffer device 80x24
bfin-otp: initialized
bfin-uart: Blackfin serial driver
bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 48) is a BFIN-UART
brd: module loaded
register bfin atapi driver
scsi0 : pata-bf54x
ata1: PATA max UDMA/66 irq 68
physmap platform flash device: 02000000 at 20000000
physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank
Intel/Sharp Extended Query Table at 0x010A
Using buffer write method
Using auto-unlock on power-up/resume
cfi_cmdset_0001: Erase suspend on write enabled
RedBoot partition parsing not available
Using physmap partition information
Creating 3 MTD partitions on "physmap-flash.0":
0x000000000000-0x000000040000 : "bootloader(nor)"
0x000000040000-0x000000440000 : "linux kernel(nor)"
0x000000440000-0x000001000000 : "file system(nor)"
m25p80 spi0.1: m25p16 (2048 Kbytes)
Creating 2 MTD partitions on "m25p80":
0x000000000000-0x000000040000 : "bootloader(spi)"
0x000000040000-0x000000200000 : "linux kernel(spi)"
BF5xx on-chip NAND FLash Controller Driver, Version 1.2 (c) 2007 Analog Devices, Inc.
bf5xx-nand bf5xx-nand.0: data_width=8, wr_dly=3, rd_dly=3
NAND device: Manufacturer ID: 0x20, Chip ID: 0xda (ST Micro NAND 256MiB 3,3V 8-bit)
Creating 2 MTD partitions on "NAND 256MiB 3,3V 8-bit":
0x000000000000-0x000000400000 : "linux kernel(nand)"
0x000000400000-0x000010000000 : "file system(nand)"
smsc911x: Driver version 2008-10-21.
smsc911x-mdio: probed
ata1.00: ATA-7: FUJITSU MHW2040AT, 0000000B, max UDMA/100
ata1.00: 78140160 sectors, multi 16: LBA
eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1)
net eth0: MAC Address: 00:e0:22:fe:bd:b8
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
ata1.00: configured for UDMA/66
blk_queue_max_segments: set to minimum 1
scsi 0:0:0:0: Direct-Access ATA FUJITSU MHW2040A 0000 PQ: 0 ANSI: 5
input: bf54x-keys as /devices/platform/bf54x-keys/input/input0
sd 0:0:0:0: [sda] 78140160 512-byte logical blocks: (40.0 GB/37.2 GiB)
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
i2c /dev entries driver
sd 0:0:0:0: [sda] Write Protect is off
sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
sda:
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
dma rx:0 tx:1, err irq:10, regs:ffc00800
AD1980 SoC Audio Codec
asoc: AC97 <-> bf5xx-ac97 mapping ok
ALSA device list:
#0: bf5xx-board (AD1980)
TCP cubic registered
NET: Registered protocol family 17
rtc-bfin rtc-bfin: setting system clock to 1970-01-07 19:41:21 UTC (589281)
sda1 sda2
sd 0:0:0:0: [sda] Attached SCSI disk
net eth0: SMSC911x/921x identified at 0x24000000, IRQ: 175
IP-Config: Complete:
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf548-ezkit, domain=, nis-domain=(none),
bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=
Freeing unused kernel memory: 7720k freed
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - http://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.16.2 (2010-08-23 17:51:15 CST) hush - the humble shell
root:/> modprobe bfin_twi_lcd
bfin_twi_lcd: loaded
root:/> lsmod
Module Size Used by
bfin_twi_lcd 2553 0
root:/> cd sys/bus/i2c/devices
root:/sys/bus/i2c/devices> ls
0-0022 0-002b i2c-0
Follow-ups
--- steven miao 2010-08-26 05:06:18
same as 6197
--- angelia wu 2010-08-30 01:45:51
i test it again according wiki and now the bug is disappear.
so i closed the bug 6201.
Thank you steven miao.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
kernel.548twi_lcd.config application/x-config 49923 angelia wu
user.548twi_lcd.config application/x-config 49072 angelia wu