[#6206] no input device in ADP5588 testing on BF537-STAMP.
Submitted By: angelia wu
Open Date
2010-08-26 03:59:53 Close Date
2010-08-26 06:59:55
Priority:
Medium Assignee:
Michael Hennerich
Status:
Closed Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Blackfin Linux:2010R1
Category:
N/A Board:
STAMP
Processor:
BF537 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
svn-4681
App binary format:
Summary: no input device in ADP5588 testing on BF537-STAMP.
Details:
no input device in ADP5588 testing on BF537-STAMP.
the log as follow.
Using bfin_mac device
TFTP from server 10.100.4.174; our IP address is 10.100.4.50
Filename 'uImage'.
Load address: 0x1000000
Loading: #################################################################
#################################################################
###############################################################
done
Bytes transferred = 4735142 (4840a6 hex)
## Booting kernel from Legacy Image at 01000000 ...
Image Name: bf537-2.6.34.5-ADI-2010R1-pre-sv
Created: 2010-08-26 7:39:59 UTC
Image Type: Blackfin Linux Kernel Image (gzip compressed)
Data Size: 4735078 Bytes = 4.5 MiB
Load Address: 00001000
Entry Point: 001ab684
Verifying Checksum ... OK
Uncompressing Kernel Image ... OK
Starting Kernel at = 001ab684
Linux version 2.6.34.5-ADI-2010R1-pre-svn9105 (test@uclinux41) (gcc version 4.3.5 (ADI-trunk/svn-4681) ) #120 Thu Aug 26 15:39:54 CST 2010
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart0] enabled
early printk enabled on early_BFuart0
Limiting kernel memory to 56MB due to anomaly 05000263
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x0011d468
rodata = 0x0011d468-0x0017daec
bss = 0x0017e000-0x0018e584
data = 0x0018e584-0x001a0000
stack = 0x0019e000-0x001a0000
init = 0x001a0000-0x008ca000
available = 0x008ca000-0x03800000
DMA Zone = 0x03f00000-0x04000000
Hardware Trace Active and Enabled
Boot Mode: 0
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF537 Rev 0.2
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 500 MHz core clock and 125 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-back) in data cache
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 14224
Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50:10.100.4.174:10.100.4.174:f
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 47776k/65536k RAM, (7336k init code, 1137k kernel code, 523k data, 1024k dma, 7740k reserved)
Hierarchical RCU implementation.
NR_IRQS:138
Configuring Blackfin Priority Driven Interrupts
console [ttyBF0] enabled, bootconsole disabled
Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)
Security Framework initialized
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (35 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
stamp_init(): registering device resources
bio: create slab <bio-0> at 0
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7
i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400
Switching to clocksource bfin_cs_cycles
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
msgmni has been set to 93
io scheduler noop registered
io scheduler cfq registered (default)
bfin-uart: Blackfin serial driver
bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART
brd: module loaded
bfin_mii_bus: probed
bfin_mii_bus: Can't get IRQ 65535 (PHY)
bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)
bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
i2c /dev entries driver
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
TCP cubic registered
NET: Registered protocol family 17
IP-Config: Complete:etting system clock to 1970-01-04 11:16:12 UTC (299772)
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf537-stamp, domain=, nis-domain=(none),
bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=
dma_alloc_init: dma_page @ 0x0292d000 - 256 pages at 0x03f00000
Freeing unused kernel memory: 7336k freed
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - http://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.16.2 (2010-08-26 14:18:35 CST) hush - the humble shell
root:/> PHY: 0:01 - Link is Up - 100/Full
root:/> modprobe adp5588_keys
root:/> lsmod
Module Size Used by
adp5588_keys 4013 0
root:/> cd /bin/
root:/bin> event_test /dev/input/event0
evtest: No such file or directory
root:/bin> lsmod
root:/bin>
Follow-ups
--- Michael Hennerich 2010-08-26 05:10:51
Assign to me
--- Michael Hennerich 2010-08-26 05:47:57
KBUILD_MODNAME normalizes "-" to "_". This is none obvious
and results
that the id name for ADP5588 is "adp5588_keys" while the other
supported one is "adp5587-keys".
Use an obvious id name string for both supported devices.
fixed on trunk
please try again.
-Michael
--- angelia wu 2010-08-26 06:59:55
yes,i tried again and found this bug is indeed disappear. so i closed it .
Thank you Michael.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
kernel.537adp5588.config application/x-config 38445 angelia wu
user.537adp5588.config application/x-config 49083 angelia wu