[#6244] Build trunk kernel fails at built-in.o
Submitted By: Vivi Li
Open Date
2010-09-07 03:16:38 Close Date
2010-09-07 23:55:34
Priority:
Medium High Assignee:
Mike Frysinger
Status:
Closed Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Category:
Make Errors Board:
Processor:
ALL Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2010_Aug_04
App binary format:
Summary: Build trunk kernel fails at built-in.o
Details:
Build trunk kernel fails at built-in.o since kernel version 9126.
--
CC init/version.o
LD init/built-in.o
LD .tmp_vmlinux1
arch/blackfin/mach-common/built-in.o: In function `sys_call_table':
(.data+0x6d0): undefined reference to `sys_fanotify_init'
(.data+0x6d4): undefined reference to `sys_fanotify_mark'
(.data+0x6d8): undefined reference to `sys_prlimit64'
make[1]: *** [.tmp_vmlinux1] Error 1
make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x'
make: *** [linux] Error 1
Follow-ups
--- Mike Frysinger 2010-09-07 11:57:31
oops, should be fixed by marking them _sys_ni_syscall
--- Vivi Li 2010-09-07 23:55:34
OK now.
Close it.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found