[#6268] can not enter u-boot in bf526-ezbrd board 1.1 after reboot from trunk kernel
Submitted By: Vivi Li
Open Date
2010-09-20 05:42:22
Priority:
Medium Assignee:
Nobody
Status:
Open Fixed In Release:
N/A
Found In Release:
2010R1-RC5 Release:
Category:
N/A Board:
Processor:
BF526 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Out of Date
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2010_Aug_04
App binary format:
Summary: can not enter u-boot in bf526-ezbrd board 1.1 after reboot from trunk kernel
Details:
Can not enter u-boot in bf526-ezbrd board 1.1 after reboot from trunk kernel.
I can see this bug happens on board 1.1, silicon 0.2. No such problem on board 0.2, silicon 0.0.
Bellow is the log:
--
root:/> version
kernel: Linux release 2.6.34.7-ADI-2010R1-pre-svn9148, build #75 Sat Sep 18 03:59:17 CST 2010
toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-trunk/svn-4747)
user-dist: release svn-9818, build #1353 Sat Sep 18 03:58:29 CST 2010
root:/> reboot
Restarting system.
U-Boot 2010.06-svn2399 (ADI-2010R1-pre) (Sep 20 2010 - 07:24:32)
CPU: ADSP bf526-0.0 (Detected Rev: 0.2) (parallel flash boot)
Board: ADI BF526 EZ-Board board
Support: http://blackfin.uclinux.org/
Clock: VCO: 400 MHz, Core: 400 MHz, System: 80 MHz
RAM: 64 MiB
Flash: 4 MiB
In: serial
Out: serial
Err: serial
KGDB: [on serial] ready
Net: bfin_mac
Hit any key to stop autoboot: 3
(hit any key, can not enter uboot)
Follow-ups
--- Sonic Zhang 2012-01-12 05:04:05
Out of date since 2011R1
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found