[#6273] MTD NAND driver broken on BF537
Submitted By: Jay Ku
Open Date
2010-09-24 12:45:47
Priority:
Medium Assignee:
steven miao
Status:
Open Fixed In Release:
N/A
Found In Release:
N/A Release:
9821
Category:
N/A Board:
Processor:
ALL Silicon Revision:
0.3
Is this bug repeatable?:
Yes Resolution:
Rejected
Uboot version or rev.:
Toolchain version or rev.:
4927
App binary format:
Summary: MTD NAND driver broken on BF537
Details:
MTD platform flash driver appears to be broken. Lots of invalid bad eraseblocks are reported at boot, nandtest fails, etc. I'm using custom board with BF537 + NAND04GW3B2DN6E configured identically to BF537 Stamp + ADI CF/IDE/NAND expander board (except I'm using PF14 instead of PF3 for the ready signal from the flash). See this thread for more info:
http://blackfin.uclinux.org/gf/project/uclinux-dist/forum/?_forum_action=MessageReply&message_id=93721&thread_id=42815&action=ForumBrowse&forum_id=39
Follow-ups
--- steven miao 2010-10-14 02:55:22
I tested on BF537-stamp with CF/IDE/NAND extender board but cannt repeat this
error. It's OK on ADI's board.
root:/>
root:/> flash_eraseall /dev/mtd1
Erasing 128 Kibyte @ 7c00000 -- 100 % complete.
root:/> cat /proc/version
Linux version 2.6.34.7-ADI-2010R1-pre-svn9165 (steven@debiansteven) (gcc
version 4.1.2 (ADI svn)) #164 Sun Sep 26 14:17:08 CST 2010
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found