[#6278] adp8860 doesn't work right when writing a nonzero value to ambient_light_zone
Submitted By: Vivi Li
Open Date
2010-09-28 05:29:47 Close Date
2010-11-05 06:26:03
Priority:
Medium Assignee:
Michael Hennerich
Status:
Closed Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Category:
Drivers Board:
STAMP
Processor:
BF537 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3_2010R1-RC3
App binary format:
N/A
Summary: adp8860 doesn't work right when writing a nonzero value to ambient_light_zone
Details:
adp8860 doesn't work right when writing a nonzero value to ambient_light_zone.
Write 1 to ambient_light_zone, value remains 2;
Write 3 to ambient_light_zone, value becomes 4 and D6-D14 are off;
When write 0 to ambient_light_zone, it works right and return to normal operation.
Bellow is the log:
--
Linux version 2.6.34.7-ADI-2010R1-pre-svn9171 (test@linux-vivi) (gcc version 4.3.5 (ADI-2010R1-RC3) ) #9 Mon Sep 27 15:01:56 CST0
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart0] enabled
early printk enabled on early_BFuart0
Limiting kernel memory to 56MB due to anomaly 05000263
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x0010dbf0
rodata = 0x0010dbf0-0x00164964
bss = 0x00165000-0x00175464
data = 0x00175464-0x00186000
stack = 0x00184000-0x00186000
init = 0x00186000-0x002f5000
available = 0x002f5000-0x03800000
DMA Zone = 0x03f00000-0x04000000
Hardware Trace Active and Enabled
Boot Mode: 0
Reset caused by Software reset
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF537 Rev 0.2
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 500 MHz core clock and 125 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-back) in data cache
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 14224
Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 53748k/65536k RAM, (1468k init code, 1074k kernel code, 482k data, 1024k dma, 7740k reserved)
Hierarchical RCU implementation.
NR_IRQS:138
Configuring Blackfin Priority Driven Interrupts
console [ttyBF0] enabled, bootconsole disabled
console [ttyBF0] enabled, bootconsole disabled
Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)
Security Framework initialized
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (35 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
stamp_init(): registering device resources
bio: create slab <bio-0> at 0
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7
i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400
Switching to clocksource bfin_cs_cycles
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
msgmni has been set to 104
io scheduler noop registered
io scheduler cfq registered (default)
adp8860_bl 0-002a: adp8860 Rev.7 Backlight
bfin-uart: Blackfin serial driver
bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART
brd: module loaded
bfin_mii_bus: probed
bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)
bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
TCP cubic registered
NET: Registered protocol family 17
rtc-bfin rtc-bfin: setting system clock to 1970-01-01 05:17:39 UTC (19059)
IP-Config: Complete:
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf537-stamp, domain=, nis-domain=(none),
bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=
dma_alloc_init: dma_page @ 0x02327000 - 256 pages at 0x03f00000
Freeing unused kernel memory: 1468k freed
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - http://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.16.2 (2010-09-27 14:59:50 CST) hush - the humble shell
root:/> PHY: 0:01 - Link is Up - 100/Full
root:/> cat /sys/class/backlight/adp8860_bl/ambient_light_zone
2
root:/> echo 1 > /sys/class/backlight/adp8860_bl/ambient_light_zone
root:/> cat /sys/class/backlight/adp8860_bl/ambient_light_zone
2
root:/> echo 3 > /sys/class/backlight/adp8860_bl/ambient_light_zone
root:/> cat /sys/class/backlight/adp8860_bl/ambient_light_zone
4
root:/>
--
Follow-ups
--- Michael Hennerich 2010-09-28 11:54:01
assign to me.
-Michael
--- Vivi Li 2010-09-28 22:22:36
Hi Michael,
I did following stuff during adp8860. Please inform me if you find anything
inappropriate or test case I can add:
* Connect J30 adp886x adapter board to TWI interface on BF537-STAMP:
VBAT → P10.2, SDA → P10.6, SCL → P10.5, GND → P10.20
* Cover the photosensor D2 in ADP8860 daughter card, LED D6-D14 will dim;
* Change brightness of D6-D14 through
/sys/class/backlight/adp8860_bl/brightness;
* Other LEDs will blink when /sys/class/leds/adp8860-led7/brightness is
nonzero.
-Vivi
--- Vivi Li 2010-09-28 22:30:05
I thought ambient_light_zone should be only set to 1, 2 and 3, as mentioned in
wiki ADP8860 features 3 individually programmable Ambient Light Sensing Zones.
But later on the same page ambient_light_zone is an integer between 1 to 5.
I suppose there is something wrong.
Please refer to:
https://docs.blackfin.uclinux.org/doku.php?id=linux-kernel:drivers:adp8860.
--- Michael Hennerich 2010-09-29 04:50:38
Hi Vivi,
Good catch!
I fixed the driver as well as the documentation page.
video: backlight: adp8860: Fix ambient_light_zone overwrite handling
Get/Set current Ambient Light Zone. Reading returns integer between 1..3
(1 = Daylight, 2 = office, 3 = dark). Writing a value between 1..3 forces the
Backlight controller
to enter the corresponding Ambient Light Zone. Writing 0 returns to normal
operation.
Fix valid range and make sure we subtract 1, since the register definition
(CFGR:BLV) requires it.
Fixed on trunk and 2010R1 branch.
-Michael
--- Vivi Li 2010-11-05 06:26:03
OK, close it.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.kernel.adp8860 application/octet-stream 31832 Vivi Li