[#6327] Can not detect ad73322 on sport1 in trunk and 2010r1 on 537stamp
Submitted By: Vivi Li
Open Date
2010-11-02 05:57:22 Close Date
2010-11-16 07:17:29
Priority:
Medium Assignee:
Bob Liu
Status:
Closed Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Category:
Drivers Board:
Processor:
BF537 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
2010r1-rc4
App binary format:
Summary: Can not detect ad73322 on sport1 in trunk and 2010r1 on 537stamp
Details:
Can not detect ad73322 on sport1 on bf537-stamp in trunk and 2010r1 branch. Sport0 is OK.
--
Linux version 2.6.34.7-ADI-2010R1-svn9290 (test@uclinux56-ad73322-snormtd-df) (gcc version 4.3.5 (ADI-2010R1-RC4) ) #129 Tue Nov0
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart0] enabled
early printk enabled on early_BFuart0
Limiting kernel memory to 56MB due to anomaly 05000263
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x0012e940
rodata = 0x0012e940-0x00191930
bss = 0x00192000-0x001a2c9c
data = 0x001a2c9c-0x001b6000
stack = 0x001b4000-0x001b6000
init = 0x001b6000-0x00896000
available = 0x00896000-0x03800000
DMA Zone = 0x03e00000-0x04000000
Hardware Trace Active and Enabled
Boot Mode: 0
Reset caused by Software reset
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF537 Rev 0.2
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 500 MHz core clock and 125 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-back) in data cache
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 14224
Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 47984k/65536k RAM, (7040k init code, 1206k kernel code, 542k data, 2048k dma, 6716k reserved)
Hierarchical RCU implementation.
NR_IRQS:138
Configuring Blackfin Priority Driven Interrupts
console [ttyBF0] enabled, bootconsole disabled
Calibrating delay loop... 993.28 BogoMIPS (lpj=1986560)
Security Framework initialized
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (35 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
stamp_init(): registering device resources
bio: create slab <bio-0> at 0
Advanced Linux Sound Architecture Driver Version 1.0.22.1.
Switching to clocksource bfin_cs_cycles
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
msgmni has been set to 93
io scheduler noop registered
io scheduler cfq registered (default)
bfin-uart: Blackfin serial driver
bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART
brd: module loaded
bfin_mii_bus: probed
bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)
bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
dma_alloc_init: dma_page @ 0x028d8000 - 512 pages at 0x03e00000
dma rx:3 tx:4, err irq:45, regs:ffc00800
pin group conflict! request pin 29 func 1 conflict with pin 31 func 0
Requesting Peripherals failed
ALSA device list:
#0: Analog Devices AD73322 at PF10 SPORT0
TCP cubic registered
NET: Registered protocol family 17
IP-Config: Complete:etting system clock to 1970-01-01 07:33:37 UTC (27217)
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf537-stamp, domain=, nis-domain=(none),
bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=
Freeing unused kernel memory: 7040k freed
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - http://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.16.2 (2010-11-02 14:52:51 GMT) hush - the humble shell
root:/>
Follow-ups
--- Vivi Li 2010-11-02 06:36:52
Same error happens with test case spi_coexistence.
And its last passed time is 2010_Sep_16_20_09, ucdist version 9817, kernel
version 9142.
Bellow is the log:
Linux version 2.6.34.7-ADI-2010R1-pre-svn9148
(test@uclinux58-mmc-usblan-btuart) (gcc version 4.3.5 (ADI-trunk/svn-4747) )
#129 Sat Sep 18 15:54:21 GMT 2010
text = 0x00001000-0x0014d3f8
rodata = 0x0014d3f8-0x001bdf1c
bss = 0x001be000-0x001cecf4
data = 0x001cecf4-0x001e2000
stack = 0x001e0000-0x001e2000
init = 0x001e2000-0x008e5000
available = 0x008e5000-0x03800000
DMA Zone = 0x03f00000-0x04000000
Kernel command line: root=/dev/mtdblock0 rw ip=10.100.4.50
earlyprintk=serial,uart0,57600 console=ttyBF0,57600
ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:bf537-stamp:eth0:off
Memory available: 47668k/65536k RAM, (7180k init code, 1328k kernel code, 596k
data, 1024k dma, 7740k reserved)
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0,
regs_base@ffc00500, dma channel@7
bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1,
mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)
mmc_spi spi0.4: ASSUMING 3.2-3.4 V slot power
mmc_spi spi0.4: SD/MMC host mmc0, no DMA, no WP, no poweroff
<3>pin grounp conflict! request pin 29 func 1 conflict with pin 31 func
0
mmc_spi spi0.4: can't change chip-select polarity
No soundcards found.
rtc-bfin rtc-bfin: setting system clock to 1971-04-17 02:13:56 UTC (40702436)
mmc0: host does not support reading read-only switch. assuming write-enable.
mmc0: new SD card on SPI
mmcblk0: mmc0:0000 SD256 241 MiB
mmcblk0: p1
IP-Config: Complete:
dma_alloc_init: dma_page @ 0x0292c000 - 256 pages at 0x03f00000
Freeing unused kernel memory: 7180k freed
BusyBox v1.16.2 (2010-09-18 15:50:46 GMT) hush - the humble shell
root:/> ^[[6nversionPHY: 0:01 - Link is Up - 100/Full
--- Bob Liu 2010-11-07 21:43:29
fixed.
1. config the kernel with CONFIG_SND_BF5XX_SPORT_NUM=2
2. update commit 9497.
--- Bob Liu 2010-11-07 21:44:53
Sorry commit 9479 not 9497.
--- Vivi Li 2010-11-16 07:17:29
Ad73322 can be detected now.
Close it.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.linux.audio_ad73322 application/octet-stream 36821 Vivi Li