[#6341] kgdb test fail for xenomai kernel
Submitted By: Vivi Li
Open Date
2010-11-15 22:13:41 Close Date
2010-11-19 02:42:38
Priority:
Medium Assignee:
Sonic Zhang
Status:
Closed Fixed In Release:
N/A
Found In Release:
2010R1 Release:
Category:
N/A Board:
Processor:
BF537 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
2010r1-rc4
App binary format:
Summary: kgdb test fail for xenomai kernel
Details:
kgdb test fail for xenomai kernel in trunk and branch.
--
Starting Kernel at = 00201834
console [ttyBF0] enabled, bootconsole disabled
Calibrating delay loop... 991.23 BogoMIPS (lpj=1982464)
Security Framework initialized
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (15 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (34 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
stamp_init(): registering device resources
bio: create slab <bio-0> at 0
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7
Switching to clocksource bfin_cs_cycles
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
I-pipe: Domain Xenomai registered.
Xenomai: hal/blackfin started.
Xenomai: scheduling class idle registered.
Xenomai: scheduling class rt registered.
Xenomai: real-time nucleus v2.5.3 (Hordes Of Locusts) loaded.
Xenomai: starting native API services.
Xenomai: starting POSIX services.
Xenomai: starting RTDM services.
msgmni has been set to 93
io scheduler noop registered
io scheduler cfq registered (default)
bfin-uart: Blackfin serial driver
bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART
brd: module loaded
bfin_mii_bus: probed
bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)
bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1
console [netcon0] enabled
netconsole: network logging started
kgdboe: local port 6443
kgdboe: local IP 10.100.4.50
kgdboe: interface 'eth0'
kgdboe: remote port 6442
kgdboe: remote IP 10.100.4.174
kgdboe: remote ethernet address ff:ff:ff:ff:ff:ff
kgdboe: device eth0 not up yet, forcing it
kgdboe: carrier detect appears untrustworthy, waiting 4 seconds
PHY: 0:01 - Link is Up - 100/Full
kgdb: Registered I/O driver kgdboe.
kgdboe: debugging over ethernet enabled
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
TCP cubic registered
NET: Registered protocol family 17
rtc-bfin rtc-bfin: setting system clock to 1972-09-13 10:29:41 UTC (85228181)
dma_alloc_init: dma_page @ 0x0298d000 - 256 pages at 0x03f00000
Freeing unused kernel memory: 7116k freed
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - http://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.16.2 (2010-11-09 22:44:56 GMT-8) hush - the humble shell
root:/> ^[[6nversion
kernel: Linux release 2.6.34.7-ADI-2010R1-svn9479, build #4 Wed Nov 10 05:33:23 GMT-8 2010
toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-2010R1-RC4)
user-dist: release svn-9913, build #9 Wed Nov 10 05:31:47 GMT-8 2010
root:/> ^[[6nsuccessful boot attempt
************** STEP 3: Start KGDB TEST (ethernet)
ifconfig eth0 10.100.4.50
root:/> ^[[6nspawn bfin-uclinux-gdb /home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x/vmlinux
^[[?1034hGNU gdb 6.6
Copyright (C) 2006 Free Software Foundation, Inc.
GDB is free software, covered by the GNU General Public License, and you are
welcome to change it and/or distribute copies of it under certain conditions.
Type "show copying" to see the conditions.
There is absolutely no warranty for GDB. Type "show warranty" for details.
This GDB was configured as "--host=i686-pc-linux-gnu --target=bfin-uclinux"...
(gdb)
Case 1 ...PASS
target remote udp:10.100.4.50:6443
warning: The remote protocol may be unreliable over UDP.
Some events may be lost, rendering further debugging impossible.
Remote debugging using udp:10.100.4.50:6443
Case 2 ...PASS
kgdb_breakpoint ()
at /home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x/arch/blackfin/include/asm/irqflags.h:29
29 asm volatile("cli %0;" : "=d" (flags));
(gdb) break kgdb_test
Breakpoint 1 at 0x84da: file arch/blackfin/kernel/kgdb_test.c, line 56.
Case 3 ...PASS
(gdb) c
Continuing.
Case 4 ...PASS
root:/> ^[[6n[New Thread 214]
[Switching to Thread 214]
Breakpoint 1, kgdb_test (name=0x14cdd0 "hello world!", len=12, count=85, z=16)
at arch/blackfin/kernel/kgdb_test.c:56
56 pr_alert("kgdb name(%d): %s, %d, %d\n", len, name, count, z);
Case 5 ...PASS
(gdb) hbreak 58
Hardware assisted breakpoint 2 at 0x8500: file arch/blackfin/kernel/kgdb_test.c, line 58.
Case 6 ...PASS
info b
Num Type Disp Enb Address What
1 breakpoint keep y 0x000084da in kgdb_test
breakpoint already hit 1 time
2 hw breakpoint keep y 0x00008500 in kgdb_test
at arch/blackfin/kernel/kgdb_test.c:58
Case 7 ...PASS
(gdb) list
51 #endif
52
53
54 int kgdb_test(char *name, int len, int count, int z)
55 {
57 count = z;
58 return count;
59 }
60
Case 8 ...PASS
bt
#0 kgdb_test (name=0x14cdd0 "hello world!", len=12, count=85, z=16)
Case 9 ...PASS
#1 0x00008530 in kgdb_test_proc_read (file=0x2085d20, buf=0x2c69e80 "",
count=4096, ppos=0x2b51eec) at arch/blackfin/kernel/kgdb_test.c:65
#2 0x000a0b30 in proc_reg_read (file=0x2085d20,
buf=0xc <Address 0xc out of bounds>, count=85, ppos=0x2b51eec)
at fs/proc/inode.c:163
#3 0x000767d2 in vfs_read (file=0x2085d20, buf=0x2c69e80 "",
count=<value optimized out>, pos=0x2b51eec) at fs/read_write.c:293
#4 0x000768f8 in sys_read (fd=<value optimized out>, buf=0x2c69e80 "",
count=4096) at fs/read_write.c:383
#5 0xffa00a64 in system_call () at include/linux/thread_info.h:86
(gdb) spawn /bin/sh
^[[?1034huclinux82-537-adeos:~/work/cruise/checkouts/uclinux-dist/testsuites/kgdb> ps aux | grep bfin-uclinux-gdb
test 7713 2.0 3.3 40136 34400 pts/2 Ss+ 05:34 0:00 bfin-uclinux-gdb /home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x/vmlinux
test 7724 0.0 0.0 3064 728 pts/3 S+ 05:35 0:00 grep bfin-uclinux-gdb
uclinux82-537-adeos:~/work/cruise/checkouts/uclinux-dist/testsuites/kgdb> kill - 9 `pidof bfin-uclinux-gdb`
uclinux82-537-adeos:~/work/cruise/checkouts/uclinux-dist/testsuites/kgdb>
Case 10 ...FAIL
KGDB TEST (ethernet) FAIL
KGDB TEST (ethernet) ............[FAIL]
Follow-ups
--- Sonic Zhang 2010-11-17 01:20:16
When ADEOS and kgdb are both enabled, single step in linux kernel may be
scheduled to Xenomai core after return from interrupt hanlders. This
blocks gdb continue operation after a break point is hit. So, disable
interrupt when running gdb single step.
--- Vivi Li 2010-11-19 02:42:37
OK now. Close it.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.linux.kgdb application/octet-stream 40478 Vivi Li
config.config.kgdb application/octet-stream 49226 Vivi Li