[#6405] Can not ping between two adf7021
Submitted By: Vivi Li
Open Date
2010-12-13 23:24:30
Priority:
Medium Assignee:
Michael Hennerich
Status:
Open Fixed In Release:
N/A
Found In Release:
2011R1 Release:
Category:
N/A Board:
N/A
Processor:
BF537 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Assigned (Not Start)
Uboot version or rev.:
Toolchain version or rev.:
trunk
App binary format:
N/A
Summary: Can not ping between two adf7021
Details:
Can not ping between two adf7021.
This happens on 2010r1 branch and trunk.
--
Linux version 2.6.34.7-ADI-2010R1-svn9479 (test@uclinux41) (gcc version 4.3.5 (ADI-2010R1-RC4) ) #260 Mon Nov 8 12:07:49 CST 2010
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart0] enabled
early printk enabled on early_BFuart0
Limiting kernel memory to 56MB due to anomaly 05000263
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x001206e0
rodata = 0x001206e0-0x0018e0c4
bss = 0x0018f000-0x0019f514
data = 0x0019f514-0x001ba000
stack = 0x001b8000-0x001ba000
init = 0x001ba000-0x00897000
available = 0x00897000-0x03800000
DMA Zone = 0x03f00000-0x04000000
Hardware Trace Active and Enabled
Boot Mode: 0
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF537 Rev 0.2
Warning: Compiled for Rev 2, but running on Rev 3
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 500 MHz core clock and 125 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-back) in data cache
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 14224
Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 47980k/65536k RAM, (7028k init code, 1149k kernel code, 615k data, 1024k dma, 7740k reserved)
Hierarchical RCU implementation.
NR_IRQS:138
Configuring Blackfin Priority Driven Interrupts
console [ttyBF0] enabled, bootconsole disabled
console [ttyBF0] enabled, bootconsole disabled
Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)
Security Framework initialized
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (35 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
stamp_init(): registering device resources
bio: create slab <bio-0> at 0
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7
Switching to clocksource bfin_cs_cycles
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
msgmni has been set to 93
alg: No test for stdrng (krng)
io scheduler noop registered
io scheduler cfq registered (default)
bfin-uart: Blackfin serial driver
bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART
brd: module loaded
dma_alloc_init: dma_page @ 0x028de000 - 256 pages at 0x03f00000
adf702x spi0.18: ADF702XNet Wireless Ethernet driver
bfin_mii_bus: probed
bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)
bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
TCP cubic registered
NET: Registered protocol family 17
rtc-bfin rtc-bfin: setting system clock to 1970-01-01 00:15:37 UTC (937)
Freeing unused kernel memory: 7028k freed
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For™¥¹zj¤ed proce'$HH 'Y88b \___________________________________/
:8P ' :888• •Í±…
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - https://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.16.2 (2010-11-08 10:24:51 CST) hush - the humble shell
root:/> PuTTY
sh: can't execute 'PuTTY': No such file or directory
root:/>
root:/>
root:/>
root:/>
root:/>
root:/> ifconfig
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
root:/> ifconfig eth0 192.168.1.4
root:/> ifconfig
eth0 Link encap:Ethernet HWaddr 22:DA:E2:A8:86:2A
inet addr:192.168.1.4 Bcast:192.168.1.255 Mask:255.255.255.0
UP BROADCAST RUNNING MULTICAST MTU:576 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
root:/> ping 192.168.1.4
PING 192.168.1.4 (192.168.1.4): 56 data bytes
64 bytes from 192.168.1.4: seq=0 ttl=64 time=0.392 ms
64 bytes from 192.168.1.4: seq=1 ttl=64 time=0.228 ms
64 bytes from 192.168.1.4: seq=2 ttl=64 time=0.237 ms
64 bytes from 192.168.1.4: seq=3 ttl=64 time=0.226 ms
64 bytes from 192.168.1.4: seq=4 ttl=64 time=0.239 ms
64 bytes from 192.168.1.4: seq=5 ttl=64 time=0.227 ms
^C
--- 192.168.1.4 ping statistics ---
6 packets transmitted, 6 packets received, 0% packet loss
round-trip min/avg/max = 0.226/0.258/0.392 ms
root:/>
root:/>
(set up another adf7021 and set ip to 192.168.1.3)
root:/> ping 192.168.1.3
PING 192.168.1.3 (192.168.1.3): 56 data bytes
--
Follow-ups
--- Sonic Zhang 2010-12-13 23:45:49
Michael, can you take a look?
--- Michael Hennerich 2010-12-14 05:29:44
Sonic,
Did this test ever pass?
I assume not. It's very likely a board configuration problem.
I wouldn't consider this a critical bug.
I'll take a look once I have time.
-Michael
--- Vivi Li 2010-12-14 22:15:06
Michael,
I never test the ping function before as I had only one adf7021 board. Another
adf7021 board arrived just a week ago.
-Vivi
--- Vivi Li 2011-12-22 03:29:58
I've test with two adf7021 boards and they can't ping to each other.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.linux.adf702x application/octet-stream 36000 Vivi Li