[#6448] Fail to build blackfin_cam.c on bf561-ezkit after kernel upgrade in latest trunk
Submitted By: Vivi Li
Open Date
2011-01-17 04:02:41 Close Date
2011-01-17 04:28:13
Priority:
Medium Assignee:
Scott Jiang
Status:
Closed Fixed In Release:
N/A
Found In Release:
2011R1 Release:
Category:
Make Errors Board:
Processor:
BF561 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Duplicate
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2010_Dec_09
App binary format:
Summary: Fail to build blackfin_cam.c on bf561-ezkit after kernel upgrade in latest trunk
Details:
Fail to build blackfin_cam.c on bf561-ezkit after kernel upgrade in latest trunk.
Last passed version:
--
kernel: Linux release 2.6.36.2-ADI-2011R1-pre-svn9542, build #28 Wed Jan 5 22:32:43 CST 2011
toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-trunk/svn-5013)
user-dist: release svn-10036, build #426 Wed Jan 5 22:31:55 CST 2011
First failed version:
kernel: Linux release 2.6.37-ADI-2011R1-pre-svn9548, build #34 Fri Jan 7 00:00:34 CST 2011
user-dist: release svn-10036, build #493 Thu Jan 6 23:59:36 CST 2011
Bellow is the error log:
CC drivers/media/video/blackfin/blackfin_cam.o
In file included from drivers/media/video/blackfin/blackfin_cam.c:84:
drivers/media/video/blackfin/adv7183b.h:79:1: warning: "DMA_WDSIZE_16" redefined
drivers/media/video/blackfin/adv7183b.h:72:1: warning: this is the location of the previous definition
drivers/media/video/blackfin/adv7183b.h:80:1: warning: "PPI_PACKING" redefined
drivers/media/video/blackfin/adv7183b.h:73:1: warning: this is the location of the previous definition
drivers/media/video/blackfin/blackfin_cam.c:118: warning: data definition has no type or storage class
drivers/media/video/blackfin/blackfin_cam.c:118: warning: type defaults to ‘int’ in declaration of ‘I2C_CLIENT_INSMOD’
drivers/media/video/blackfin/blackfin_cam.c:1391: error: unknown field ‘get_unmapped_area’ specified in initializer
drivers/media/video/blackfin/blackfin_cam.c:1391: warning: initialization from incompatible pointer type
make[5]: *** [drivers/media/video/blackfin/blackfin_cam.o] Error 1
make[4]: *** [drivers/media/video/blackfin] Error 2
make[4]: *** Waiting for unfinished jobs....
Follow-ups
--- Mike Frysinger 2011-01-17 04:28:13
dupe of [#6437]
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.camera_adv7183 application/octet-stream 33654 Vivi Li