[#6562] pound stress test fails now
Submitted By: Mingquan Pan
Open Date
2011-04-28 04:51:44 Close Date
2011-05-25 03:37:30
Priority:
Medium Assignee:
steven miao
Status:
Closed Fixed In Release:
N/A
Found In Release:
2011R1 Release:
Category:
N/A Board:
Processor:
ALL Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Not reproducible
Uboot version or rev.:
Toolchain version or rev.:
5013
App binary format:
Summary: pound stress test fails now
Details:
pound stress test fails now.
BusyBox v1.18.4 (2011-04-21 05:24:17 CST) hush - the humble shell^M
^M
root:/> ^[[6nversiPHY: 0:01 - Link is Up - 100/Full^M
on^M
kernel: Linux release 2.6.39-rc4-ADI-2011R1-pre-svn9863, build #315 Thu Apr 21 10:41:55 CST 2011^M
toolchain: bfin-uclinux-gcc release Using built-in specs. Target: bfin-uclinux Configured with: /home/test/work/cruise/checkouts/toolchain/gcc-4.3/configure --build=i686-pc-linux-gnu --host=i686-pc-linux-gnu --target=bfin-uclinux --prefix=/home/test/work/cruise/test_scripts/toolchain/toolchain-build/toolchain-2010_Dec_09_03_12/bfin-uclinux --disable-libstdcxx-pch --with-sysroot=/home/test/work/cruise/test_scripts/toolchain/toolchain-build/toolchain-2010_Dec_09_03_12/bfin-uclinux/bfin-uclinux/runtime --enable-threads=posix --enable-clocale=generic --disable-symvers --disable-libssp --disable-libffi --disable-libgcj --enable-version-specific-runtime-libs --enable-__cxa_atexit --with-bugurl=URL:http://blackfin.uclinux.org/gf/project/toolchain/tracker --with-pkgversion=ADI-trunk/svn-5013 Thread model: posix gcc version 4.3.5 (ADI-trunk/svn-5013) ^M
user-dist: release svn-10144, build #4357 Thu Apr 21 10:40:57 CST 2011^M
root:/> ^[[6nsuccessful boot attempt
************** STEP 4: Start testing.
ls /etc/pound/mycert.pem^M
^[[0;0m/etc/pound/mycert.pem^[[0m^M
root:/> ^[[6nls /usr/local/etc/pound.cfg^M
^[[0;0m/usr/local/etc/pound.cfg^[[0m^M
root:/> ^[[6nifconfig eth0 10.100.4.50^M
root:/> ^[[6nboa -c /etc &^M
[1] 167 boa -c /etc^M
root:/> ^[[6n[18/May/1970:01:03:18 +0000] boa: server version Boa/0.94.14rc21^M
[18/May/1970:01:03:18 +0000] boa: server built Apr 21 2011 at 05:24:13.^M
[18/May/1970:01:03:18 +0000] boa: starting server pid=168, port 80^M
pound &^M
[2] 169 pound^M
[1] Done boa -c /etc^M
root:/> ^[[6nps aux^M
PID USER VSZ STAT COMMAND^M
1 root 104 S /init^M
2 root 0 SW [kthreadd]^M
3 root 0 SW [ksoftirqd/0]^M
4 root 0 SW [kworker/0:0]^M
5 root 0 SW [kworker/u:0]^M
6 root 0 SW [rcu_kthread]^M
7 root 0 SW< [khelper]^M
8 root 0 SW [kworker/u:1]^M
46 root 0 SW [sync_supers]^M
48 root 0 SW [bdi-default]^M
50 root 0 SW< [kblockd]^M
52 root 0 SW< [bfin-spi.0]^M
74 root 0 SW [khungtaskd]^M
75 root 0 SW [kswapd0]^M
.....
161 root 464 S /sbin/klogd -n^M
162 root 32 S /bin/watchdogd -f -s^M
168 root 288 S boa -c /etc^M
169 root 1688 S pound^M
170 root 1688 S pound^M
171 root 1688 S pound^M
172 root 1688 S pound^M
spawn fl-run-test test_Simple.py^M
ADI ucLinux Group^M
https://10.100.4.50/test^M
rcp -rp ../test root@10.100.4.50:/home/httpd/^M
rcp ok! Start webserver test.^M
Try 0^M
/index.html ----OK!^M
/BlackfinUboot.htm ----OK!^M
/BlackfinuClinux.htm ----OK!^M
Try 1^M
...
....
Try 823^M
Try 824^M
Try 825^M
pound test fail to exit.
Last passed time: 2011_Apr_19_21_11, ucdist ver: 10142, kernel ver: 9857
Case 1 ...FAIL
Follow-ups
--- steven miao 2011-05-10 22:41:41
manual test passed
test_simple: Try 999
Try 999
test_simple: GET: http://10.99.29.106/test/index.html
Page 2998: Get /index.html ...
test_simple: Done in 0.005s
test_simple: Load css and images...
test_simple: Done in 0.000s
/index.html ----OK!
test_simple: GET: http://10.99.29.106/test/BlackfinUboot.htm
Page 2999: Get /BlackfinUboot.htm ...
test_simple: Done in 0.006s
/BlackfinUboot.htm ----OK!
test_simple: GET: http://10.99.29.106/test/BlackfinuClinux.htm
Page 3000: Get /BlackfinuClinux.htm ...
test_simple: Done in 0.007s
/BlackfinuClinux.htm ----OK!
test_simple: tearDown.
.
----------------------------------------------------------------------
Ran 1 test in 7635.229s
OK
--- Mingquan Pan 2011-05-25 03:37:30
It looks this test goes back to normal on the regression machines now.
So close for now.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found