[#6653] ssm2602 fails to work on trunk
Submitted By: Vivi Li
Open Date
2011-06-16 04:48:12 Close Date
2011-08-15 06:39:10
Priority:
Medium Assignee:
Scott Jiang
Status:
Closed Fixed In Release:
N/A
Found In Release:
2011R1 Release:
Category:
Drivers Board:
N/A
Processor:
BF527 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Duplicate
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2010_Dec_09
App binary format:
N/A
Summary: ssm2602 fails to work on trunk
Details:
ssm2602 fails to work on trunk. It can't be detected.
Bellow is log:
--
Linux version 2.6.39.1-ADI-2011R1-pre-svn9931 (test@uclinux63-527-usbdev) (gcc version 4.3.5 (ADI-2010R1-RC4) ) #6 Wed Jun 15 221
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart1] enabled
early printk enabled on early_BFuart1
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x001790c8
rodata = 0x001790c8-0x001f8ba0
bss = 0x001f9000-0x0020abcc
data = 0x0020abcc-0x00224000
stack = 0x00222000-0x00224000
init = 0x00224000-0x00912000
available = 0x00912000-0x03e00000
DMA Zone = 0x03e00000-0x04000000
Hardware Trace active and enabled
Boot Mode: 1
Reset caused by Software reset
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF527 Rev 0.2
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 525 MHz core clock and 131 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-back) in data cache
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 15748
Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart1,57600 console=tty0 console=ttyBF1,57600 if
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 53592k/65536k RAM, (7096k init code, 1504k kernel code, 684k data, 2048k dma, 612k reserved)
NR_IRQS:159
Configuring Blackfin Priority Driven Interrupts
console [ttyBF1] enabled, bootconsole disabled
console [ttyBF1] enabled, bootconsole disabled
Calibrating delay loop... 1044.48 BogoMIPS (lpj=2088960)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (41 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
ezkit_init(): registering device resources
bio: create slab <bio-0> at 0
SCSI subsystem initialized
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400
Advanced Linux Sound Architecture Driver Version 1.0.24.
musb-hdrc: version 6.0, musb-dma, host, debug=0
musb-hdrc musb-hdrc: MUSB HDRC host driver
musb-hdrc musb-hdrc: new USB bus registered, assigned bus number 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc: USB Host mode controller at ffc03800 using DMA, IRQ 59
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCntries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
debug-mmrs: setting up Blackfin MMR debugfs
msgmni has been set to 104
io scheduler noop registered (default)
bfin-uart: Blackfin serial driver
bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART
bfin-otp: initialized
brd: module loaded
adp5520 0-0032: failed writing 0x80 to 0x00
adp5520 0-0032: failed to write
adp5520: probe of 0-0032 failed with error -1
bfin-spi bfin-spi.0: transfer: unsupported bits_per_word
m25p80: probe of spi0.1 failed with error -22
bfin_mii_bus: probed
bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=25)@sclk=131MHz)
bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
ad7879 0-002c: Failed to write AD7879 Touchscreen
ad7879: probe of 0-002c failed with error -1
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
bfin-i2s bfin-i2s.1: dma rx:5 tx:6, err irq:16, regs:ffc00900
ALSA device list:
No soundcards found.
TCP cubic registered
NET: Registered protocol family 17
rtc-bfin rtc-bfin: setting system clock to 1999-01-29 12:32:52 UTC (917613172)
musb_stage0_irq 810: unhandled DISCONNECT transition (a_idle)
IP-Config: Complete:
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf527-ezkit, domain=, nis-domain=(none),
bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=
dma_alloc_init: dma_page @ 0x02916000 - 512 pages at 0x03e00000
Freeing unused kernel memory: 7096k freed
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - https://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.18.4 (2011-06-15 21:59:28 CST) hush - the humble shell
root:/> PHY: 0:01 - Link is Up - 100/Full
root:/> tone
ERROR: failed to open DAC device /dev/dsp
root:/>
--
Follow-ups
--- Scott Jiang 2011-07-05 06:33:47
duplicate of #6638
--- Vivi Li 2011-08-15 06:39:09
OK now, close it.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.linux.audio_ssm2603 application/octet-stream 48068 Vivi Li