[#6788] BF561-ezkit SMP kernel can't wake up through uart in latest trunk
Submitted By: Vivi Li
Open Date
2011-09-06 05:08:36 Close Date
2012-01-17 00:29:46
Priority:
Medium Assignee:
Vivi Li
steven miao
Status:
Closed Fixed In Release:
N/A
Found In Release:
2011R1 Release:
Category:
N/A Board:
Processor:
BF561 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2011R1-RC1
App binary format:
Summary: BF561-ezkit SMP kernel can't wake up through uart in latest trunk
Details:
BF561-ezkit SMP kernel can't wake up from standby mode through uart after kernel is upgraded to 3.0.0.
Last passed version:
--
kernel: Linux release 2.6.39.3-ADI-2011R1-pre-svn10024, build #36 SMP Mon Jul 18 11:00:52 GMT 2011
toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-trunk/svn-5013)
user-dist: release svn-10258, build #295 Mon Jul 18 10:59:49 GMT 2011
Bellow is the error log:
Linux version 3.0.0-ADI-2011R1-pre-svn10071 (test@uclinux65-561-SMP) (gcc version 4.3.5 (ADI-2011R1-RC1) ) #158 SMP Mon Sep 5 02:39:14 GMT 2011
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart0] enabled
early printk enabled on early_BFuart0
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x00134d68
rodata = 0x00134d80-0x00190de4
bss = 0x00191000-0x001a2438
data = 0x001a2440-0x001b4000
stack = 0x001b2000-0x001b4000
init = 0x001b4000-0x0071c000
available = 0x0071c000-0x03f00000
DMA Zone = 0x03f00000-0x04000000
Hardware Trace active and enabled
Boot Mode: 0
Reset caused by Software reset
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF561 Rev 0.5
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 600 MHz core clock and 100 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
L2 SRAM : uncacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-through) in data cache
L2 SRAM : uncacheable in data cache
PERCPU: Embedded 7 pages/cpu @007a1000 s4480 r8192 d16000 u32768
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 16002
Kernel command line: root=/dev/mtdblock0 rw ip=10.100.4.50 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:bf561-ezkit:eth0:off
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 56592k/65536k RAM, (5536k init code, 1231k kernel code, 509k data, 1024k dma, 644k reserved)
Hierarchical RCU implementation.
NR_IRQS:153
Configuring Blackfin Priority Driven Interrupts
console [ttyBF0] enabled, bootconsole disabled
Calibrating delay loop... 1185.79 BogoMIPS (lpj=2371584)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
Booting Core B.
Brought up 2 CPUs
Instruction Cache Enabled for CPU1
Data Cache Enabled for CPU1
SMP: Total of 2 processors activated (2371.58 BogoMIPS).
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 16 KB (15 KB free)
Blackfin L2 SRAM: 128 KB (127 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
ezkit_init(): registering device resources
bio: create slab <bio-0> at 0
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc00500, dma channel@16
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 128 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 128 (order: 0, 4096 bytes)
NET: Registered protocol family 1
debug-mmrs: setting up Blackfin MMR debugfs
msgmni has been set to 110
io scheduler noop registered (default)
bfin-uart: Blackfin serial driver
bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 35) is a BFIN-UART
brd: module loaded
physmap platform flash device: 00800000 at 20000000
physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000020 Chip ID 0x0022ed
Amd/Fujitsu Extended Query Table at 0x0040
Amd/Fujitsu Extended Query version 1.3.
physmap-flash.0: Swapping erase regions for top-boot CFI table.
number of CFI chips: 1
Using physmap partition information
Creating 5 MTD partitions on "physmap-flash.0":
0x000000000000-0x000000040000 : "bootloader(nor)"
0x000000040000-0x000000200000 : "linux kernel(nor)"
0x000000200000-0x0000007f0000 : "file system(nor)"
0x0000007f0000-0x0000007fe000 : "config(nor)"
0x0000007fe000-0x000000800000 : "u-boot env(nor)"
smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@fluxnic.net>
eth0: SMC91C11xFD (rev 2) at 2c010300 IRQ 82 [nowait]
eth0: Ethernet addr: 00:e0:22:fe:ba:29
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
TCP cubic registered
NET: Registered protocol family 17
smc91x smc91x.0: eth0: link down
smc91x smc91x.0: eth0: link up, 100Mbps, full-duplex, lpa 0x41E1
IP-Config: Complete:
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf561-ezkit, domain=, nis-domain=(none),
bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=
Freeing unused kernel memory: 5536k freed
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - http://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.18.4 (2011-09-04 20:41:52 GMT) hush - the humble shell
root:/> echo enabled > /sys/class/tty/ttyBF0/power/wakeup
root:/> cat /sys/class/tty/ttyBF0/power/wakeup
enabled
root:/> echo standby > /sys/power/state
PM: Syncing filesystems ... done.
Freezing user space processes ... (elapsed 0.02 seconds) done.
Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done.
Suspending console(s) (use no_console_suspend to debug)
Follow-ups
--- steven miao 2011-09-23 05:55:52
it hangs when disable_nonboot_cpu call workqueue callback on CPU_DOWN_PREPARE
action
--- Sonic Zhang 2011-11-01 06:22:06
ISUPP interrupts are disabled in IMASK1 in suspend. But, a new thread is created
on and scheduled to run on the other core by IPI.
--- steven miao 2011-11-29 05:52:23
add IRQF_NO_SUSPEND | IRQF_FORCE_RESUME to irq flags, supplement irq should not
be disabled
--- Vivi Li 2011-12-07 04:57:29
OK in branch.
Need further confirmation after regression test is switched back to trunk.
--- Vivi Li 2012-01-17 00:58:26
OK in trunk.
Close this bug.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.linux.uart_wakeup application/octet-stream 29656 Vivi Li