[#6824] Fail to record with adau1361
Submitted By: Vivi Li
Open Date
2011-10-19 01:58:17 Close Date
2011-11-14 21:51:36
Priority:
Medium High Assignee:
Lars-Peter Clausen
Status:
Closed Fixed In Release:
N/A
Found In Release:
2011R1 Release:
Category:
N/A Board:
Processor:
BF537 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2011R1-RC2
App binary format:
Summary: Fail to record with adau1361
Details:
Can't detect adau1361 in latest trunk.
--
Starting Kernel at = 001e5c48
Linux version 3.0.0-ADI-2011R1-pre-svn10097 (test@linux-cdlb) (gcc version 4.3.5 (ADI-2011R1-RC2) ) #3 Wed Oct 19 13:38:32 CST 21
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart0] enabled
early printk enabled on early_BFuart0
Limiting kernel memory to 56MB due to anomaly 05000263
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x0014c508
rodata = 0x0014c508-0x001b8114
bss = 0x001b9000-0x001c9328
data = 0x001c9328-0x001de000
stack = 0x001dc000-0x001de000
init = 0x001de000-0x00959000
available = 0x00959000-0x03800000
DMA Zone = 0x03e00000-0x04000000
Hardware Trace active and enabled
Boot Mode: 0
Reset caused by Software reset
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF537 Rev 0.2
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 500 MHz core clock and 125 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-back) in data cache
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 14224
Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 47164k/65536k RAM, (7660k init code, 1325k kernel code, 583k data, 2048k dma, 6756k reserved)
NR_IRQS:146
Configuring Blackfin Priority Driven Interrupts
console [ttyBF0] enabled, bootconsole disabled
Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (35 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
stamp_init(): registering device resources
bio: create slab <bio-0> at 0
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc00500, dma channel@7
i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400
Advanced Linux Sound Architecture Driver Version 1.0.24.
Switching to clocksource bfin_cs_cycles
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
debug-mmrs: setting up Blackfin MMR debugfs
msgmni has been set to 92
io scheduler noop registered (default)
bfin-uart: Blackfin serial driver
bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART
brd: module loaded
bfin_mii_bus: probed
bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)
bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
bfin-i2s bfin-i2s.0: dma rx:3 tx:4, err irq:45, regs:ffc00800
ALSA device list:
No soundcards found.
TCP cubic registered
NET: Registered protocol family 17
rtc-bfin rtc-bfin: setting system clock to 1970-01-01 07:05:50 UTC (25550)
IP-Config: Complete:
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf537-stamp, domain=, nis-domain=(none),
bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=
dma_alloc_init: dma_page @ 0x029bd000 - 512 pages at 0x03e00000
Freeing unused kernel memory: 7660k freed
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - http://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.18.4 (2011-10-19 13:36:03 CST) hush - the humble shell
root:/> PHY: 0:01 - Link is Up - 100/Full
root:/>
root:/> tone
ERROR: failed to open DAC device /dev/dsp
Follow-ups
--- Vivi Li 2011-11-11 06:25:39
In latest 2011r1 branch, this card can be detected. And output is OK as I use
aplay and tone.
But arecord fails.
I attach EVAL-ADAU1X61EBZ(Rev B) to BF537-STAMP board. Input connector is
J24(IN3/4).
After I enable the "Right Playback Mixer Right Bypass Volume" and
"Left Playback Mixer Left Bypass Volume", I can hear sound directly
from input to the outputs.
--- Lars-Peter Clausen 2011-11-14 01:27:00
The same setup works fine here. Please check your physical connections:
http://wiki.analog.com/resources/tools-software/linux-drivers/sound/adau1361#hardware_configuration
Does it record an empty file or or a file filled with silence?
Does the number of SPORT RX interrupts change in /proc/interrupts during
record?
--- Vivi Li 2011-11-14 22:03:54
It finally works after I re-connect J6-2 to P6-8.
Thanks Lars.
Close this bug.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.config.audio_adau1361 application/octet-stream 51310 Vivi Li
config.linux.audio_adau1361 application/octet-stream 37028 Vivi Li