[#6848] Can not detect ad1836 on bf533-stamp in latest trunk
Submitted By: Vivi Li
Open Date
2011-10-26 03:46:42 Close Date
2012-01-16 01:59:47
Priority:
Medium Assignee:
Scott Jiang
Status:
Closed Fixed In Release:
N/A
Found In Release:
2011R1 Release:
Category:
N/A Board:
Processor:
BF533 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2011R1-RC2
App binary format:
FDPIC
Summary: Can not detect ad1836 on bf533-stamp in latest trunk
Details:
Can not detect ad1836 on bf533-stamp in latest trunk.
BF537-STAMP is OK.
--
Linux version 3.0.0-ADI-2011R1-pre-svn10098 (test@ulinux77-533stamp-ad1836) (gcc version 4.3.5 (ADI-2011R1-RC2) ) #498 Tue Oct 21
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart0] enabled
early printk enabled on early_BFuart0
Limiting kernel memory to 56MB due to anomaly 05000263
Board Memory: 128MB
Kernel Managed Memory: 128MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x001492e8
rodata = 0x001492e8-0x001b2138
bss = 0x001b3000-0x001c329c
data = 0x001c329c-0x001d4000
stack = 0x001d2000-0x001d4000
init = 0x001d4000-0x0086a000
available = 0x0086a000-0x03800000
DMA Zone = 0x07e00000-0x08000000
Hardware Trace active and enabled
Boot Mode: 0
Reset caused by Software reset
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF533 Rev 0.3
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 497 MHz core clock and 82 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-back) in data cache
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 14224
Kernel command line: root=/dev/mtdblock0 rw clkin_hz=11059200 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 48120k/131072k RAM, (6744k init code, 1312k kernel code, 556k data, 2048k dma, 72292k reserved)
NR_IRQS:81
Configuring Blackfin Priority Driven Interrupts
console [ttyBF0] enabled, bootconsole disabled
Calibrating delay loop... 989.18 BogoMIPS (lpj=1978368)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 64 KB (51 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
stamp_init(): registering device resources
bio: create slab <bio-0> at 0
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc00500, dma channel@5
Advanced Linux Sound Architecture Driver Version 1.0.24.
Switching to clocksource bfin_cs_cycles
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
debug-mmrs: setting up Blackfin MMR debugfs
msgmni has been set to 93
io scheduler noop registered (default)
bfin-uart: Blackfin serial driver
bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 21) is a BFIN-UART
brd: module loaded
smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@fluxnic.net>
eth0: SMC91C11xFD (rev 1) at 20300300 IRQ 40 [nowait]
eth0: Ethernet addr: 00:e0:22:fe:07:5b
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
bfin-tdm bfin-tdm.0: no platform_data
ALSA device list:
No soundcards found.
TCP cubic registered
NET: Registered protocol family 17
rtc-bfin rtc-bfin: setting system clock to 1970-01-01 08:02:59 UTC (28979)
smc91x smc91x.0: eth0: link down
smc91x smc91x.0: eth0: link up, 100Mbps, full-duplex, lpa 0x45E1
IP-Config: Complete:
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf533-stamp, domain=, nis-domain=(none),
bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=
dma_alloc_init: dma_page @ 0x02874000 - 512 pages at 0x07e00000
Freeing unused kernel memory: 6744k freed
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - http://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.18.4 (2011-10-25 03:54:04 CST) hush - the humble shell
root:/> version
kernel: Linux release 3.0.0-ADI-2011R1-pre-svn10098, build #498 Tue Oct 25 03:56:23 CST 2011
toolchain: bfin-linux-uclibc-gcc release gcc version 4.3.5 (ADI-2011R1-RC2)
user-dist: release svn-10450, build #6338 Tue Oct 25 03:54:28 CST 2011
root:/>
Follow-ups
--- Scott Jiang 2011-10-27 23:34:46
fixed
--- Vivi Li 2012-01-16 02:28:13
AD1836 can be detected in trunk.
Close this bug.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.config.audio_ad1836 application/octet-stream 51955 Vivi Li
config.linux.audio_ad1836 application/octet-stream 34452 Vivi Li