[#6877] Fail to use wireless cf card on bf537-stamp in 2011r1 branch
Submitted By: Vivi Li
Open Date
2011-11-14 00:26:48 Close Date
2011-11-25 01:40:34
Priority:
Medium High Assignee:
steven miao
Status:
Closed Fixed In Release:
N/A
Found In Release:
2011R1 Release:
Category:
N/A Board:
Processor:
BF537 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Rejected
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2011R1-RC2
App binary format:
FLAT
Summary: Fail to use wireless cf card on bf537-stamp in 2011r1 branch
Details:
Fail to use wireless cf card on bf537-stamp in 2011r1 branch.
It passed in 2010r1 branch.
--
Linux version 3.0.8-ADI-2011R1-svn10227 (test@uclinux50-bf537-9960-1836) (gcc version 4.3.5 (ADI-2011R1-RC2) ) #12 Sun Nov 13 211
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart0] enabled
early printk enabled on early_BFuart0
Limiting kernel memory to 56MB due to anomaly 05000263
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x00162118
rodata = 0x00162118-0x001d1fb4
bss = 0x001d2000-0x001e1c7c
data = 0x001e1c7c-0x001f6000
stack = 0x001f4000-0x001f6000
init = 0x001f6000-0x009a2000
available = 0x009a2000-0x03800000
DMA Zone = 0x03f00000-0x04000000
Hardware Trace active and enabled
Boot Mode: 0
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF537 Rev 0.2
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 500 MHz core clock and 62 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-back) in data cache
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 14224
Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 46872k/65536k RAM, (7856k init code, 1412k kernel code, 592k data, 1024k dma, 7780k reserved)
NR_IRQS:146
Configuring Blackfin Priority Driven Interrupts
console [ttyBF0] enabled, bootconsole disabled
Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (34 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
stamp_init(): registering device resources
bio: create slab <bio-0> at 0
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc00500, dma channel@7
cfg80211: Calling CRDA to update world regulatory domain
Switching to clocksource bfin_cs_cycles
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
debug-mmrs: setting up Blackfin MMR debugfs
msgmni has been set to 91
io scheduler noop registered (default)
bfin-uart: Blackfin serial driver
bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART
brd: module loaded
bfin_mii_bus: probed
bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=11)@sclk=62MHz)
bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1
bfin_cf_pcmcia bfin_cf_pcmcia: Blackfin CompactFlash/PCMCIA Socket Driver
bfin_cf_pcmcia bfin_cf_pcmcia: : on irq 54
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
TCP cubic registered
NET: Registered protocol family 17
rtc-bfin rtc-bfin: setting system clock to 1970-01-01 00:09:32 UTC (572)
IP-Config: Complete:
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf537-stamp, domain=, nis-domain=(none),
bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=
dma_alloc_init: dma_page @ 0x0294b000 - 256 pages at 0x03f00000
Freeing unused kernel memory: 7856k freed
pcmcia_socket pcmcia_socket0: pccard: PCMCIA card inserted into slot 0
pcmcia 0.0: pcmcia: registering new device pcmcia0.0 (IRQ: 54)
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - http://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.18.4 (2011-11-13 20:56:50 CST) hush - the humble shell
root:/> PHY: 0:01 - Link is Up - 100/Full
root:/> version
kernel: Linux release 3.0.8-ADI-2011R1-svn10227, build #12 Sun Nov 13 21:38:25 CST 2011
toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-2011R1-RC2)
user-dist: release svn-10489, build #167 Sun Nov 13 21:37:46 CST 2011
root:/>
root:/> modprobe orinoco_cs
root:/> lsmod
Module Size Used by
orinoco_cs 4053 0
orinoco 47894 1 orinoco_cs
root:/> ifconfig
eth0 Link encap:Ethernet HWaddr 00:E0:22:FE:00:03
inet addr:10.100.4.50 Bcast:10.100.4.255 Mask:255.255.255.0
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:2 errors:0 dropped:0 overruns:0 frame:0
TX packets:1 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:120 (120.0 B) TX bytes:42 (42.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
root:/> dmesg |tail
PHY: 0:01 - Link is Up - 100/Full
orinoco 0.15 (David Gibson <hermes@gibson.dropbear.id.au>, Pavel Roskin <proski@gnu.org>, et al)
Follow-ups
--- steven miao 2011-11-23 22:12:21
it works in 2011R1, maybe it's a hardware issue
--- steven miao 2011-11-24 00:35:02
need Support Prism 2/2.5 chipset selected now
--- Vivi Li 2011-11-25 01:55:30
OK.
Close it.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.config.wireless application/octet-stream 52126 Vivi Li
config.linux.wireless application/octet-stream 37022 Vivi Li