[#6882] Can't use S24_LE format to record audio with adau1361 on bf537-stamp.
Submitted By: Vivi Li
Open Date
2011-11-15 01:22:05
Priority:
Medium Assignee:
Lars-Peter Clausen
Status:
Open Fixed In Release:
N/A
Found In Release:
2011R1 Release:
Category:
N/A Board:
Processor:
BF537 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2011R1-RC2
App binary format:
Summary: Can't use S24_LE format to record audio with adau1361 on bf537-stamp.
Details:
Can't use S24_LE format to record audio with adau1361 on bf537-stamp.
I found this on 2011r1 branch and 2011R1_ADAU. This bug looks similar to me as bug [#6739].
--
Linux version 3.0.8-ADI-2011R1-svn10227 (test@linux73-bf537-wt-adxl) (gcc version 4.3.5 (ADI-2011R1-RC2) ) #12 Tue Nov 15 11:58:1
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart0] enabled
early printk enabled on early_BFuart0
Limiting kernel memory to 56MB due to anomaly 05000263
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x0014fd50
rodata = 0x0014fd50-0x001bdf6c
bss = 0x001be000-0x001ce340
data = 0x001ce340-0x001e2000
stack = 0x001e0000-0x001e2000
init = 0x001e2000-0x0091d000
available = 0x0091d000-0x03800000
DMA Zone = 0x03e00000-0x04000000
Hardware Trace active and enabled
Boot Mode: 0
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF537 Rev 0.2
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 500 MHz core clock and 125 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-through) in data cache
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 14224
Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 47404k/65536k RAM, (7404k init code, 1339k kernel code, 585k data, 2048k dma, 6756k reserved)
NR_IRQS:146
Configuring Blackfin Priority Driven Interrupts
bfin-rtc: invalid date; resetting
console [ttyBF0] enabled, bootconsole disabled
Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (35 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
stamp_init(): registering device resources
bio: create slab <bio-0> at 0
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc00500, dma channel@7
i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400
Advanced Linux Sound Architecture Driver Version 1.0.24.
Switching to clocksource bfin_cs_cycles
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
debug-mmrs: setting up Blackfin MMR debugfs
msgmni has been set to 92
io scheduler noop registered (default)
bfin-uart: Blackfin serial driver
bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART
brd: module loaded
bfin_mii_bus: probed
bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)
bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
bfin-i2s bfin-i2s.0: dma rx:3 tx:4, err irq:45, regs:ffc00800
dma_alloc_init: dma_page @ 0x02971000 - 512 pages at 0x03e00000
asoc: adau-hifi <-> bfin-i2s.0 mapping ok
ALSA device list:
#0: bfin-eval-adau1x61
TCP cubic registered
NET: Registered protocol family 17
rtc-bfin rtc-bfin: setting system clock to 1970-01-01 07:05:47 UTC (25547)
IP-Config: Complete:
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf537-stamp, domain=, nis-domain=(none),
bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=
Freeing unused kernel memory: 7404k freed
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - http://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.18.4 (2011-11-15 11:56:11 CST) hush - the humble shell
root:/> PHY: 0:01 - Link is Up - 100/Full
root:/> arecord -f S24_LE -r 48000 -c 2 -t wav -d 5 wav
Recording WAVE 'wav' : Signed 24 bit Little Endian, Rate 48000 Hz, Stereo
sport status error: ROVF
...
Follow-ups
--- Lars-Peter Clausen 2011-11-15 03:57:16
Could this be a SPORT issue?
Do you know what the fix was for [#6739]?
--- Scott Jiang 2011-11-15 21:58:29
Hi Lars, it's caused by alsa config file. If you use aplay -v, you will find
plugins don't work.I have told Mark Brown to fix it, so you must modify all adau
config file in alsa lib.
--- Lars-Peter Clausen 2011-11-16 02:50:47
Scott, we don't have any adau config files. I think this is a problem with the
SPORT and 24bit playback/record.
--- Scott Jiang 2011-11-16 21:55:38
scott@scott-desktop:~/Projects/src/bf533/lib/alsa-lib/alsa-lib-1.0.24/src/conf/cards$
ls |grep ADAU
ADAU1361.conf
ADAU1371.conf
ADAU1373.conf
--- Lars-Peter Clausen 2011-11-17 12:55:33
oops. i was only searching for lower case adau, sorry.
But this bug is still a problem with the SPORT ASoC code.
--- Sonic Zhang 2011-11-25 02:38:19
Vivi update name in adau1361 alsa conf
--- Vivi Li 2011-12-02 04:06:36
Hi Lars,
The sound card name is too long and is cut to "bfin-eval-adau1". ALSA
plug-in will fail to work. Could you fix that?
root:/> cat /proc/asound/cards
0 [bfinevaladau1x6]: bfin-eval-adau1 - bfin-eval-adau1x61
bfin-eval-adau1x61
root:/>
In other boards such like ad1836, we have shorter name:
0 [bfinad1836 ]: bfin-ad1836 - bfin-ad1836
bfin-ad1836
--- Vivi Li 2011-12-15 02:43:42
Now device name is modify to eval-adau1x61 by Lars in 2011R1 branch. Accordingly
I update card name to eval-adau1x61 in alsa conf in 2011R1 branch.
0 [evaladau1x61 ]: eval-adau1x61 - eval-adau1x61
eval-adau1x61
root:/> cat /usr/share/alsa/cards/eval-adau1x61.conf
eval-adau1x61.pcm.default {
@args [ CARD ]
@args.CARD {
type string
}
type asym
playback.pcm {
type plug
slave.pcm {
@func concat
strings [ "dmix:CARD=" $CARD ]
capture.pcm {
strings [ "dsnoop:CARD=" $CARD ]
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.config.adau1361 application/octet-stream 51322 Vivi Li
config.linux.adau1361 application/octet-stream 37173 Vivi Li