[#6932] Fail to set bitrate to 1000000 in bf548-ezkit for can bus test
Submitted By: Vivi Li
Open Date
2011-12-23 02:04:31
Priority:
Medium Assignee:
steven miao
Status:
Open Fixed In Release:
N/A
Found In Release:
2011R1 Release:
Category:
N/A Board:
Processor:
BF548 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2011r1-rc2
App binary format:
Summary: Fail to set bitrate to 1000000 in bf548-ezkit for can bus test
Details:
Fail to set bitrate to 1000000 in bf548-ezkit for can bus test.
Bf537-STAMP can work.
--
Linux version 3.0.8-ADI-2011R1-svn10231 (test@linux73-bf537-wt-adxl) (gcc version 4.3.5 (ADI-2011R1-RC2) ) #87 Wed Nov 30 18:09:1
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart1] enabled
early printk enabled on early_BFuart1
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x001ab848
rodata = 0x001ab848-0x0023e518
bss = 0x0023f000-0x00252af0
data = 0x00252af0-0x0026e000
stack = 0x0026c000-0x0026e000
init = 0x0026e000-0x00ad0000
available = 0x00ad0000-0x03e00000
DMA Zone = 0x03e00000-0x04000000
Hardware Trace active and enabled
Boot Mode: 1
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF548 Rev 0.2
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 525 MHz core clock and 131 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
L2 SRAM : uncacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-through) in data cache
L2 SRAM : uncacheable in data cache
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 15748
Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart1,57600 console=tty0 console=ttyBF1,57600 if
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 51808k/65536k RAM, (8584k init code, 1706k kernel code, 778k data, 2048k dma, 612k reserved)
NR_IRQS:295
Configuring Blackfin Priority Driven Interrupts
console [ttyBF1] enabled, bootconsole disabled
Calibrating delay loop... 1044.48 BogoMIPS (lpj=2088960)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (41 KB free)
Blackfin L2 SRAM: 128 KB (128 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
ezkit_init(): registering device resources
bio: create slab <bio-0> at 0
SCSI subsystem initialized
spi spi0.2: Warning: SPI CPHA not set: Slave Select not under software control!
See Documentation/blackfin/bfin-spi-notes.txt
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc00500, dma channel@4
bfin-spi bfin-spi.1: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc02300, dma channel@5
i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc00700
i2c-bfin-twi i2c-bfin-twi.1: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc02200
Advanced Linux Sound Architecture Driver Version 1.0.24.
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
debug-mmrs: setting up Blackfin MMR debugfs
msgmni has been set to 101
io scheduler noop registered (default)
bf54x-lq043: FrameBuffer initializing...
dma_alloc_init: dma_page @ 0x02b09000 - 512 pages at 0x03e00000
bfin-uart: Blackfin serial driver
bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 48) is a BFIN-UART
bfin-otp: initialized
brd: module loaded
register bfin atapi driver
scsi0 : pata-bf54x
ata1: PATA max UDMA/66 irq 68
physmap platform flash device: 02000000 at 20000000
physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000089 Chip ID 0x00881e
Intel/Sharp Extended Query Table at 0x010A
Using buffer write method
Using auto-unlock on power-up/resume
cfi_cmdset_0001: Erase suspend on write enabled
Using physmap partition information
Creating 5 MTD partitions on "physmap-flash.0":
0x000000000000-0x000000080000 : "bootloader(nor)"
0x000000080000-0x000000480000 : "linux kernel(nor)"
0x000000480000-0x000000fe0000 : "file system(nor)"
0x000000fe0000-0x000000ff8000 : "config(nor)"
0x000000ff8000-0x000001000000 : "u-boot env(nor)"
m25p80 spi0.1: m25p16 (2048 Kbytes)
Creating 2 MTD partitions on "m25p80":
0x000000000000-0x000000080000 : "bootloader(spi)"
0x000000080000-0x000000200000 : "linux kernel(spi)"
BF5xx on-chip NAND FLash Controller Driver, Version 1.2 (c) 2007 Analog Devices, Inc.
bf5xx-nand bf5xx-nand.0: data_width=8, wr_dly=3, rd_dly=3
NAND device: Manufacturer ID: 0x20, Chip ID: 0xda (ST Micro NAND 256MiB 3,3V 8-bit)
Creating 3 MTD partitions on "NAND 256MiB 3,3V 8-bit":
0x000000000000-0x000000080000 : "bootloader(nand)"
0x000000080000-0x000000480000 : "linux kernel(nand)"
0x000000480000-0x000010000000 : "file system(nand)"
CAN device driver interface
smsc911x: Driver version 2008-10-21
smsc911x-mdio: probed
smsc911x smsc911x.0: eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1)
smsc911x smsc911x.0: eth0: MAC Address: 00:e0:22:fe:bf:4c
input: bf54x-keys as /devices/platform/bf54x-keys/input/input0
ata1.00: ATA-7: FUJITSU MHW2040AT, 0000000B, max UDMA/100
ata1.00: 78140160 sectors, multi 16: LBA
rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0
i2c /dev entries driver
bfin-wdt: initialized: timeout=20 sec (nowayout=0)
ata1.00: configured for UDMA/66
blk_queue_max_segments: set to minimum 1
scsi 0:0:0:0: Direct-Access ATA FUJITSU MHW2040A 0000 PQ: 0 ANSI: 5
ALSA device list:
No soundcards found.
TCP cubic registered
NET: Registered protocol family 17
sd 0:0:0:0: [sda] 78140160 512-byte logical blocks: (40.0 GB/37.2 GiB)
sd 0:0:0:0: [sda] Write Protect is off
can: controller area network core (rev 20090105 abi 8)
sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
rtc-bfin rtc-bfin: setting system clock to 1970-01-06 08:03:46 UTC (461026)
sda: sda1 sda2
sd 0:0:0:0: [sda] Attached SCSI disk
smsc911x smsc911x.0: eth0: SMSC911x/921x identified at 0x24000000, IRQ: 175
IP-Config: Complete:
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf548-ezkit, domain=, nis-domain=(none),
bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=
Freeing unused kernel memory: 8584k freed
_____________________________________
a8888b. / Welcome to the uClinux distribution \
d888888b. / _ _ \
8P"YP"Y88 / | | |_| __ __ (TM) |
8|o||o|88 _____/ | | _ ____ _ _ \ \/ / |
8' .88 \ | | | | _ \| | | | \ / |
8`._.' Y8. \ | |__ | | | | | |_| | / \ |
d/ `8b. \ \____||_|_| |_|\____|/_/\_\ |
dP . Y8b. \ For embedded processors including |
d8:' " `::88b \ the Analog Devices Blackfin /
d8" 'Y88b \___________________________________/
:8P ' :888
8a. : _a88P For further information, check out:
._/"Yaa_: .| 88P| - http://blackfin.uclinux.org/
\ YP" `| 8P `. - http://docs.blackfin.uclinux.org/
/ \.___.d| .' - http://www.uclinux.org/
`--..__)8888P`._.' jgs/a:f - http://www.analog.com/blackfin
Have a lot of fun...
BusyBox v1.18.4 (2011-11-30 18:07:05 CST) hush - the humble shell
root:/> version
kernel: Linux release 3.0.8-ADI-2011R1-svn10231, build #87 Wed Nov 30 18:09:20 CST 2011
toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-2011R1-RC2)
user-dist: release svn-10530, build #29 Wed Nov 30 18:08:32 CST 2011
root:/>
root:/> modprobe bfin-can
bfin_can bfin_can.0: bfin_can device registered(®_base=ffc02a00, rx_irq=54, tx_irq=55, err_irq=39, sclk=131250000)
bfin_can bfin_can.1: bfin_can device registered(®_base=ffc03200, rx_irq=77, tx_irq=78, err_irq=69, sclk=131250000)
root:/> lsmod
Module Size Used by
bfin_can 4524 0
root:/> ip link set can0 type can bitrate 1000000
bfin_can bfin_can.0: bitrate error 0.5%
bfin_can bfin_can.0: setting CLOCK=0x002b TIMING=0x0000
root:/> cansend can0 123#11223344
write: Network is down
Follow-ups
--- steven miao 2012-01-16 06:07:25
fixed in socket can, bit-timing calculate use first found bit rate prescaler
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.config.canbus application/octet-stream 52145 Vivi Li
config.linux.canbus application/octet-stream 43655 Vivi Li