[#6951] build camera kernel fails on 561-ezkit trunk
Submitted By: Mingquan Pan
Open Date
2012-01-12 02:23:47 Close Date
2012-02-21 02:20:30
Priority:
Medium Assignee:
Scott Jiang
Status:
Closed Fixed In Release:
N/A
Found In Release:
N/A Release:
Category:
N/A Board:
N/A
Processor:
BF561 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
2011r1-rc4
App binary format:
N/A
Summary: build camera kernel fails on 561-ezkit trunk
Details:
build camera kernel fails on 561-ezkit trunk.
CC arch/blackfin/kernel/irqchip.o^M
CC arch/blackfin/kernel/dma-mapping.o^M
CC arch/blackfin/mach-bf561/ints-priority.o^M
CC arch/blackfin/mach-bf561/dma.o^M
CC arch/blackfin/kernel/flat.o^M
LD arch/blackfin/mach-common/built-in.o^M
CC arch/blackfin/mach-bf561/coreb.o^M
CC arch/blackfin/mach-bf561/boards/ezkit.o^M
AS arch/blackfin/kernel/fixed_code.o^M
CC arch/blackfin/kernel/reboot.o^M
CC arch/blackfin/kernel/bfin_gpio.o^M
LD arch/blackfin/mach-bf561/built-in.o^M
CC arch/blackfin/kernel/cplb-nompu/cplbinit.o^M
arch/blackfin/mach-bf561/boards/ezkit.c:436: error: unknown field ‘type’ specified in initializer^M
arch/blackfin/mach-bf561/boards/ezkit.c:436: error: ‘PPI_TYPE_PPI’ undeclared here (not in a function)^M
arch/blackfin/mach-bf561/boards/ezkit.c:439: warning: initialization makes integer from pointer without a cast^M
make[2]: *** [arch/blackfin/mach-bf561/boards/ezkit.o] Error 1^M
make[1]: *** [arch/blackfin/mach-bf561/boards] Error 2^M
make[1]: *** Waiting for unfinished jobs....^M
CC arch/blackfin/kernel/cplb-nompu/cplbmgr.o^M
CC arch/blackfin/kernel/bfin_dma.o^M
CC arch/blackfin/kernel/exception.o^M
LD arch/blackfin/kernel/cplb-nompu/built-in.o^M
CC arch/blackfin/kernel/dumpstack.o^M
CC arch/blackfin/kernel/time-ts.o^M
CC arch/blackfin/kernel/binfmt_elf_fdpic.o^M
CC arch/blackfin/kernel/cplbinfo.o^M
Follow-ups
--- Mingquan Pan 2012-01-19 03:52:02
After kernel updating, the building error now changes to:
CC [M] drivers/media/common/tuners/xc5000.o^M
CC [M] fs/nfs/nfs2xdr.o^M
CC drivers/media/video/v4l2-device.o^M
CC [M] drivers/media/common/tuners/xc4000.o^M
drivers/media/video/v4l2-device.c: In function
‘v4l2_device_release_subdev_node’:^M
drivers/media/video/v4l2-device.c:201: error: incompatible types in
assignment^M
drivers/media/video/v4l2-device.c: In function
‘v4l2_device_register_subdev_nodes’:^M
drivers/media/video/v4l2-device.c:240: error: incompatible types in
assignment^M
drivers/media/video/v4l2-device.c:246: error: wrong type argument to unary
exclamation mark^M
drivers/media/video/v4l2-device.c:248: error: incompatible type for argument 1
of ‘video_unregister_device’^M
drivers/media/video/v4l2-device.c: In function
‘v4l2_device_unregister_subdev’:^M
drivers/media/video/v4l2-device.c:277: error: incompatible type for argument 1
of ‘video_unregister_device’^M
make[4]: *** [drivers/media/video/v4l2-device.o] Error 1^M
make[3]: *** [drivers/media/video] Error 2^M
make[3]: *** Waiting for unfinished jobs....^M
--- Scott Jiang 2012-02-10 04:02:33
fixed.
--- Mingquan Pan 2012-02-21 02:58:15
Yes, it builds ok now. Close.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found