[#6952] mount spi flash on bf526 ezbrd fail on trunk head
Submitted By: Mingquan Pan
Open Date
2012-01-12 03:23:26 Close Date
2012-01-17 05:00:08
Priority:
Medium Assignee:
Scott Jiang
Status:
Closed Fixed In Release:
N/A
Found In Release:
N/A Release:
Category:
N/A Board:
Processor:
BF526 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Assigned (Not Start)
Uboot version or rev.:
Toolchain version or rev.:
2011r1-rc4
App binary format:
Summary: mount spi flash on bf526 ezbrd fail on trunk head
Details:
mount spi flash on bf526 ezbrd fail on trunk head.
## Booting kernel from Legacy Image at 02000000 ...
Image Name: bf526-0.0-3.1.0-ADI-2012R1-pre-s
Created: 2012-01-10 8:31:08 UTC
Image Type: Blackfin Linux Kernel Image (gzip compressed)
Data Size: 2142309 Bytes = 2 MiB
Load Address: 00001000
Entry Point: 001ccca8
Verifying Checksum ... OK
Uncompressing Kernel Image ... OK
Starting Kernel at = 001ccca8
Linux version 3.1.0-ADI-2012R1-pre-svn10275 (test@uclinux81-bf526) (gcc version 4.3.5 (ADI-2011R1-RC4) ) #54 Tue Jan 10 16:31:00 CST 2012
register early platform devices
bootconsole [early_shadow0] enabled
bootconsole [early_BFuart1] enabled
early printk enabled on early_BFuart1
Board Memory: 64MB
Kernel Managed Memory: 64MB
Memory map:
fixedcode = 0x00000400-0x00000490
text = 0x00001000-0x0013c778
rodata = 0x0013c778-0x001a0c28
bss = 0x001a1000-0x001b1510
data = 0x001b1510-0x001c4000
stack = 0x001c2000-0x001c4000
init = 0x001c4000-0x003bd000
available = 0x003bd000-0x03f00000
DMA Zone = 0x03f00000-0x04000000
Hardware Trace active and enabled
Boot Mode: 1
Blackfin support (C) 2004-2010 Analog Devices, Inc.
Compiled for ADSP-BF526 Rev 0.0
Blackfin Linux support by http://blackfin.uclinux.org/
Processor Speed: 400 MHz core clock and 80 MHz System Clock
NOMPU: setting up cplb tables
Instruction Cache Enabled for CPU0
External memory: cacheable in instruction cache
Data Cache Enabled for CPU0
External memory: cacheable (write-back) in data cache
Built 1 zonelists in Zone order, mobility grouping off. Total pages: 16002
Kernel command line: root=/dev/mtdblock0 rw ip=10.100.4.50 earlyprintk=serial,uart1,57600 console=ttyBF1,57600 ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:bf526-ezbrd:eth0:off
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory available: 60076k/65536k RAM, (2020k init code, 1261k kernel code, 543k data, 1024k dma, 612k reserved)
NR_IRQS:159
Configuring Blackfin Priority Driven Interrupts
console [ttyBF1] enabled, bootconsole disabled
Calibrating delay loop... 792.57 BogoMIPS (lpj=1585152)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
Blackfin Scratchpad data SRAM: 4 KB
Blackfin L1 Data A SRAM: 16 KB (16 KB free)
Blackfin L1 Data B SRAM: 16 KB (16 KB free)
Blackfin L1 Instruction SRAM: 48 KB (41 KB free)
NET: Registered protocol family 16
Blackfin DMA Controller
ezbrd_init(): registering device resources
bio: create slab <bio-0> at 0
bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc00500, dma channel@7
i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
debug-mmrs: setting up Blackfin MMR debugfs
JFFS2 version 2.2. (NAND) 2001-2006 Red Hat, Inc.
msgmni has been set to 117
io scheduler noop registered (default)
bfin-uart: Blackfin serial driver
bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART
bfin-otp: initialized
brd: module loaded
physmap platform flash device: 00400000 at 20000000
physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000020 Chip ID 0x008815
Intel/Sharp Extended Query Table at 0x0039
cfi_cmdset_0001: Erase suspend on write enabled
Using physmap partition information
Creating 3 MTD partitions on "physmap-flash.0":
0x000000000000-0x000000040000 : "bootloader(nor)"
0x000000040000-0x000000200000 : "linux kernel(nor)"
0x000000200000-0x000000400000 : "file system(nor)"
m25p80 spi0.1: sst25wf040 (512 Kbytes)
Creating 2 MTD partitions on "m25p80":
0x000000000000-0x000000040000 : "bootloader(spi)"
0x000000040000-0x000000080000 : "linux kernel(spi)"
bfin_mii_bus: probed
bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=15)@sclk=80MHz)
bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1
TCP cubic registered
NET: Registered protocol family 17
dma_alloc_init: dma_page @ 0x023da000 - 256 pages at 0x03f00000
IP-Config: Complete:
device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,
host=bf526-ezbrd, domain=, nis-domain=(none),
...
BusyBox v1.18.4 (2012-01-09 23:57:38 CST) hush - the humble shell
root:/> versiPHY: 0:01 - Link is Up - 100/Full
on
kernel: Linux release 3.1.0-ADI-2012R1-pre-svn10275, build #54 Tue Jan 10 16:31:00 CST 2012
toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-2011R1-RC4)
user-dist: release svn-10617, build #637 Tue Jan 10 16:30:09 CST 2012
root:/> successful boot attempt
************** STEP 3: MTD test
cat /proc/mtd
dev: size erasesize name
mtd0: 00040000 00010000 "bootloader(nor)"
mtd1: 001c0000 00010000 "linux kernel(nor)"
mtd2: 00200000 00010000 "file system(nor)"
mtd3: 00040000 00001000 "bootloader(spi)"
mtd4: 00040000 00001000 "linux kernel(spi)"
root:/>
Case 1 ...PASS
************** STEP 4: Mount MTD
mount -t jffs2 /dev/mtdblock4 /mnt
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000000: 0xe10e instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000004: 0xe14e instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000008: 0xe10d instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x0000000c: 0xe14d instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000010: 0x6190 instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000014: 0x6001 instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000018: 0x3629 instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x0000001c: 0x3639 instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000020: 0x3c19 instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000024: 0xe300 instead
Further such events for this erase block will not be printed
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00001000: 0x9709 instead
...Further such events for this erase block will not be printed^M
Empty flash at 0x00033508 ends at 0x0003350c^M
Empty flash at 0x00033918 ends at 0x0003391c^M
Empty flash at 0x00033924 ends at 0x00033928^M
Empty flash at 0x00033980 ends at 0x00033988^M
Empty flash at 0x0003398c ends at 0x00033994^M
Empty flash at 0x00033998 ends at 0x0003399c^M
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00034000: 0x9178 instead^M
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00034008: 0x92e4 instead^M
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x0003400c: 0x0002 instead^M
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00034014: 0x8ad8 instead^M
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00034018: 0x92ec instead^M
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x0003401c: 0x9308 instead^M
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00034020: 0xa7a0 instead^M
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00034024: 0x9334 instead^M
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00034028: 0x0010 instead^M
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x0003402c: 0x0001 instead^M
Further such events for this erase block will not be printed^M
Cowardly refusing to erase blocks on filesystem with no valid JFFS2 nodes^M
empty_blocks 11, bad_blocks 0, c->nr_blocks 64^M
mount: mounting /dev/mtdblock4 on /mnt failed
Last passed time: 2011_Dec_11_16_22.
Uclinux-dist version: 10570.
Kernel verion: 10259, git-id: de8f67b314312a4bc9e5003ecde6c28a6be607bc
Case 2 ...FAIL
Follow-ups
--- Mingquan Pan 2012-01-17 05:28:51
The flash chip restore back to ok after doing flash erase on it. So close.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found