[#7074] build awg kernel stops at bfin_sport.c
Submitted By: Mingquan Pan
Open Date
2012-04-26 22:38:44 Close Date
2012-05-14 04:48:05
Priority:
Medium Assignee:
Aaron Wu
Status:
Closed Fixed In Release:
N/A
Found In Release:
N/A Release:
Category:
N/A Board:
N/A
Processor:
BF537 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
ADI-trunk/svn-5764
App binary format:
N/A
Summary: build awg kernel stops at bfin_sport.c
Details:
build awg kernel stops at bfin_sport.c.
LD usr/built-in.o^M
CC arch/blackfin/mach-bf537/boards/stamp.o^M
LD arch/blackfin/mach-bf537/boards/built-in.o^M
GZIP kernel/config_data.gz^M
CHK kernel/config_data.h^M
UPD kernel/config_data.h^M
CC kernel/configs.o^M
LD kernel/built-in.o^M
CC drivers/char/bfin_sport.o^M
drivers/char/bfin_sport.c: In function ‘sport_configure’:^M
drivers/char/bfin_sport.c:692: error: called object ‘"<3>"’ is not a function^M
drivers/char/bfin_sport.c:700: error: called object ‘"<3>"’ is not a function^M
drivers/char/bfin_sport.c: In function ‘bfin_sport_probe’:^M
drivers/char/bfin_sport.c:856: warning: format ‘%x’ expects type ‘unsigned int’, but argument 2 has type ‘struct miscdevice *’^M
make[3]: *** [drivers/char/bfin_sport.o] Error 1^M
make[2]: *** [drivers/char] Error 2^M
make[1]: *** [drivers] Error 2^M
make[1]: *** Waiting for unfinished jobs....^M
Follow-ups
--- Aaron Wu 2012-05-04 05:11:26
delet the redundant macro
--- Mingquan Pan 2012-05-14 05:47:56
It builds ok now. Close.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found