[#7153] build spi net device fails for no enc28j60_hw.h
Submitted By: Mingquan Pan
Open Date
2012-06-08 01:32:40 Close Date
2012-06-29 03:14:27
Priority:
Medium Assignee:
Bob Liu
Status:
Closed Fixed In Release:
N/A
Found In Release:
N/A Release:
Category:
N/A Board:
Processor:
BF537 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Fixed
Uboot version or rev.:
Toolchain version or rev.:
ADI-2012r1-beta1
App binary format:
Summary: build spi net device fails for no enc28j60_hw.h
Details:
build spi net device fails for no enc28j60_hw.h.
GZIP kernel/config_data.gz^M
CHK kernel/config_data.h^M
UPD kernel/config_data.h^M
CC kernel/configs.o^M
LD kernel/built-in.o^M
CC drivers/net/ethernet/microchip/enc28j60.o^M
CC drivers/net/enc28j60.o^M
drivers/net/enc28j60.c:32:25: error: enc28j60_hw.h: No such file or directory^M
drivers/net/enc28j60.c:75: error: ‘MAX_FRAMELEN’ undeclared here (not in a function)^M
drivers/net/enc28j60.c: In function ‘spi_read_buf’:^M
drivers/net/enc28j60.c:100: error: ‘ENC28J60_READ_BUF_MEM’ undeclared (first use in this function)^M
drivers/net/enc28j60.c:100: error: (Each undeclared identifier is reported only once^M
drivers/net/enc28j60.c:100: error: for each function it appears in.)^M
drivers/net/enc28j60.c: In function ‘spi_write_buf’:^M
drivers/net/enc28j60.c:128: error: ‘ENC28J60_WRITE_BUF_MEM’ undeclared (first use in this function)^M
drivers/net/enc28j60.c: In function ‘spi_read_op’:^M
drivers/net/enc28j60.c:151: error: ‘SPRD_MASK’ undeclared (first use in this function)^M
drivers/net/enc28j60.c:154: error: ‘ADDR_MASK’ undeclared (first use in this function)^M
drivers/net/enc28j60.c: In function ‘spi_write_op’:^M
drivers/net/enc28j60.c:173: error: ‘ADDR_MASK’ undeclared (first use in this function)^M
drivers/net/enc28j60.c: In function ‘enc28j60_soft_reset’:^M
drivers/net/enc28j60.c:187: error: ‘ENC28J60_SOFT_RESET’ undeclared (first use in this function)^M
drivers/net/enc28j60.c: In function ‘enc28j60_set_bank’:^M
drivers/net/enc28j60.c:198: error: ‘BANK_MASK’ undeclared (first use in this function)^M
drivers/net/enc28j60.c:203: error: ‘EIE’ undeclared (first use in this function)^M
drivers/net/enc28j60.c:203: error: ‘ECON1’ undeclared (first use in this function)^M
drivers/net/enc28j60.c:207: error: ‘ECON1_BSEL0’ undeclared (first use in this function)^M
drivers/net/enc28j60.c:209: error: ‘ENC28J60_BIT_FIELD_SET’ undeclared (first use in this function)^M
drivers/net/enc28j60.c:212: error: ‘ENC28J60_BIT_FIELD_CLR’ undeclared (first use in this function)^M
drivers/net/enc28j60.c:215: error: ‘ECON1_BSEL1’ undeclared (first use in this function)^M
drivers/net/enc28j60.c: In function ‘nolock_reg_bfset’:^M
drivers/net/enc28j60.c:244: error: ‘ENC28J60_BIT_FIELD_SET’ undeclared (first use in this function)^M
drivers/net/enc28j60.c: In function ‘nolock_reg_bfclr’:^M
drivers/net/enc28j60.c:262: error: ‘ENC28J60_BIT_FIELD_CLR’ undeclared (first use in this function)^M
drivers/net/enc28j60.c: In function ‘nolock_regb_read’:^M
drivers/net/enc28j60.c:280: error: ‘ENC28J60_READ_CTRL_REG’ undeclared (first use in this function)^M
Follow-ups
--- Scott Jiang 2012-06-15 02:51:50
Kernel update issue. Bob will take a look at it.
--- Bob Liu 2012-06-18 05:03:58
fixed
--- Vivi Li 2012-06-29 04:15:01
OK now.
Close it.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
No Files Were Found