[#7169] bonnie++ test may fail with atapi on bf548-ezkit
Submitted By: Vivi Li
Open Date
2012-06-26 03:57:56 Close Date
2012-09-04 05:37:18
Priority:
Medium Assignee:
Sonic Zhang
Status:
Closed Fixed In Release:
N/A
Found In Release:
N/A Release:
Category:
N/A Board:
EZKIT Lite
Processor:
BF548 Silicon Revision:
Is this bug repeatable?:
Yes Resolution:
Rejected
Uboot version or rev.:
Toolchain version or rev.:
gcc4.3-2012_Feb_15
App binary format:
Summary: bonnie++ test may fail with atapi on bf548-ezkit
Details:
bonnie++ test may fail with atapi on bf548-ezkit.
Bellow is the log from regression machine:
--
mount /dev/sda2 /mnt/hd2
root:/> time bonnie++ -u root -d /mnt/hd2 -s 200M
Using uid:0, gid:0.
Writing a byte at a time...ata1: lost interrupt (Status 0x50)
ata1.00: exception Emask 0x0 SAct 0x0 SErr 0x0 action 0x6 frozen
ata1.00: failed command: WRITE DMA
ata1.00: cmd ca/00:08:fc:08:fa/00:00:00:00:00/e0 tag 0 dma 4096 out
res 40/00:00:00:00:00/00:00:00:00:00/00 Emask 0x4 (timeout)
ata1.00: status: { DRDY }
ata1: soft resetting link
ata1.00: configured for UDMA/66
ata1.00: device reported invalid CHS sector 0
ata1: EH complete
ata1: lost interrupt (Status 0x50)
done
Writing intelligently...done
Rewriting...attempt to access beyond end of device
sda2: rw=0, want=134744080, limit=40965750
attempt to access beyond end of device
Boatite mpat itoI a ccres s eberyoende e)nd of device
: sndat2:u ruw=e0,o w
ant=134744080, limit=40965750
Bellow is my result by manul test:
root:/> time bonnie++ -u root -d /mnt/ -s 50M
Rewriting...done
Reading a byte at a time...done
Reading intelligently...done
start 'em...done...EXT2-fs (sda2): error: ext2_check_page: bad entry in directory #2: : rec_len is smaller than minimal - offset0
done...done...done...done...
Create files in sequential order...Can't make directory ./Bonnie.327
Cleaning up test directory after error.
Bonnie: drastic I/O error (rmdir): No such file or directory
Command exited with non-zero status 1
real 2m 26.02s
user 0m 15.29s
sys 1m 27.01s
root:/>
Follow-ups
--- Vivi Li 2012-07-04 02:53:40
Add a patch in build script to change BFIN_MAX_SG_SEGMENTS to 1 in bf54x atapi
driver. Check later to see the result.
--- Vivi Li 2012-07-27 03:01:49
This bug still exists after this patch is applied. So revert this patch as it's
not useful.
U-boot is updated to latest and this bug seems to disappear after 90 rounds of
test. Though bonnie++ failed 5 times with different error. It simply hangs in
the middle of bonnie++ and kernel reboots.
--- Vivi Li 2012-09-04 06:35:21
This bug disappeared after I replaced the power supply of bf548-ezkit in
regression machine.
Power problem, not a bug. So close it.
Files
Changes
Commits
Dependencies
Duplicates
Associations
Tags
File Name File Type File Size Posted By
config.config.atapi_hd application/octet-stream 51589 Vivi Li
config.linux.atapi_hd application/octet-stream 45757 Vivi Li