Article [#3820] Kernel can't wake up from standby mode when cause Wakeup event by SIC_IWR value.

[#3820] Kernel can't wake up from standby mode when cause Wakeup event by SIC_IWR value.

Submitted By: Vivi Li

Open Date

2008-01-08 00:41:46     Close Date

2008-01-23 02:48:35

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

toolchain 4.1-2007_Nov_27

App binary format:

N/A     

Summary: Kernel can't wake up from standby mode when cause Wakeup event by SIC_IWR value.

Details:

Build kernel with default options, in which Power Management is enabled and cause Wakeup Event by SIC_IWR value.

It can't wake up from standby mode.

Below is the log:

----

root:~> echo 'standby' > /sys/power/state

echo 'standby' > /sys/power/state

Stopping tasks ... done.

Suspending console(s)

----

For BF533-EZKIT/BF533-STAMP, the same problem happens.

For BF561-EZKIT, Power Management is not supported and kernel building fails with Power Management enabled.

Follow-ups

--- Sonic Zhang                                              2008-01-17 03:39:54

Fixed.

Only RTC interrupt can wake up deeper sleep core.

--- Vivi Li                                                  2008-01-23 04:51:28

For BF533-EZKIT and BF533-STAMP, set SIC_IWR to 0x80, tests pass.

For BF537-EZKIT, set SIC_IWR to 0x8, tests pass.

So close this bug.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.