Article [#3849] SPI mmc driver can't auto create entrys of spi_mmc1 and spi_mmc2 in /sys/block/spi_mmc/ after system reboot

[#3849] SPI mmc driver can't auto create entrys of spi_mmc1 and spi_mmc2 in /sys/block/spi_mmc/ after system reboot

Submitted By: Vivi Li

Open Date

2008-01-23 00:17:19     Close Date

2008-03-17 02:33:13

Priority:

Medium High     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

2007_Oct_07

App binary format:

N/A     

Summary: SPI mmc driver can't auto create entrys of spi_mmc1 and spi_mmc2 in /sys/block/spi_mmc/ after system reboot

Details:

There are two folders (spi_mmc1/spi_mmc2) in /sys/block/spi_mmc/ when two partitions have been made in MMC card by fdisk.

Then reboot kernel.

There is no such folder in /sys/block/spi_mmc/ unless command "fdisk /dev/spi_mmc" is executed. They should be created automatically by driver when kernel boot up.

No such bug in 2007R1 release.

Below is the log after system reboot:

--

root:/> ls /sys/block/

ram0     ram11    ram14    ram3     ram6     ram9

ram1     ram12    ram15    ram4     ram7     spi_mmc

ram10    ram13    ram2     ram5     ram8

root:/> ls /sys/block/spi_mmc/

capability  holders     range       size        stat        uevent

dev         queue       removable   slaves      subsystem

root:/> fdisk /dev/spi_mmc

spi_mmc: spi_mmc1 spi_mmc2

The number of cylinders for this disk is set to 2045.

There is nothing wrong with that, but this is larger than 1024,

and could in certain setups cause problems with:

1) software that runs at boot time (e.g., old versions of LILO)

2) booting and partitioning software from other OSs

   (e.g., DOS FDISK, OS/2 FDISK)

Command (m for help): p

Disk /dev/spi_mmc: 8 heads, 62 sectors, 2045 cylinders

Units = cylinders of 496 * 512 bytes

       Device Boot    Start       End    Blocks   Id  System

/dev/spi_mmc1             1      1033    256153   83  Linux

/dev/spi_mmc2          1034      2045    250976   83  Linux

Command (m for help): q

root:/> ls /sys/block/spi_mmc/

capability  queue       size        spi_mmc2    uevent

dev         range       slaves      stat

holders     removable   spi_mmc1    subsystem

root:/>

--

Follow-ups

--- Sonic Zhang                                              2008-03-11 00:07:32

Graf,

could you also take a look?

--- Graf Yang                                                2008-03-13 06:50:36

Fixed this bug in 2008R1 and Trunk.

When probing the spi_mmc driver, we should firstly validate the card then call

add_disk(). The original code use schedule_work(&pdev->cd_ws) to call

spi_mmc_revalidate(), this can't ensure the validation work have been done

before add_disk().

--- Vivi Li                                                  2008-03-17 02:33:12

OK now. Close it. Thanks!

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.