Article [#3857] ndso on bf533 fails for low stack size

[#3857] ndso on bf533 fails for low stack size

Submitted By: Mingquan Pan

Open Date

2008-01-24 21:28:04     Close Date

2008-02-21 05:34:31

Priority:

Medium     Assignee:

Michael Hennerich

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

08r1-6

App binary format:

N/A     

Summary: ndso on bf533 fails for low stack size

Details:

ndso on bf533 fails for low stack size.

root:/> ndso &

103

root:/> Data access misaligned address violation

- Attempted misaligned data memory or data cache access.

Defered Exception context

CURRENT PROCESS:

COMM=ndso PID=103

TEXT = 0x03240040-0x0324f3e0  DATA = 0x0324f3e4-0x032527f4

BSS = 0x032527f4-0x03252f14   USER-STACK = 0x03254f84

return address: [0x0324a562]; contents of:

0x0324a540:  ffff  6ff0  e580  fffe  6181  0808  1032  0000

0x0324a550:  0000  e580  ffff  3220  e120  0063  3248  6ff9

0x0324a560:  5aac [9112] 0a02  17e9  c080  1813  c683  5180

0x0324a570:  c111  8613  c111  981a  c683  1180  c40b  0200

SEQUENCER STATUS:               Not tainted

SEQSTAT: 00002024  IPEND: 0030  SYSCFG: 0006

  HWERRCAUSE: 0x0

  EXCAUSE   : 0x24

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x037d4000> /* unknown address */

RETX: <0x0324a562> [ ndso + 0xa522 ]

RETS: <0x0324a5e2> [ ndso + 0xa5a2 ]

PC  : <0x0324a562> [ ndso + 0xa522 ]

DCPLB_FAULT_ADDR: <0x03252e5c> [ ndso + 0x12e5c ]

ICPLB_FAULT_ADDR: <0x0324a562> [ ndso + 0xa522 ]

PROCESSOR STATE:

R0 : 00000063    R1 : 0000076c    R2 : 000000be    R3 : 66666667

R4 : 032403a8    R5 : 00000000    R6 : 0000003f    R7 : 0000003f

P0 : 03252dce    P1 : 03252dcd    P2 : 03252e5d    P3 : 032524c8

P4 : 00000025    P5 : 03252e38    FP : 03250c0c    SP : 037d3f24

LB0: 03248551    LT0: 0324854e    LC0: 00000000

LB1: 03247a35    LT1: 03247a34    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 03250b11

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 032524c8

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 000002f8   A0.x: 00000000   A1.w: 000002f8   A1.x: 00000000

USP : 03250c00  ASTAT: 02000002

Hardware Trace:

   0 Target : <0x00004814> { _trap_c + 0x0 }

     Source : <0xffa00774> { _exception_to_level5 + 0xb4 }

   1 Target : <0xffa006c0> { _exception_to_level5 + 0x0 }

     Source : <0xffa0061c> { _ex_trap_c + 0x5c }

   2 Target : <0xffa005c0> { _ex_trap_c + 0x0 }

     Source : <0xffa00814> { _trap + 0x28 }

   3 Target : <0xffa007ec> { _trap + 0x0 }

     Source : <0x0324a560> [ ndso + 0xa520 ]

   4 Target : <0x0324a552> [ ndso + 0xa512 ]

     Source : <0x0324a536> [ ndso + 0xa4f6 ]

   5 Target : <0x0324a4d6> [ ndso + 0xa496 ]

     Source : <0x0324a5e2> [ ndso + 0xa5a2 ]

   6 Target : <0x0324a5e2> [ ndso + 0xa5a2 ]

     Source : <0x03248554> [ ndso + 0x8514 ]

   7 Target : <0x03248546> [ ndso + 0x8506 ]

     Source : <0x03248516> [ ndso + 0x84d6 ]

   8 Target : <0x0324850c> [ ndso + 0x84cc ]

     Source : <0x0324a5de> [ ndso + 0xa59e ]

   9 Target : <0x0324a5ca> [ ndso + 0xa58a ]

     Source : <0x0324a4d2> [ ndso + 0xa492 ]

  10 Target : <0x0324a4cc> [ ndso + 0xa48c ]

     Source : <0x0324a5fa> [ ndso + 0xa5ba ]

  11 Target : <0x0324a5fa> [ ndso + 0xa5ba ]

     Source : <0x03248554> [ ndso + 0x8514 ]

  12 Target : <0x03248546> [ ndso + 0x8506 ]

     Source : <0x03248516> [ ndso + 0x84d6 ]

  13 Target : <0x0324850c> [ ndso + 0x84cc ]

     Source : <0x0324a5f6> [ ndso + 0xa5b6 ]

  14 Target : <0x0324a5e4> [ ndso + 0xa5a4 ]

     Source : <0x0324a4c6> [ ndso + 0xa486 ]

  15 Target : <0x0324a4c2> [ ndso + 0xa482 ]

     Source : <0x03248554> [ ndso + 0x8514 ]

Stack from 037d3f04:

        00011178 ffa00778 0014256c 0014256c 00142568 00000003 032403a8 03245e56

        0324a562 00000030 00002024 00000000 037d4000 0324a562 0324a562 0324a5e2

        00000063 02000002 03247a35 03248551 03247a34 0324854e 00000000 00000000

        000002f8 00000000 000002f8 00000000 00000000 00000000 00000000 00000000

        00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

        00000000 00000000 032524c8 03250b11 03250c00 03250c0c 03252e38 00000025

Call Trace:

                                                                                                                                                          

test@linux:~/checkouts/test_suites.1026> bfin-uclinux-flthdr -p ndso

ndso

    Magic:        bFLT

    Rev:          4

    Build Date:   Fri Jan 25 08:55:08 2008

    Entry:        0x44

    Data Start:   0xf3e0

    Data End:     0x127f0

    BSS End:      0x12f10

    Stack Size:   0x4000

    Reloc Start:  0x127f0

    Reloc Count:  0x756

    Flags:        0x1 ( Load-to-Ram )

If the size rises to 0x7530 by :

test@linux:~/checkouts/test_suites.1026> bfin-uclinux-flthdr -s30000 ndso

test@linux:~/checkouts/test_suites.1026> bfin-uclinux-flthdr -p ndso

ndso

    Magic:        bFLT

    Rev:          4

    Build Date:   Fri Jan 25 08:55:08 2008

    Entry:        0x44

    Data Start:   0xf3e0

    Data End:     0x127f0

    BSS End:      0x12f10

    Stack Size:   0x7530

    Reloc Start:  0x127f0

    Reloc Count:  0x756

    Flags:        0x1 ( Load-to-Ram )

then the case is ok.

But on bf537, 0x4000 is ok.

Follow-ups

--- Michael Hennerich                                        2008-02-07 07:26:18

Fixed

-Michael

--- Mingquan Pan                                             2008-02-21 05:34:30

Yes,close.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.