Article [#3960] When generate a file into ext2 fs on one specific SD card on BF548-EZKIT, there will be data transferring error

[#3960] When generate a file into ext2 fs on one specific SD card on BF548-EZKIT, there will be data transferring error

Submitted By: Vivi Li

Open Date

2008-03-06 04:55:45    

Priority:

Very Low     Assignee:

Nobody

Status:

Open     Fixed In Release:

N/A

Found In Release:

2008R1-RC8     Release:

Category:

N/A     Board:

N/A

Processor:

BF548     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

N/A

Uboot version or rev.:

    Toolchain version or rev.:

08r1-8

App binary format:

N/A     

Summary: When generate a file into ext2 fs on one specific SD card on BF548-EZKIT, there will be data transferring error

Details:

When generate a file on SD card through SDIOMMC port on BF548-EZKIT, there will be data transferring error 2.

No such error message for MMC card.

Below is the log:

--

root:/> echo 100 > /proc/sys/vm/pagecache_ratio

root:/> mount -t ext2 /dev/mmcblk0p1 /mnt/

root:/> umount /mnt/

root:/> mount -t ext2 -o sync /dev/mmcblk0p1 /mnt/

root:/> time dd if=/dev/zero of=/mnt/10.bin bs=1M count=10

mmcblk0: error 2 transferring data

mmcblk0: error 2 transferring data

mmcblk0: error 2 transferring data

mmcblk0: error 2 transferring data

mmcblk0: error 2 transferring data

mmcblk0: error 2 transferring data

mmcblk0: error 2 transferring data

mmcblk0: error 2 transferring data

mmcblk0: error 2 transferring data

mmcblk0: error 2 transferring data

mmcblk0: error 2 transferring data

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8201

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8208

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8213

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8215

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8218

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8221

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8229

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8237

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8240

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8245

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8247

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8250

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8253

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8261

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8269

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8272

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8277

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8279

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8282

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8285

EXT2-fs error (device mmcblk0p1): ext2_new_block: Allocating block in system zone - block = 8321

mmcblk0: error 2 transferring data

mmcblk0: error 2 transferring data

mmcblk0: error 2 transferring data

mmcblk0: error 2 transferring data

10+0 records in

10+0 records out

real    0m 29.67s

user    0m 0.00s

sys     0m 0.76s

root:/>

--

Follow-ups

--- Vivi Li                                                  2008-03-06 05:00:43

This error message "mmcblk0: error 2 transferring data" only appears

for ext2 fs.

--- Cliff Cai                                                2008-03-17 03:10:11

It's ok on v1.3 BF548.

Cliff

--- Vivi Li                                                  2008-03-19 03:34:40

Now only a 1GB SD card from Transcend still have this problem.

--- Cliff Cai                                                2008-03-25 23:32:43

The error number means a CRC error.After setting the bus-width to 1 bit the card

can work properly. So maybe you need to test more cards to see if the problem is

caused by sdh or card itself.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.