Article [#3985] my bf54x board can't be in low clocking

[#3985] my bf54x board can't be in low clocking

Submitted By: Meihui Fan

Open Date

2008-03-25 00:01:14     Close Date

2008-07-20 11:14:18

Priority:

High     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2008R1-RC8     Release:

svn trunk

Category:

Kernel Functions     Board:

Custom

Processor:

BF549     Silicon Revision:

0.0/0.1

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

svn trunk(1.1.6)     Toolchain version or rev.:

svn trunk(4.1.2)

App binary format:

N/A     

Summary: my bf54x board can't be in low clocking

Details:

Hi folks,

When I try to re-program clocks in low rate while kernel boots, it seems my bf54x board (customized reference to BF548-EZKIT) would hang or trigger double-fault exception. e.g.:

   --- Clock/PLL Setup                                                     

   (12000000) Crystal Frequency in Hz                                      

   [*] Re-program Clocks while Kernel boots?

   [ ]   Bypass PLL                                                        

   [ ]     Half Clock In                                                   

   (10)    VCO Multiplier                                                  

         Core Clock Divider (1)  --->                                      

   (2)   System Clock Divider

The board is clocking in 528/132 MHz from U-Boot.

I did many tests, and I believe the matter is the `System Clock Divider'. While the board works well on VCOM=44 and SCLKD=4, it involved in double-fault exception on VCOM=44 and SCLKD=12.

Follow-ups

--- Sonic Zhang                                              2008-03-28 06:19:46

Fixed.

--- Meihui Fan                                               2008-04-01 04:48:37

The latest svn trunk is still not works on my board...

How's going on the ezkit?

--- Robin Getz                                               2008-04-20 21:50:11

The DDR min speed specified by JEDEC is 84MHz - you have it set for 60.

-Robin

--- Robin Getz                                               2008-07-20 11:14:18

Closing since it seems to be fixed, and no comments in months.

-Robin

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.