Article [#4015] portmap needs to port to nommu too

[#4015] portmap needs to port to nommu too

Submitted By: Mingquan Pan

Open Date

2008-04-07 04:14:47     Close Date

2009-03-02 05:28:22

Priority:

Medium     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2008R1.5-RC3     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

08r1-8

App binary format:

N/A     

Summary: portmap needs to port to nommu too

Details:

trunk portmap needs to port to nommu too.It also has  Function not implemented failure when executed.

The kernel info:

Linux version 2.6.24.3-ADI-2008R2-pre-svn4482 (test@uclinux51-ad9960-ad1836) (gcc version 4.1.2 (ADI svn)) #8 Mon Mar 24 23:24:41 CST 2008^

...

root:/> portmap &^M

portmap: fork: Function not implemented^M

128^M

ro

Follow-ups

--- Mike Frysinger                                           2008-04-07 04:20:22

just use the -f option in the meantime

--- Graf Yang                                                2008-04-17 08:31:42

As Mike have pointed out, we must use -f option to put it run on foreground.

Thus it will not call fork().

--- Graf Yang                                                2008-07-15 02:49:58

Could it be closed?

--- Mike Frysinger                                           2008-07-15 03:15:20

the question is whether to make the daemonize step work for no mmu, or just

force people to use -f

it doesnt particularly matter to me either way

--- Sonic Zhang                                              2008-07-15 22:20:11

-f is acceptable for NOMMU.

--- Jie Zhang                                                2009-06-01 03:29:04

I have committed a patch for portmap to enclose fork with NO_MMU macro.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.