Article [#4058] i2ctwi BFIN_TWIKEYPAD_IRQ_PFX has no value for bf527 ezkit on 08r1

[#4058] i2ctwi BFIN_TWIKEYPAD_IRQ_PFX has no value for bf527 ezkit on 08r1

Submitted By: Mingquan Pan

Open Date

2008-04-24 05:06:36     Close Date

2008-05-07 03:08:06

Priority:

Medium     Assignee:

Bryan Wu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

08r1-8

App binary format:

N/A     

Summary: i2ctwi BFIN_TWIKEYPAD_IRQ_PFX has no value for bf527 ezkit on 08r1

Details:

i2ctwi BFIN_TWIKEYPAD_IRQ_PFX has no value for bf527 ezkit on 08r1.

In linux-2.6.x/drivers/input/misc/Kconfig of 08r1, there is:

config BFIN_TWIKEYPAD_IRQ_PFX

        int "IRQ"

        depends on (BLACKFIN && TWI_KEYPAD)

        default "72" if BFIN537_STAMP

        default "39" if BFIN533_STAMP

        default "212" if BFIN548_EZKIT

        help

          Choose an GPIO as Keypad interrupt [33..120]

No value set to BFIN527_EZKIT.

Follow-ups

--- Bryan Wu                                                 2008-04-30 03:11:14

It was fixed in trunk and 2008R1 branch.

-Bryan

--- Mingquan Pan                                             2008-05-07 03:08:06

Yed,close.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.