Article [#4090] XIP can't work in flash

[#4090] XIP can't work in flash

Submitted By: Vivi Li

Open Date

2008-05-07 03:34:32     Close Date

2010-02-10 03:47:16

Priority:

Medium     Assignee:

Bernd Schmidt

Barry Song

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

08r1-rc8

App binary format:

N/A     

Summary: XIP can't work in flash

Details:

XIP can not work properly in parallel nor flash. Root was mounted as romfs, but it failed after dma_alloc_init.

XIP(ROMFS_FS) and parallel nor flash are enabled in kernel, and ramfs is disabled. Disable other unrelated options to reduce size.

The process is to write rootfs.romfs into flash and run kernel vmImage with bootargs "root=/dev/mtdblock2 rootfstype=romfs ro". Both formats of fdpic and shared-flat in bf537-stamp are tested.

Kernel and user configs of fdpic format are attached.

Bellow is the log with fdpic format:

--

bfin> tftp 0x1000000 rootfs.romfs

Using Blackfin EMAC device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'rootfs.romfs'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #############################################################

done

Bytes transferred = 2638848 (284400 hex)

bfin> protect off 0x20120000 0x203effff

............................................. done

Un-Protected 45 sectors

bfin> erase 0x20120000 0x203effff

............................................. done

Erased 45 sectors

bfin> cp.b 0x1000000 0x20120000 0x284400

Copy to Flash... done

bfin> tftp 0x1000000 vmImage

Using Blackfin EMAC device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'vmImage'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         ######################################

done

Bytes transferred = 859644 (d1dfc hex)

bfin> set bootargs root=/dev/mtdblock2 rootfstype=romfs ro

bfin> bootm 0x1000000

## Booting image at 01000000 ...

   Image Name:   Linux-2.6.24.5-ADI-2008R2-pre-sv

   Created:      2008-05-07   6:12:38 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    859580 Bytes = 839.4 kB

   Load Address: 00001000

   Entry Point:  00172000

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 172000

Linux version 2.6.24.5-ADI-2008R2-pre-svn4705 (test@Linux165-ViviLi) (gcc version 4.1.2 (ADI svn)) 8

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001044d0

  rodata    = 0x00104600-0x001507b4

  bss       = 0x001507c0-0x0015ea84

  data      = 0x0015ea84-0x00172000

    stack   = 0x00170000-0x00172000

  init      = 0x00172000-0x0018d000

  available = 0x0018d000-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Blackfin support (C) 2004-2008 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 100 MHz System Clock

NOMPU: setting up cplb tables for global access

Instruction Cache Enabled

Data Cache Enabled (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14224

Kernel command line: root=/dev/mtdblock2 rootfstype=romfs ro

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console [ttyBF0] enabled

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 55172k/65536k RAM, (108k init code, 1037k kernel code, 439k data, 1024k dma, 7756)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin Data A SRAM: 16 KB (15 KB free)

Blackfin Data B SRAM: 16 KB (16 KB free)

Blackfin Instruction SRAM: 48 KB (41 KB free)

Security Framework initialized

Mount-cache hash table entries: 512

net_namespace: 64 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

ROMFS MTD (C) 2006 Red Hat, Inc.

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

RAMDISK driver initialized: 16 RAM disks of 4096K size 1024 blocksize

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(md)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

physmap platform flash device: 00400000 at 20000000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank

Amd/Fujitsu Extended Query Table at 0x0040

number of CFI chips: 1

cfi_cmdset_0002: Disabling erase-suspend-program due to code brokenness.

RedBoot partition parsing not available

Using physmap partition information

Creating 4 MTD partitions on "physmap-flash.0":

0x00000000-0x00040000 : "Bootloader"

0x00040000-0x00120000 : "Kernel"

0x00120000-0x003f0000 : "RootFS"

0x003f0000-0x00400000 : "MAC Address"

bfin-spi bfin-spi.0: Blackfin BF5xx on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500,7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 10:27:39 UTC (37659)

ROMFS: Mounting image 'rom 48214880'

VFS: Mounted root (romfs filesystem) readonly.

Freeing unused kernel memory: 108k freed

dma_alloc_init: dma_page @ 0x0018a000 - 256 pages at 0x03f00000

Unable to load executable

Kernel panic - not syncing: No init found.  Try passing init= option to kernel.

--

Bellow is the process and log with shared-flat format:

--

bfin> tftp 0x1000000 rootfs.romfs

Using Blackfin EMAC device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'rootfs.romfs'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #######

done

Bytes transferred = 2360320 (240400 hex)

bfin> protect off 0x20120000 0x203effff

............................................. done

Un-Protected 45 sectors

bfin> erase 0x20120000 0x203effff

............................................. done

Erased 45 sectors

bfin> cp.b 0x1000000 0x20120000 0x240400

Copy to Flash... done

bfin> tftp 0x1000000 vmImage

Using Blackfin EMAC device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'vmImage'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #######################################

done

Bytes transferred = 860292 (d2084 hex)

bfin> set bootargs root=/dev/mtdblock2 rootfstype=romfs ro

bfin> bootm

## Booting image at 01000000 ...

   Image Name:   Linux-2.6.24.5-ADI-2008R2-pre-sv

   Created:      2008-05-06   9:59:43 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    860228 Bytes = 840.1 kB

   Load Address: 00001000

   Entry Point:  00172000

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 172000

Linux version 2.6.24.5-ADI-2008R2-pre-svn4705 (test@Linux165-ViviLi) (gcc version 4.1.2 (ADI svn)) 8

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001044d0

  rodata    = 0x00104600-0x001509f4

  bss       = 0x00150a00-0x0015ecc4

  data      = 0x0015ecc4-0x00172000

    stack   = 0x00170000-0x00172000

  init      = 0x00172000-0x0018d000

  available = 0x0018d000-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Reset caused by Software reset

Blackfin support (C) 2004-2008 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 100 MHz System Clock

NOMPU: setting up cplb tables for global access

Instruction Cache Enabled

Data Cache Enabled (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14224

Kernel command line: root=/dev/mtdblock2 rootfstype=romfs ro

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console [ttyBF0] enabled

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 55172k/65536k RAM, (108k init code, 1037k kernel code, 439k data, 1024k dma, 7756)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin Data A SRAM: 16 KB (15 KB free)

Blackfin Data B SRAM: 16 KB (16 KB free)

Blackfin Instruction SRAM: 48 KB (41 KB free)

Security Framework initialized

Mount-cache hash table entries: 512

net_namespace: 64 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

ROMFS MTD (C) 2006 Red Hat, Inc.

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

RAMDISK driver initialized: 16 RAM disks of 4096K size 1024 blocksize

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(md)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

physmap platform flash device: 00400000 at 20000000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank

Amd/Fujitsu Extended Query Table at 0x0040

number of CFI chips: 1

cfi_cmdset_0002: Disabling erase-suspend-program due to code brokenness.

RedBoot partition parsing not available

Using physmap partition information

Creating 4 MTD partitions on "physmap-flash.0":

0x00000000-0x00040000 : "Bootloader"

0x00040000-0x00120000 : "Kernel"

0x00120000-0x003f0000 : "RootFS"

0x003f0000-0x00400000 : "MAC Address"

bfin-spi bfin-spi.0: Blackfin BF5xx on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500,7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 10:56:23 UTC (39383)

ROMFS: Mounting image 'rom 48202c4b'

VFS: Mounted root (romfs filesystem) readonly.

Freeing unused kernel memory: 108k freed

dma_alloc_init: dma_page @ 0x0018a000 - 256 pages at 0x03f00000

Unable to mmap process text, errno 38

Kernel panic - not syncing: No init found.  Try passing init= option to kernel.

--

The error messages are from binfmt_flat.c and binfmt_elf_fdpic.c in linux-2.6.x/fs/.

Follow-ups

--- Mike Frysinger                                           2008-09-25 02:11:15

you have to disable CONFIG_ROMFS_MTD_FS and then it'll work fine ... ive updated

the docs:

  docs.blackfin.uclinux.org/doku.php?id=linux-kernel:xip

--- Bernd Schmidt                                            2008-09-25 05:01:19

Huh?  ROMFS_MTD_FS is the only XIP filesystem we have.  The bug is quite

probably valid.

--- Mike Frysinger                                           2008-09-25 05:08:53

sorry, i misunderstood the ROMFS relationship.  an easier way to test is to boot

up the system like normal and then attempt to mount the NOR file system on /mnt

and execute from there.  you'll get the same crash.

--- Bernd Schmidt                                            2009-09-03 10:36:42

Should be fixed now, for the no-MPU case.  I'll fix MPU later.

--- Vivi Li                                                  2009-09-18 03:07:51

For no-MPU case, I still fail to test xip on nor flash. Bellow is the log and

config file is attached.

--

bfin> tftp 0x1000000 rootfs.romfs

Using Blackfin EMAC device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'rootfs.romfs'.

Load address: 0x1000000

Loading: #################################################################

         ############################################################

done

Bytes transferred = 1828864 (1be800 hex)

bfin> protect off 0x201C0000 0x203EFFFF

................................... done

Un-Protected 35 sectors

bfin> erase 0x201C0000 0x203EFFFF

................................... done

Erased 35 sectors

bfin> cp.b 0x1000000 0x201C0000 0x1be800

Copy to Flash... done

bfin> tftp 0x1000000 vmImage

Using Blackfin EMAC device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'vmImage'.

Load address: 0x1000000

Loading: ###########################################################

done

Bytes transferred = 856445 (d117d hex)

bfin> set bootargs root=/dev/mtdblock2 rootfstype=romfs ro

bfin> bootm 0x1000000

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   bf537-2.6.30.5-ADI-2010R1-pre-sv

   Created:      2009-09-17   9:41:16 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    856381 Bytes = 836.3 kB

   Load Address: 00001000

   Entry Point:  0017c4f0

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 0017c4f0

console [ttyBF0] enabled, bootconsole disabled

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 55180k/65536k RAM, (112k init code, 1012k kernel code, 464k

data, 1024k dma, 7744k reserved)

Calibrating delay loop... 997.37 BogoMIPS (lpj=1994752)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (37 KB free)

net_namespace: 296 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

ROMFS MTD (C) 2007 Red Hat, Inc.

msgmni has been set to 107

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1,

mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

physmap platform flash device: 00400000 at 20000000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank

Amd/Fujitsu Extended Query Table at 0x0040

number of CFI chips: 1

cfi_cmdset_0002: Disabling erase-suspend-program due to code brokenness.

RedBoot partition parsing not available

Using physmap partition information

Creating 4 MTD partitions on "physmap-flash.0":

0x000000000000-0x000000040000 : "bootloader(nor)"

0x000000040000-0x0000001c0000 : "linux kernel(nor)"

0x0000001c0000-0x0000003f0000 : "file system(nor)"

0x0000003f0000-0x000000400000 : "MAC Address(nor)"

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0,

regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-02-20 08:09:10 UTC (4349350)

VFS: Mounted root (romfs filesystem) readonly on device 31:2.

Freeing unused kernel memory: 112k freed

dma_alloc_init: dma_page @ 0x0018d000 - 256 pages at 0x03f00000

(It hangs here)

--

--- Bernd Schmidt                                            2009-09-19 09:44:53

Can you enable the debugging options at the top of binfmt_flat.c and try again?

It would be good to see what's going on there.

--- Vivi Li                                                  2009-09-21 00:37:44

Only fdpic format can not work and shared-flat is OK. So I modify

binfmt_elf_fdpic.c.

Bellow is the log for fdpic format:

--

Starting Kernel at = 00188530

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 997.37 BogoMIPS (lpj=1994752)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (37 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

ROMFS MTD (C) 2007 Red Hat, Inc.

msgmni has been set to 107

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0x0 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1,

mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

physmap platform flash device: 00400000 at 20000000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank

Amd/Fujitsu Extended Query Table at 0x0040

number of CFI chips: 1

cfi_cmdset_0002: Disabling erase-suspend-program due to code brokenness.

RedBoot partition parsing not available

Using physmap partition information

Creating 4 MTD partitions on "physmap-flash.0":

0x000000000000-0x000000040000 : "bootloader(nor)"

0x000000040000-0x0000001c0000 : "linux kernel(nor)"

0x0000001c0000-0x0000003f0000 : "file system(nor)"

0x0000003f0000-0x000000400000 : "MAC Address(nor)"

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0,

regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-08-06 19:52:05 UTC (18820325)

VFS: Mounted root (romfs filesystem) readonly on device 31:2.

Freeing unused kernel memory: 112k freed

dma_alloc_init: dma_page @ 0x02110000 - 256 pages at 0x03f00000

FDPIC ____ LOAD 1 ____

FDPIC Using ELF interpreter /lib/ld-uClibc.so.0

FDPIC [LOAD] va=0 of=0 fs=280c ms=280c

FDPIC mmap[2] <file> sz=280c pr=5 fl=1802 of=0 --> 20314ce0

FDPIC [LOAD] va=680c of=280c fs=378 ms=3b0

FDPIC mmap[3] <file> sz=bbc pr=3 fl=1802 of=2000 --> 0211a000

FDPIC clear[3] ad=211a000 sz=80c

FDPIC clear[3] ad=211ab84 sz=38

FDPIC Mapped Object [executable]:

FDPIC - elfhdr   : 20314ce0

FDPIC - entry    : 20315f28

FDPIC - PHDR[]   : 20314d14

FDPIC - DYNAMIC[]: 211a820

FDPIC - LOAD[0] : 20314ce0-203174eb [va=0 ms=280c]

FDPIC - LOAD[1] : 0211a80c-0211abbb [va=680c ms=3b0]

FDPIC [LOAD] va=0 of=0 fs=702c ms=702c

FDPIC mmap[0] <file> sz=702c pr=5 fl=802 of=0 --> 20275ac0

FDPIC [LOAD] va=b02c of=702c fs=3a4 ms=450

FDPIC mmap[1] <file> sz=47c pr=3 fl=802 of=7000 --> 0211c000

FDPIC clear[1] ad=211c000 sz=2c

FDPIC clear[1] ad=211c3d0 sz=ac

FDPIC Mapped Object [interpreter]:

FDPIC - elfhdr   : 20275ac0

FDPIC - entry    : 20276c20

FDPIC - PHDR[]   : 20275af4

FDPIC - DYNAMIC[]: 211c0b8

FDPIC - LOAD[0] : 20275ac0-2027caeb [va=0 ms=702c]

FDPIC - LOAD[1] : 0211c02c-0211c47b [va=b02c ms=450]

FDPIC - start_code  20314ce0

FDPIC - end_code    203174ec

FDPIC - start_data  211a80c

FDPIC - end_data    211abbc

FDPIC - start_brk   2120000

FDPIC - brk         2120000

FDPIC - start_stack 213fef0

--

--- Barry Song                                               2009-12-24 00:10:10

vivi:

The bug should have been fixed by Bernd in fdpic mode. I can pass the two

cases:

1. using initramfs, mount a flash partition and run, success

2. using romfs as rootfs directly, success, log:

root:/> mount

rootfs on / type rootfs (rw)

/dev/root on / type romfs (ro,relatime)

proc on /proc type proc (rw,nosuid,nodev,noexec,relatime)

sysfs on /sys type sysfs (rw,nosuid,nodev,noexec,relatime)

mdev on /dev type tmpfs (rw,nosuid,relatime,mode=0755,size=10M)

devpts on /dev/pts type devpts (rw,nosuid,noexec,relatime,mode=600)

var on /var type ramfs (rw,relatime)

tmp on /tmp type tmpfs (rw,nosuid,nodev,relatime)

debugfs on /sys/kernel/debug type debugfs (rw,relatime)

root:/> uname -a

Linux blackfin 2.6.32-ADI-2010R1-pre-svn8000 #72 Thu Dec 24 12:31:38 CST 2009

blackfin GNU/Linux

-barry

--- Vivi Li                                                  2010-02-10 03:46:40

OK, close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.user.fdpic    text/plain    44771    Vivi Li

config.kernel.fdpic    text/plain    19796    Vivi Li

config.xip.fdpic_9.18    application/octet-stream    27164    Vivi Li

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.