Article [#4139] build pound on trunk fails for missing OpenSSL (-lcrypto)

[#4139] build pound on trunk fails for missing OpenSSL (-lcrypto)

Submitted By: Mingquan Pan

Open Date

2008-06-02 06:34:07     Close Date

2008-07-06 23:00:23

Priority:

Medium     Assignee:

Mike Frysinger

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

08r1-8

App binary format:

N/A     

Summary: build pound on trunk fails for missing OpenSSL (-lcrypto)

Details:

build pound on trunk fails  for missing OpenSSL (-lcrypto).

make[4]: Entering directory `/home/test/work/cruise/checkouts/uclinux-dist/user/blkfin-apps/pound'

./configure --with-ssl=/home/test/work/cruise/checkouts/uclinux-dist/lib/libssl --host=bfin-uclinux \

--prefix=/usr/local --disable-super \

LDFLAGS=" -Wl,-elf2flt    -mcpu=bf537-0.2 -L/home/test/work/cruise/checkouts/uclinux-dist/lib/libssl"

configure: WARNING: If you wanted to set the --build type, don't use --host.

    If a cross compiler is detected then cross compile mode will be used.

checking for bfin-uclinux-gcc... bfin-uclinux-gcc

checking for C compiler default output file name... a.out

checking whether the C compiler works... yes

checking whether we are cross compiling... yes

checking for suffix of executables...

checking for suffix of object files... o

checking whether we are using the GNU C compiler... yes

checking whether bfin-uclinux-gcc accepts -g... yes

checking for bfin-uclinux-gcc option to accept ANSI C... none needed

checking for a BSD-compatible install... /usr/bin/install -c

checking build system type... i686-pc-linux-gnu

checking host system type... bfin-unknown-uclinux

checking target system type... bfin-unknown-uclinux

checking for the pthreads library -lpthreads... no

checking whether pthreads work without any flags... no

checking whether pthreads work with -Kthread... no

checking whether pthreads work with -kthread... no

checking for the pthreads library -llthread... no

checking whether pthreads work with -pthread... yes

checking for joinable pthread attribute... PTHREAD_CREATE_JOINABLE

checking if more special flags are required for pthreads... no

checking for cc_r... bfin-uclinux-gcc

checking for dlopen in -ldl... no

checking for socket in -lsocket... no

checking for BIO_new in -lcrypto... no

Missing OpenSSL (-lcrypto) - aborted

make[4]: *** [Makefile] Error 1

make[4]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/user/blkfin-apps/pound'

make[3]: *** [all] Error 2

make[3]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/user/blkfin-apps'

make[2]: *** [blkfin-apps] Error 2

make[2]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/user'

make[1]: *** [all] Error 2

make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/user'

make: *** [subdirs] Error 1

config.log is attached.

Follow-ups

--- Mike Frysinger                                           2008-07-04 10:16:26

should be fixed now

--- Mingquan Pan                                             2008-07-06 23:00:22

Yes,close.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.log    text/x-log    22440    Mingquan Pan

Attachments:

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.