Article [#4182] l1_app test failed in SMP kernel

[#4182] l1_app test failed in SMP kernel

Submitted By: Vivi Li

Open Date

2008-06-23 02:53:41     Close Date

2008-10-17 00:24:27

Priority:

Medium     Assignee:

Vivi Li

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

08r1.5-11

App binary format:

N/A     

Summary: l1_app test failed in SMP kernel

Details:

l1_app test failed in SMP kernel with the following log:

--

root:/> ./test_helloworld

hello

[INS] get 2 from helloworld(0xff6002e4):        TEST FAIL

[INS] get 11 from testl1(0xff600030):   TEST FAIL

[DATA] global data ret at 0xff400000:   TEST FAIL

[INS] main at 0x344a9e8:        TEST PASS

root:/> ./test_helloworld_stack

[STACK] get internal variable in at [0x378cef8]:        TEST FAIL

root:/>

--

Follow-ups

--- Graf Yang                                                2008-06-25 02:47:13

This test APP only writed for run on CoreA.

--- Mike Frysinger                                           2008-06-25 07:44:04

then the test needs updating to set cpu affinity before executing so that it

makes sure to run on Core A

--- Vivi Li                                                  2008-10-16 06:38:42

After I set affinity in test_helloworld.c, I can see bus error a few times. It

seem hard to duplicate this problem.

--- Vivi Li                                                  2008-10-17 00:24:27

Close this bug as this one is solved.

I will open a new one about l1_app.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.