Article [#4202] GPIO interrupts not disabled; edge sensitive interrupt hang system

[#4202] GPIO interrupts not disabled; edge sensitive interrupt hang system

Submitted By: Michael McTernan

Open Date

2008-06-26 05:08:25     Close Date

2008-07-10 10:24:09

Priority:

Medium     Assignee:

Michael Hennerich

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2008R1-RC8     Release:

2008R1

Category:

Kernel Functions     Board:

Custom

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

App binary format:

N/A     

Summary: GPIO interrupts not disabled; edge sensitive interrupt hang system

Details:

Hi,

In arch/blackfin/mach-common/ints-priority.c bfin_gpio_irqchip does not define .enable and .disable.  This means that the GPIOs remain in the MASKA register after disabling, causing possible further interrupts. 

This can be overlooked for edge sensitive interrupts as the kernel sets IRQ_DISABLED on the interrupt descriptors when disable_irq() is called,   preventing unexpected handler execution.

For level sensitive interrupts the situation may not be so good.  Calling disable_irq_nosync() in the interrupt handler marks the interrupt as IRQ_DISABLE but leaves the source active.  If the GPIO is not rapidly cleared the system can stall while the GPO further interrupts the processor but does nothing due to IRQ_DISABLED having been set.  (For background, my driver uses a level sensitive interrupt from the device, and merely calls disable_irq_nosync() in the interrupt in the handler, leaving the actual device access and eventual interrupt source clearing to some deferred processing as it is quite complex and involved).

The fix is to add entries for .disable and .enable into the two bfin_gpio_irqchip structures (one is for !CONFIG_BF54x, one is for the #else case):

static struct irq_chip bfin_gpio_irqchip = {

    .ack = bfin_gpio_ack_irq,

    .mask = bfin_gpio_mask_irq,

    .mask_ack = bfin_gpio_mask_ack_irq,

    .unmask = bfin_gpio_unmask_irq,

    .disable = bfin_gpio_mask_irq,     /* fix for level sensitive */

    .enable = bfin_gpio_unmask_irq,    /* fix for level sensitive */

    .set_type = bfin_gpio_irq_type,

    .startup = bfin_gpio_irq_startup,

    .shutdown = bfin_gpio_irq_shutdown,

#ifdef CONFIG_PM

    .set_wake = bfin_gpio_set_wake,

#endif

};

This drops the GPIO source from MASKA when disabled, adding it when re-enabled, and prevents actual interrupt events being generated for disabled GPOs.  This makes level sensitive interrupts easier to use, and removes any performance hit from interrupting the processor for disabled irqs. 

A patch is attached.

Kind Regards,

Mike

Follow-ups

--- Michael McTernan                                         2008-06-26 06:44:03

Correction: title should read "level sensitive interrupts hang

system".

--- Michael Hennerich                                        2008-06-26 06:44:46

Assign to me.

I fixed a similar issue some time ago for internal irqs.

  blackfin.uclinux.org/gf/project/linux-kernel/scmsvn/?action=browse&path=%2F&view=rev&revision=4299

At that point I thought it wouldn't be an issue for GPIO irqs.

-Michael

--- Michael Hennerich                                        2008-06-26 07:02:19

Fixed on 2008R1 and on trunk.

Thanks for pointing this out.

IIRC the code used to call mask instead, in case disable is not implemented.

But this must have changed in the meanwhile. For enable I think this is still

the case.

-Michael

--- Michael Hennerich                                        2008-07-10 10:24:09

close it.

-Michael

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

gpio-enabledisable.patch    application/octet-stream    790    Michael McTernan

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.