Article [#4270] linphone has underrun through ad73322 card on bf537

[#4270] linphone has underrun through ad73322 card on bf537

Submitted By: Mingquan Pan

Open Date

2008-07-22 05:13:20     Close Date

2008-07-29 05:54:19

Priority:

Medium High     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

08r1.5-14

App binary format:

N/A     

Summary: linphone has underrun through ad73322 card on bf537

Details:

linphone has underrun when testing through ad73322 card on bf537.Normally it would print twice in about 20 miniutes.

lackfin support (C) 2004-2007 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 100 MHz System Clock

Board Memory: 64MB

Kernel Managed Memory: 64MB                                                                                                                               

...Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).

dma_alloc_init: dma_page @ 0x033af000 - 512 pages at 0x03e00000

ALSA device list:

  #0: Analog Devices AD73322 at PF10 SPORT0 rx/tx dma 3/4 err irq 45

TCP cubic registered                                                                                                                                      

...

spawn linphonec

Ready.

linphonec>

Case 1 ...PASS

linphonec

NLS disabled.

Ready

Warning: video is disabled in linphonec.

linphonec>

Case 1 ...PASS

<sip:toto@10.100.4.50> is calling you.

Case 2 ...PASS

answer

Connected.

Case 2 ...PASS

call sip:test@10.100.4.174

Contacting sip:test@10.100.4.174

linphonec> linphonec> Connected.

linp

Case 2 ...PASS

honec> underrun happened!!!

underrun happened!!!

Case 3 ...FAIL

Follow-ups

--- Cliff Cai                                                2008-07-28 22:53:11

Adjusting the DMA period size seems help to sovle this problem.

Cliff

--- Mingquan Pan                                             2008-07-29 05:54:17

Yeah, it didn't print underrun in more than an hour now.So close.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.