Article [#4279] In BF533-EZKIT 08r1 branch, irq number of BFIN Timer Tick is changed

[#4279] In BF533-EZKIT 08r1 branch, irq number of BFIN Timer Tick is changed

Submitted By: Vivi Li

Open Date

2008-07-25 03:35:42     Close Date

2008-07-27 22:49:42

Priority:

Medium     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

08r1.5-13

App binary format:

N/A     

Summary: In BF533-EZKIT 08r1 branch, irq number of BFIN Timer Tick is changed

Details:

In BF533-EZKIT 08r1 branch, irq number of BFIN Timer Tick has been changed from 6 to 23.

--

Linux version 2.6.22.19-ADI-2008R1.5-svn5045 (test@uclinux46-bf533ezkit) (gcc version 4.1.2 (ADI sv8

Hardware Trace Active and Enabled

Warning: limiting memory to 31MB due to hardware anomaly 05000263

Reset caused by Software reset

Blackfin support (C) 2004-2007 Analog Devices, Inc.

Compiled for ADSP-BF533 Rev 0.3

Warning: Compiled for Rev 3, but running on Rev 4

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 594 MHz core clock and 118 MHz System Clock

Board Memory: 32MB

Kernel Managed Memory: 32MB

Memory map:

  text      = 0x00001000-0x0011f170

  rodata    = 0x00120000-0x0016ad60

  data      = 0x0016b000-0x0017c000

    stack   = 0x0016c000-0x0016e000

  init      = 0x0017c000-0x0049b000

  bss       = 0x0049b000-0x004c56d0

  available = 0x004c56d0-0x01eff000

  DMA Zone  = 0x01f00000-0x02000000

Instruction Cache Enabled

Data Cache Enabled (write-through)

Built 1 zonelists.  Total pages: 7874

Kernel command line: root=/dev/mtdblock0 rw ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:f

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 128 (order: 7, 512 bytes)

I-pipe 1.7-00: pipeline enabled.

Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)

Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)

Memory available: 26556k/32768k RAM, (3196k init code, 1144k kernel code, 541k data, 1024k dma, 308)

Blackfin Scratchpad data SRAM: 4 KB

Blackfin Data A SRAM: 16 KB (15 KB free)

Blackfin Data B SRAM: 16 KB (16 KB free)

Blackfin Instruction SRAM: 64 KB (55 KB free)

Security Framework v1.0.0 initialized

Mount-cache hash table entries: 512

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

ezkit_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 1024 (order: 1, 8192 bytes)

TCP bind hash table entries: 1024 (order: 0, 4096 bytes)

TCP: Hash tables configured (established 1024 bind 1024)

TCP reno registered

I-pipe: Domain Xenomai registered.

Xenomai: hal/blackfin started.

Xenomai: real-time nucleus v2.4.0 (Bells Of Lal) loaded.

Xenomai: starting default API services.

Xenomai: starting POSIX services.

Xenomai: starting RTDM services.

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 21) is a BFIN-UART

RAMDISK driver initialized: 16 RAM disks of 4096K size 1024 blocksize

smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@cam.org>

eth0: SMC91C11xFD (rev 1) at 20310300 IRQ 42 [nowait]

eth0: Ethernet addr: 00:e0:22:fe:b1:2e

bfin-spi bfin-spi.0: Blackfin BF5xx on-chip SPI Contoller Driver, Version 1.0, regs_base@ffc00500, 5

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

TCP cubic registered

NET: Registered protocol family 1

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting the system clock to 2004-05-31 22:54:18 (1086044058)

eth0: link down

IP-Config: Complete:

      device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=10.100.4.50, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 3196k freed

dma_alloc_init: dma_page @ 0x00498000 - 256 pages at 0x01f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

  u  p ,8 .1.0 08M b p s ,    f u|l|l_-|d|u|p|l|e|x|,| /l p a   0 x|C

                                                                     5 E   d/      `8b.       \ 1

\____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.4.1 (2008-07-24 16:24:17 CST) Built-in shell (msh)

Enter 'help' for a list of built-in commands.

root:/>

root:/>

root:/>

root:/>

root:/> cat /proc/interrupts

21:          0   BFIN_UART_RX

22:       6073   BFIN_UART_TX

23:       4898   BFIN Timer Tick

42:          1   eth0

Err:          0

root:/>

--

Follow-ups

--- Sonic Zhang                                              2008-07-25 06:44:49

This is a test script fault in Xenomai case. Forget to unselect Xemonai option

after testing.

--- Vivi Li                                                  2008-07-27 22:49:41

OK now. Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.