Article [#4282] build kernel with power management failed in 08r1 branch BF533-EZKIT

[#4282] build kernel with power management failed in 08r1 branch BF533-EZKIT

Submitted By: Vivi Li

Open Date

2008-07-27 23:06:31     Close Date

2008-07-28 05:03:58

Priority:

Medium     Assignee:

Vivi Li

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

N/A

Uboot version or rev.:

    Toolchain version or rev.:

08r1.5-13

App binary format:

N/A     

Summary: build kernel with power management failed in 08r1 branch BF533-EZKIT

Details:

In 08r1 branch BF533-EZKIT, build kernel with power management failed with the following error message. Attached is the config.

--

  LD      .tmp_vmlinux1^M

  KSYM    .tmp_kallsyms1.S^M

  AS      .tmp_kallsyms1.o^M

  LD      .tmp_vmlinux2^M

  KSYM    .tmp_kallsyms2.S^M

  AS      .tmp_kallsyms2.o^M

  LD      vmlinux^M

  SYSMAP  System.map^M

  SYSMAP  .tmp_System.map^M

  MODPOST vmlinux^M

  OBJCOPY arch/blackfin/boot/vmlinux.bin^M

  GZIP    arch/blackfin/boot/vmlinux.gz^M

  UIMAGE  arch/blackfin/boot/vmImage^M

Image Name:   Linux-2.6.22.19-ADI-2008R1.5-svn^M

Created:      Sun Jul 27 21:58:20 2008^M

Image Type:   Blackfin Linux Kernel Image (gzip compressed)^M

Data Size:    864510 Bytes = 844.25 kB = 0.82 MB^M

Load Address: 0x00001000^M

Entry Point:  0x00164000^M

Kernel: arch/blackfin/boot/vmImage is ready^M

  Building modules, stage 2.^M

  MODPOST 30 modules^M

ERROR: "sport_set_tx_callback" [sound/soc/blackfin/snd-soc-bf5xx.ko] undefined!^M

ERROR: "sport_config_tx_dma" [sound/soc/blackfin/snd-soc-bf5xx.ko] undefined!^M

ERROR: "sport_set_rx_callback" [sound/soc/blackfin/snd-soc-bf5xx.ko] undefined!^M

ERROR: "sport_tx_stop" [sound/soc/blackfin/snd-soc-bf5xx.ko] undefined!^M

ERROR: "sport_done" [sound/soc/blackfin/snd-soc-bf5xx.ko] undefined!^M

ERROR: "sport_rx_stop" [sound/soc/blackfin/snd-soc-bf5xx.ko] undefined!^M

ERROR: "sport_config_rx_dma" [sound/soc/blackfin/snd-soc-bf5xx.ko] undefined!^M

ERROR: "sport_handle" [sound/soc/blackfin/snd-soc-bf5xx.ko] undefined!^M

ERROR: "bf5xx_pcm_to_frame" [sound/soc/blackfin/snd-soc-bf5xx.ko] undefined!^M

ERROR: "sport_rx_start" [sound/soc/blackfin/snd-soc-bf5xx.ko] undefined!^M

ERROR: "sport_tx_start" [sound/soc/blackfin/snd-soc-bf5xx.ko] undefined!^M

ERROR: "bf5xx_frame_to_pcm" [sound/soc/blackfin/snd-soc-bf5xx.ko] undefined!^M

make[2]: *** [__modpost] Error 1^M

make[1]: *** [modules] Error 2^M

make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x'^M

make: *** [linux] Error 1^M

--

Follow-ups

--- Sonic Zhang                                              2008-07-27 23:58:37

Need to update the build script.

--- Vivi Li                                                  2008-07-28 05:03:57

Build script is updated. Close it.

Thanks!

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.power    text/plain    23821    Vivi Li

Attachments:

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.