Article [#4324] unload spi_mmc driver module may cause race condition when spi framework is enabled

[#4324] unload spi_mmc driver module may cause race condition when spi framework is enabled

Submitted By: Yi Li

Open Date

2008-08-07 23:44:13     Close Date

2008-08-11 04:50:50

Priority:

Medium     Assignee:

Yi Li

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

2008r1 branch

Category:

N/A     Board:

STAMP

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

App binary format:

N/A     

Summary: unload spi_mmc driver module may cause race condition when spi framework is enabled

Details:

As reported in forum thread:

  blackfin.uclinux.org/gf/project/uclinux-dist/forum/?action=ForumBrowse&forum_id=39&_forum_action=ForumMessageBrowse&thread_id=28878

If kernel configure enables:

#

# SPI support

#

CONFIG_SPI=y

CONFIG_SPI_MASTER=y

and

"CONFIG_SPI_MMC=m

# CONFIG_SPI_MMC_FRAMEWORK_DRIVER is not set

CONFIG_SPI_MMC_BFIN_PIO_SPI=y"

at the same time, unloading "spi_mmc" driver module may cause warning (and exception).

root:/> modprobe spi_mmc                                                       

mmc_pio_spi:cs_#: 0x4, baud=0x0, flag=0xff00, ctrl=0x400                       

root:/> modprobe -r spi_mmc                                                    

WARNING: at lib/kref.c:33 kref_get()                                           

Hardware Trace:                                                                

   0 Target : <0x0000479c> { _dump_stack + 0x0 }                               

     Source : <0x0007beec> { _kref_get + 0x54 }                                

   1 Target : <0x0007beec> { _kref_get + 0x54 }                                

     Source : <0x0000d702> { _printk + 0x16 }                                  

   2 Target : <0x0000d6fe> { _printk + 0x12 }                                  

     Source : <0x0000d5b4> { _vprintk + 0x1b8 }                                

   3 Target : <0x0000d5a8> { _vprintk + 0x1ac }                                

     Source : <0xffa00cf0> { __common_int_entry + 0xd8 }                       

   4 Target : <0xffa00c8e> { __common_int_entry + 0x76 }                       

     Source : <0xffa00ac0> { _return_from_int + 0x58 }                         

   5 Target : <0xffa00ac0> { _return_from_int + 0x58 }                         

     Source : <0xffa00a96> { _return_from_int + 0x2e }                         

   6 Target : <0xffa00a68> { _return_from_int + 0x0 }                          

     Source : <0xffa00c8a> { __common_int_entry + 0x72 }                       

   7 Target : <0xffa00c88> { __common_int_entry + 0x70 }                       

     Source : <0xffa003ec> { _asm_do_IRQ + 0x68 }                              

   8 Target : <0xffa003e4> { _asm_do_IRQ + 0x60 }                              

     Source : <0x000117ee> { __local_bh_enable + 0x3e }                        

   9 Target : <0x000117b0> { __local_bh_enable + 0x0 }                         

     Source : <0x000118f8> { ___do_softirq + 0x94 }                            

  10 Target : <0x000118f0> { ___do_softirq + 0x8c }                            

     Source : <0x000118d0> { ___do_softirq + 0x6c }                            

  11 Target : <0x000118c4> { ___do_softirq + 0x60 }                            

     Source : <0x000119d8> { _tasklet_action + 0x7c }                          

  12 Target : <0x000119d2> { _tasklet_action + 0x76 }                          

     Source : <0x000119ae> { _tasklet_action + 0x52 }                          

  13 Target : <0x000119ac> { _tasklet_action + 0x50 }                          

     Source : <0x0001b456> { ___rcu_process_callbacks + 0xb6 }                 

  14 Target : <0x0001b450> { ___rcu_process_callbacks + 0xb0 }                 

     Source : <0x0001b3e6> { ___rcu_process_callbacks + 0x46 }                 

  15 Target : <0x0001b3e2> { ___rcu_process_callbacks + 0x42 }                 

     Source : <0x0001b47e> { ___rcu_process_callbacks + 0xde }                 

Stack from 00421e08:                                                           

        0002dbb2 0007bef0 0378ed44 0378ed2c 00000000 0012944c 00000021 000ffe88

        0007b342 0378eec0 0000006a 00000044 00000003 000947ee 0378ed24 00000000

        037cca60 00000001 00094806 00000017 00421e80 00009bfe 00093bd8 00094760

        00000000 00421ea8 00014658 006bd3a0 0378d08e 0378eec0 00146578 00000081

        033ecfe8 00000001 00000000 000268da 0043c028 00000000 0000000a 00421ea0

        5f697073 00636d6d 00000000 00000000 00000000 00000000 00000000 00000000

                                                                               

Call Trace:                                                                    

[<00026760>] _sys_delete_module+0x0/0x1e8                                      

[<0000fffe>] _do_exit+0x57a/0x760                                              

[<00008000>] _sram_free+0x14/0x44                                              

[<0015cec5>] _bfin_init_mmr_debugfs+0x48c5/0x7074                              

[<0015e181>] _bfin_init_mmr_debugfs+0x5b81/0x7074                              

[<0015cec4>] _bfin_init_mmr_debugfs+0x48c4/0x7074                              

[<0015e174>] _bfin_init_mmr_debugfs+0x5b74/0x7074                              

                                                                               

WARNING: at lib/kref.c:33 kref_get()                                           

Hardware Trace:                                                                

   0 Target : <0x0000479c> { _dump_stack + 0x0 }                               

     Source : <0x0007beec> { _kref_get + 0x54 }                                

   1 Target : <0x0007beec> { _kref_get + 0x54 }                                

     Source : <0x0000d702> { _printk + 0x16 }                                  

   2 Target : <0x0000d6fe> { _printk + 0x12 }                                  

     Source : <0x0000d5b4> { _vprintk + 0x1b8 }                                

   3 Target : <0x0000d5a8> { _vprintk + 0x1ac }                                

     Source : <0xffa00cf0> { __common_int_entry + 0xd8 }                       

   4 Target : <0xffa00c8e> { __common_int_entry + 0x76 }                       

     Source : <0xffa00ac0> { _return_from_int + 0x58 }                         

   5 Target : <0xffa00ac0> { _return_from_int + 0x58 }                         

     Source : <0xffa00a96> { _return_from_int + 0x2e }                         

   6 Target : <0xffa00a68> { _return_from_int + 0x0 }                          

     Source : <0xffa00c8a> { __common_int_entry + 0x72 }                       

   7 Target : <0xffa00c88> { __common_int_entry + 0x70 }                       

     Source : <0xffa003ec> { _asm_do_IRQ + 0x68 }                              

   8 Target : <0xffa003e4> { _asm_do_IRQ + 0x60 }                              

     Source : <0x000117ee> { __local_bh_enable + 0x3e }                        

   9 Target : <0x000117b0> { __local_bh_enable + 0x0 }                         

     Source : <0x000118f8> { ___do_softirq + 0x94 }                            

  10 Target : <0x000118f0> { ___do_softirq + 0x8c }                            

     Source : <0x000118d0> { ___do_softirq + 0x6c }                            

  11 Target : <0x000118c4> { ___do_softirq + 0x60 }                            

     Source : <0x000119d8> { _tasklet_action + 0x7c }                          

  12 Target : <0x000119d2> { _tasklet_action + 0x76 }                          

     Source : <0x000119ae> { _tasklet_action + 0x52 }                          

  13 Target : <0x000119ac> { _tasklet_action + 0x50 }                          

     Source : <0x0001b456> { ___rcu_process_callbacks + 0xb6 }                 

  14 Target : <0x0001b450> { ___rcu_process_callbacks + 0xb0 }                 

     Source : <0x0001b3e6> { ___rcu_process_callbacks + 0x46 }                 

  15 Target : <0x0001b3e2> { ___rcu_process_callbacks + 0x42 }                 

     Source : <0x0001b47e> { ___rcu_process_callbacks + 0xde }                 

Stack from 00421e08:                                                           

        0002dbb2 0007bef0 0378ed44 0378ed2c 00000000 0012944c 00000021 000ffe88

        0007b342 0378eec0 0000006a 00000044 00000003 000947ee 0378ed24 0378ed24

        00000081 0007b304 00094806 00000017 00421e80 00009bfe 00093be6 00094760

        00000000 00421ea8 00014658 006bd3a0 0378d08e 0378eec0 00146578 00000081

        033ecfe8 00000001 00000000 000268da 0043c028 00000000 0000000a 00421ea0

        5f697073 00636d6d 00000000 00000000 00000000 00000000 00000000 00000000

                                                                               

Call Trace:                                                                    

[<00026760>] _sys_delete_module+0x0/0x1e8                                      

[<0000fffe>] _do_exit+0x57a/0x760                                              

[<00008000>] _sram_free+0x14/0x44                                              

[<0015cec5>] _bfin_init_mmr_debugfs+0x48c5/0x7074                              

[<0015e181>] _bfin_init_mmr_debugfs+0x5b81/0x7074                              

[<0015cec4>] _bfin_init_mmr_debugfs+0x48c4/0x7074                              

[<0015e174>] _bfin_init_mmr_debugfs+0x5b74/0x7074                              

                                                                               

NULL pointer access (probably)                                                 

Kernel OOPS in progress                                                        

Defered Exception context                                                      

CURRENT PROCESS:                                                               

COMM=rmmod PID=102                                                             

TEXT = 0x00600000-0x00656e40        DATA = 0x00430e40-0x0043c134               

BSS = 0x0043c134-0x00440000  USER-STACK = 0x0045feb0                          

                                                                               

return address: [0x000f6e8a]; contents of:                                     

0x000f6e60:  3045  0064  6c66  0127  3006  05b3  0010  ac5a                    

0x000f6e70:  3042  0807  17eb  6006  2fef  ac5a  9117  2fe3                    

0x000f6e80:  05fd  3228  0167  6fa6  916a [a0d7] e3ff  ffc2                    

0x000f6e90:  0c00  1c09  0c07  1807  3217  6c66  0127  3045                    

                                                                               

SEQUENCER STATUS:               Not tainted                                    

SEQSTAT: 00000027  IPEND: 8030  SYSCFG: 0006                                  

  HWERRCAUSE: 0x0                                                              

  EXCAUSE   : 0x27                                                             

  physical IVG15 asserted : <0xffa00e50> { _evt_system_call + 0x0 }            

  logical irq   6 mapped  : <0xffa00250> { _timer_interrupt + 0x0 }            

  logical irq  18 mapped  : <0x000912b8> { _bfin_serial_dma_rx_int + 0x0 }     

  logical irq  19 mapped  : <0x00091224> { _bfin_serial_dma_tx_int + 0x0 }     

  logical irq  24 mapped  : <0x0009abd4> { _bf537mac_interrupt + 0x0 }         

RETE: <0x00000000> /* Maybe null pointer? */                                  

RETN: <0x00421e40> /* unknown address */                                      

RETX: <0x000f6e8a> { _klist_del + 0xa }                                       

RETS: <0x000f6f18> { _klist_remove + 0xc }                                    

PC  : <0x000f6e8a> { _klist_del + 0xa }                                       

DCPLB_FAULT_ADDR: <0x0000000c> /* Maybe null pointer? */                       

ICPLB_FAULT_ADDR: <0x000f6e8a> { _klist_del + 0xa }                            

                                                                               

PROCESSOR STATE:                                                               

R0 : 0378ed78    R1 : 0378ed24    R2 : 0000001f    R3 : 0000001f              

R4 : 00608850    R5 : 00432108    R6 : 00000000    R7 : 0378ed78              

P0 : 0000000a    P1 : 0014c954    P2 : 00000000    P3 : 0014d764              

P4 : 0378ed24    P5 : 0378ed78    FP : 0045fd54    SP : 00421d64              

LB0: 0015e181    LT0: 0015e174    LC0: 00000000                               

LB1: 0007eaec    LT1: 0007eae2    LC1: 00000000                               

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 033ecfe8              

B1 : 00000000    L1 : 00000000    M1 : 03362bac    I1 : 0000180b              

B2 : 00000000    L2 : 00000000    M2 : 033e4534    I2 : 00421cc4              

B3 : 00000000    L3 : 00000000    M3 : 033e453c    I3 : 00000000              

A0.w: 0000007f   A0.x: 00000000   A1.w: 0000007f   A1.x: 00000000              

USP : 0045fd48  ASTAT: 02002020                                                

                                                                               

Hardware Trace:                                                                

   0 Target : <0x000048c0> { _trap_c + 0x0 }                                   

     Source : <0xffa0075c> { _exception_to_level5 + 0xb4 }                     

   1 Target : <0xffa006a8> { _exception_to_level5 + 0x0 }                      

     Source : <0xffa00604> { _ex_trap_c + 0x5c }                               

   2 Target : <0xffa005a8> { _ex_trap_c + 0x0 }                                

     Source : <0xffa00442> { _ex_workaround_261 + 0x22 }                       

   3 Target : <0xffa00420> { _ex_workaround_261 + 0x0 }                        

     Source : <0xffa007fc> { _trap + 0x28 }                                    

   4 Target : <0xffa007d4> { _trap + 0x0 }                                     

     Source : <0xffa0054a> { _bfin_return_from_exception + 0xe }               

   5 Target : <0xffa0053c> { _bfin_return_from_exception + 0x0 }               

     Source : <0xffa00432> { _ex_workaround_261 + 0x12 }                       

   6 Target : <0xffa00420> { _ex_workaround_261 + 0x0 }                        

     Source : <0xffa007fc> { _trap + 0x28 }                                    

   7 Target : <0xffa007d4> { _trap + 0x0 }                                     

     Source : <0x000f6e88> { _klist_del + 0x8 }                                

   8 Target : <0x000f6e80> { _klist_del + 0x0 }                                

     Source : <0x000f6f14> { _klist_remove + 0x8 }                             

   9 Target : <0x000f6f0c> { _klist_remove + 0x0 }                             

     Source : <0x00093c1a> { _bus_remove_driver + 0x5e }                       

  10 Target : <0x00093c12> { _bus_remove_driver + 0x56 }                       

     Source : <0x00093bee> { _bus_remove_driver + 0x32 }                       

  11 Target : <0x00093be6> { _bus_remove_driver + 0x2a }                       

     Source : <0x0007be4a> { _kref_put + 0x52 }                                

  12 Target : <0x0007be42> { _kref_put + 0x4a }                                

     Source : <0x0007b2a6> { _kobject_put + 0x12 }                             

  13 Target : <0x0007b2a6> { _kobject_put + 0x12 }                             

     Source : <0x0007b296> { _kobject_put + 0x2 }                              

  14 Target : <0x0007b294> { _kobject_put + 0x0 }                              

     Source : <0x0007b2fc> { _kobject_cleanup + 0x54 }                         

  15 Target : <0x0007b2f4> { _kobject_cleanup + 0x4c }                         

     Source : <0x0007b2ea> { _kobject_cleanup + 0x42 }                         

Stack from 00421d44:                                                           

        00421d48 ffa00760 0014656c 0014656c 00146568 63725f5f 72705f75 7365636f

        000f6e8a 00008030 00000027 00000000 00421e40 000f6e8a 000f6e8a 000f6f18

        0378ed78 02002020 0007eaec 0015e181 0007eae2 0015e174 00000000 00000000

        0000007f 00000000 0000007f 00000000 00000000 00000000 00000000 00000000

        00000000 00000000 00000000 00000000 033e453c 033e4534 03362bac 00000000

        00000000 00421cc4 0000180b 033ecfe8 0045fd48 0045fd54 0378ed78 0378ed24

                                                                               

Call Trace:                                                                    

[<000f6f18>] _klist_remove+0xc/0x1c                                            

[<00009bfe>] _task_running_tick+0x202/0x278                                    

[<00093be6>] _bus_remove_driver+0x2a/0x8c                                      

[<00093c1e>] _bus_remove_driver+0x62/0x8c                                      

[<00094760>] _driver_unregister+0x0/0x4                                        

[<00014658>] _run_timer_softirq+0x14/0x16c                                     

[<0378d08e>] _cleanup_module+0x1a/0x2c [spi_mmc]                               

[<000268da>] _sys_delete_module+0x17a/0x1e8                                    

[<00026760>] _sys_delete_module+0x0/0x1e8                                      

[<0000fffe>] _do_exit+0x57a/0x760                                              

[<00008000>] _sram_free+0x14/0x44                                              

[<0015cec5>] _bfin_init_mmr_debugfs+0x48c5/0x7074                              

[<0015e181>] _bfin_init_mmr_debugfs+0x5b81/0x7074                              

[<0015cec4>] _bfin_init_mmr_debugfs+0x48c4/0x7074                              

[<0015e174>] _bfin_init_mmr_debugfs+0x5b74/0x7074                              

                                                                               

Modules linked in: spi_mmc                                                     

Kernel panic - not syncing: Kernel exception 

Follow-ups

--- Yi Li                                                    2008-08-08 00:46:38

A fix the Kconfig has been checked into svn branch 2008R1:

(Sorry for the reverse order)

Revision

5122

        Author

adamliyi

        Date

2008-08-07 22:28:34 -0500 (Thu, 07 Aug 2008)

        Log Message

When selecting to use SPI PIO mode, make sure SPI_MASTER will not be enabled.

Otherwise, there would be exception when unloading the driver.

See forum thread:

  blackfin.uclinux.org/gf/project/uclinux-dist/forum/?action=ForumBrowse&forum_id=39&_forum_action=ForumMessageBrowse&thread_id=28878

Modified Paths

branches/2008R1/drivers/mmc/spi_mmc/Kconfig

      * Diff

Modified: branches/2008R1/drivers/mmc/spi_mmc/Kconfig (5121 => 5122)

--- branches/2008R1/drivers/mmc/spi_mmc/Kconfig    2008-08-07 14:59:20 UTC (rev

5121)

+++ branches/2008R1/drivers/mmc/spi_mmc/Kconfig    2008-08-08 03:28:34 UTC (rev

5122)

@@ -23,13 +23,13 @@

config SPI_MMC_FRAMEWORK_DRIVER

     bool "SPI framework master"

-    depends on SPI

+    depends on SPI_MASTER

     help

       Will use the SPI master of the system. This option is platform indepenent.

config SPI_MMC_BFIN_PIO_SPI

     bool "Blackfin SPI bus directly"

-    depends on BLACKFIN

+    depends on BLACKFIN && !SPI_MASTER

     help

       Will use Blackfin SPI bus directly. No other SPI device should be used with

this option.

       The MMC/SD card will be driven in SPI PIO mode. This is a failsafe option

for testing.

--- Yi Li                                                    2008-08-08 04:39:41

Sonic mentions this fix is not good in case of BF548 (and other system with more

than on SPI bus). It is possible to set SPI framework managing one bus, while

allow other device using another bus exclusively (without using the framework).

--- Yi Li                                                    2008-08-11 00:33:43

I will revert the fix - Even if using "SPI_MMC_BFIN_PIO_SPI" driver

when "CONFIG_SPI" is enabled will cause problems, we don't limit the

user to Build the driver - it is their responsibility to use it correctly.

--- Yi Li                                                    2008-08-11 05:50:52

Since this is not a bug  - close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.